j721e Navigator Subsystem Descriptions¶
Introduction¶
This chapter provides information on the Navigator Subsystems in the j721e SoC. Some System Firmware TISCI messages take Navigator Subsystem specific inputs. This chapter provides information on the valid values for applicable TISCI message parameters.
Navigator Subsystem Device IDs¶
Some System Firmware TISCI message APIs require the device ID of the Navigator Subsystem to be modified as part of the request. Based on j721e Device IDs these are the valid Navigator Subsystem device IDs.
| Interrupt Aggregator Device Name | Interrupt Aggregator Device ID |
|---|---|
| J721E_DEV_NAVSS0_MODSS_INTAGGR_0 | 207 |
| J721E_DEV_NAVSS0_MODSS_INTAGGR_1 | 208 |
| J721E_DEV_NAVSS0_UDMASS_INTAGGR_0 | 209 |
| J721E_DEV_MCU_NAVSS0_INTAGGR_0 | 233 |
| Ring Accelerator Device Name | Ring Accelerator Device ID |
|---|---|
| J721E_DEV_NAVSS0_RINGACC_0 | 211 |
| J721E_DEV_MCU_NAVSS0_RINGACC_0 | 235 |
| UDMA Device Name | UDMA Device ID |
|---|---|
| J721E_DEV_NAVSS0_UDMAP_0 | 212 |
| J721E_DEV_MCU_NAVSS0_UDMAP_0 | 236 |
| PSI-L Proxy Navigator Device Name | PSI-L Proxy Navigator Device ID |
|---|---|
| J721E_DEV_NAVSS512L_MAIN_0 | 199 |
| J721E_DEV_NAVSS_MCU_J7_MCU_0 | 232 |
Navigator Subsystem Ring Indices¶
This section describes valid Navigator Subsystem Ring Accelerator ring indices for each Navigator ring type. The ring index and type ID are used in some Ring Accelerator based TISCI messages.
Warning
Resources marked as reserved for use by DMSC cannot be assigned to a host within the RM Board Configuration resource assignment array. The RM Board Configuration is rejected if an overlap with a reserved resource is detected.
NAVSS0_RINGACC_0
| Ring Type | Ring Index Range |
|---|---|
| UDMAP_TX_UH | 0 to 3 |
| UDMAP_TX_H | 4 to 15 |
| UDMAP_TX | 16 to 139 |
| UDMAP_TX_EXT | 140 to 299 |
| UDMAP_RX_UH | 300 to 303 |
| UDMAP_RX_H | 304 to 315 |
| UDMAP_RX | 316 to 439 |
| GP | 440 to 973 |
| Monitor Index Range | |
|---|---|
| Ring Monitors | 0 to 31 |
MCU_NAVSS0_RINGACC_0
| Ring Type | Ring Index Range |
|---|---|
| UDMAP_TX_H | 0 to 1 |
| UDMAP_TX | 2 to 45 |
| UDMAP_TX (RESERVED BY SYSTEM FIRMWARE) | 46 to 47 |
| UDMAP_RX_H | 48 to 49 |
| UDMAP_RX | 50 to 92 |
| UDMAP_RX (RESERVED BY SYSTEM FIRMWARE) | 93 to 95 |
| GP | 96 to 251 |
| GP (RESERVED BY SYSTEM FIRMWARE) | 252 to 255 |
| Monitor Index Range | |
|---|---|
| Ring Monitors | 0 to 31 |
Navigator Subsystem Channel and Flow Indices¶
This section describes valid Navigator Subsystem UDMA transmit channel and receive channel indices for each Navigator UDMA channel type. The receive flow index range has no type information since it’s required for receive flows.
Warning
Resources marked as reserved for use by DMSC cannot be assigned to a host within the RM Board Configuration resource assignment array. The RM Board Configuration is rejected if an overlap with a reserved resource is detected.
NAVSS0_UDMAP_0
| Tx Channel Type | Tx Channel Index Range |
|---|---|
| TX_UHCHAN | 0 to 3 |
| TX_HCHAN | 4 to 15 |
| TX_CHAN | 16 to 139 |
| TX_ECHAN | 140 to 299 |
| Rx Channel Type | Rx Channel Index Range |
|---|---|
| RX_UHCHAN | 0 to 3 |
| RX_HCHAN | 4 to 15 |
| RX_CHAN | 16 to 139 |
| Rx Flow Type | Rx Flow Index Range |
|---|---|
| DEFAULT | 0 to 139 |
| CONFIGURABLE | 140 to 299 |
MCU_NAVSS0_UDMAP_0
| Tx Channel Type | Tx Channel Index Range |
|---|---|
| TX_HCHAN | 0 to 1 |
| TX_CHAN | 2 to 45 |
| TX_CHAN (RESERVED BY SYSTEM FIRMWARE) | 46 to 47 |
| Rx Channel Type | Rx Channel Index Range |
|---|---|
| RX_HCHAN | 0 to 1 |
| RX_CHAN | 2 to 44 |
| RX_CHAN (RESERVED BY SYSTEM FIRMWARE) | 45 to 47 |
| Rx Flow Type | Rx Flow Index Range |
|---|---|
| DEFAULT | 0 to 44 |
| DEFAULT (RESERVED BY SYSTEM FIRMWARE) | 45 to 47 |
| CONFIGURABLE | 48 to 95 |
Navigator Subsystem Virtual Interrupts¶
This section describes Navigator Subsystem virtual interrupts. The virtual interrupts are used in interrupt management based TISCI messages.
Warning
Resources marked as reserved for use by DMSC cannot be assigned to a host within the RM Board Configuration resource assignment array. The RM Board Configuration is rejected if an overlap with a reserved resource is detected.
| Interrupt Aggregator Name | Virtual Interrupt Range |
|---|---|
| J721E_DEV_NAVSS0_MODSS_INTAGGR_0 | 0 to 63 |
| J721E_DEV_NAVSS0_MODSS_INTAGGR_1 | 0 to 63 |
| J721E_DEV_NAVSS0_UDMASS_INTAGGR_0 (RESERVED BY SYSTEM FIRMWARE) | 0 to 37 |
| J721E_DEV_NAVSS0_UDMASS_INTAGGR_0 | 38 to 255 |
| J721E_DEV_MCU_NAVSS0_INTAGGR_0 (RESERVED BY SYSTEM FIRMWARE) | 0 to 7 |
| J721E_DEV_MCU_NAVSS0_INTAGGR_0 | 8 to 255 |
Navigator Subsystem Global Events¶
This section describes Navigator Subsystem global events. The global events are used in interrupt management based TISCI messages.
Warning
Resources marked as reserved for use by DMSC cannot be assigned to a host within the RM Board Configuration resource assignment array. The RM Board Configuration is rejected if an overlap with a reserved resource is detected.
| Global Event Name | Global Event Range |
|---|---|
| NAVSS0_UDMASS_INTAGGR_0 SEVT (RESERVED BY SYSTEM FIRMWARE) | 0 to 37 |
| NAVSS0_UDMASS_INTAGGR_0 SEVT | 38 to 4607 |
| MCU_NAVSS0_INTAGGR_0 SEVT (RESERVED BY SYSTEM FIRMWARE) | 16384 to 16391 |
| MCU_NAVSS0_INTAGGR_0 SEVT | 16392 to 17919 |
| NAVSS0_MODSS_INTAGGR_0 SEVT | 20480 to 21503 |
| NAVSS0_MODSS_INTAGGR_1 SEVT | 22528 to 23551 |
| NAVSS0_UDMASS_INTAGGR_0 MEVT | 32768 to 33279 |
| MCU_NAVSS0_INTAGGR_0 MEVT | 34816 to 34943 |
| NAVSS0_UDMASS_INTAGGR_0 GEVT | 36864 to 37375 |
| MCU_NAVSS0_INTAGGR_0 GEVT | 39936 to 40191 |
| NAVSS0_UDMAP_0 TRIGGER | 49152 to 50175 |
| MCU_NAVSS0_UDMAP_0 TRIGGER | 56320 to 56575 |
Navigator Subsystem PSI-L Source and Destination Thread IDs¶
This section describes valid Navigator Subsystem PSI-L source and destination thread IDs for each thread type. The thread IDs are used in the PSI-L based TISCI messages.
Warning
PSI-L threads marked as reserved for use by DMSC cannot be assigned be linked to another thread.
| Thread Type | Thread Range |
|---|---|
| udmap0_trstrm_tx | 0x8 to 0x8 |
| udmap0_cfgstrm_tx | 0x20 to 0x20 |
| navss_main_udmap0_tx | 0x1000 to 0x108b |
| navss_main_saul0_rx | 0x4000 to 0x4003 |
| navss_main_icssg0_rx | 0x4100 to 0x4104 |
| navss_main_icssg1_rx | 0x4200 to 0x4204 |
| navss_main_pdma_main_debug_ccmcu_rx | 0x4300 to 0x4302 |
| navss_main_pdma_main_debug_mainc66_rx | 0x4304 to 0x4305 |
| navss_main_pdma_main_mcasp_g0_rx | 0x4400 to 0x4402 |
| navss_main_pdma_main_aasrc_rx | 0x4404 to 0x440b |
| navss_main_pdma_main_mcasp_g1_rx | 0x4500 to 0x4508 |
| navss_main_pdma_main_misc_g0_rx | 0x4600 to 0x460a |
| navss_main_pdma_main_misc_g1_rx | 0x460c to 0x4616 |
| navss_main_pdma_main_misc_g2_rx | 0x4618 to 0x4622 |
| navss_main_pdma_main_misc_g3_rx | 0x4624 to 0x462e |
| navss_main_pdma_main_usart_g0_rx | 0x4700 to 0x4701 |
| navss_main_pdma_main_usart_g1_rx | 0x4702 to 0x4703 |
| navss_main_pdma_main_usart_g2_rx | 0x4704 to 0x4709 |
| navss_main_pdma_main_mcan_rx | 0x470c to 0x4729 |
| navss_main_msmc0_rx | 0x4800 to 0x481f |
| navss_main_vpac_tc0_cc_rx | 0x4820 to 0x483f |
| navss_main_vpac_tc1_cc_rx | 0x4840 to 0x487f |
| navss_main_dmpac_tc0_cc_rx | 0x4880 to 0x489f |
| navss_main_csi_rx | 0x4900 to 0x49ff |
| navss_main_cpsw9_rx | 0x4a00 to 0x4a00 |
| navss_mcu_udmap0_tx | 0x6000 to 0x602d |
| navss_mcu_udmap0_tx (Reserved by System Firmware) | 0x602e to 0x602f |
| navss_mcu_pdma_cpsw0_rx | 0x7000 to 0x7000 |
| navss_mcu_pdma_mcu0_rx | 0x7100 to 0x7106 |
| navss_mcu_pdma_mcu1_rx | 0x7200 to 0x7207 |
| navss_mcu_pdma_mcu2_rx | 0x7300 to 0x7303 |
| navss_mcu_pdma_adc_rx | 0x7400 to 0x7403 |
| navss_mcu_saul0_rx (Reserved by System Firmware) | 0x7500 to 0x7501 |
| navss_mcu_saul0_rx | 0x7502 to 0x7503 |
| navss_main_udmap0_rx | 0x9000 to 0x908b |
| navss_main_saul0_tx | 0xc000 to 0xc001 |
| navss_main_icssg0_tx | 0xc100 to 0xc108 |
| navss_main_icssg1_tx | 0xc200 to 0xc208 |
| navss_main_pdma_main_mcasp_g0_tx | 0xc400 to 0xc402 |
| navss_main_pdma_main_aasrc_tx | 0xc404 to 0xc40b |
| navss_main_pdma_main_mcasp_g1_tx | 0xc500 to 0xc508 |
| navss_main_pdma_main_misc_g0_tx | 0xc600 to 0xc60a |
| navss_main_pdma_main_misc_g1_tx | 0xc60c to 0xc616 |
| navss_main_pdma_main_misc_g2_tx | 0xc618 to 0xc622 |
| navss_main_pdma_main_misc_g3_tx | 0xc624 to 0xc62e |
| navss_main_pdma_main_usart_g0_tx | 0xc700 to 0xc701 |
| navss_main_pdma_main_usart_g1_tx | 0xc702 to 0xc703 |
| navss_main_pdma_main_usart_g2_tx | 0xc704 to 0xc709 |
| navss_main_pdma_main_mcan_tx | 0xc70c to 0xc729 |
| navss_main_msmc0_tx | 0xc800 to 0xc81f |
| navss_main_vpac_tc0_cc_tx | 0xc820 to 0xc83f |
| navss_main_vpac_tc1_cc_tx | 0xc840 to 0xc87f |
| navss_main_dmpac_tc0_cc_tx | 0xc880 to 0xc89f |
| navss_main_csi_tx | 0xc900 to 0xc9ff |
| navss_main_cpsw9_tx | 0xca00 to 0xca07 |
| navss_mcu_udmap0_rx | 0xe000 to 0xe02c |
| navss_mcu_udmap0_rx (Reserved by System Firmware) | 0xe02d to 0xe02f |
| navss_mcu_pdma_cpsw0_tx | 0xf000 to 0xf007 |
| navss_mcu_pdma_mcu0_tx | 0xf100 to 0xf106 |
| navss_mcu_pdma_mcu1_tx | 0xf200 to 0xf207 |
| navss_mcu_pdma_mcu2_tx | 0xf300 to 0xf303 |
| navss_mcu_pdma_adc_tx | 0xf400 to 0xf3ff |
| navss_mcu_saul0_tx (Reserved by System Firmware) | 0xf500 to 0xf500 |
| navss_mcu_saul0_tx | 0xf501 to 0xf501 |