Secure AP Command Interface¶
Introduction¶
Note
This document is applicable to HS devices only.
On K3 HS devices, the JTAG port is closed by default. At device run-time, access to JTAG port is controlled by System Firmware using knobs provided by the hardware. An external debugger should communicate with System Firmware running via Secure Access Point (Sec AP) in the DebugSS and unlock the required debug functionality.
This document lists
- the commands that can be used by the external debugger,
- the response to the commands from software running on DMSC
- the format of the payload for the commands and responses
- the communication protocol to be used for command and data transfer.
Data transfer protocol¶
- All data is transferred one word at a time. Each word is 32 bits in length.
Transmit protocol¶
- Write the number of (remaining) words to be transmitted in the 16 msb’s of the TX control register. The 16 lsb’s are to be set as zero.
- Write the word to be transmitted into the TX data register. The write will automatically assert Bit 0 of the TX control register.
- Wait for the target to read the data by polling until Bit 0 is cleared.
- Repeat steps (1), (2) and (3) until the complete data has been transferred.
Please note that one transmit transaction can contain theoritically contain a maximum of 65535 words. This can be further limited based on the command involved.
Receive Protocol¶
- When waiting to receive data, poll the RX control register until Bit 0 is set to 1. This indicates that data is available in the RX data register.
- The 16 lsb’s of the RX Control register indicate the number of words of the data that is yet to be read.
- Read 1 word of data from RX data register. This automatically clears Bit 0 of the RX control register.
- Repeat steps (1), (2) and (3) until required data is read.
Timeout during data transfer¶
System Firmware allows for a 360 ms delay between Words of a data transfer (read/write). If a timeout occurs, System Firmware will discard the active SEC AP command.
Commands¶
Each command is a combination of
- Command ID - 1 Word
- Optional payload - N words where N depends on the command.
Get UID¶
This command is used to get the unique ID for the SOC to be used in the debug certificate. See the below command.
The command ID is 0x80B5AE71. There is no payload associated with
this command.
The response returns a 32 byte value i.e. 8 Words. The MSB of Word[0] contains the MSB of UID.
| Word[0] | Word[1] | | Word[7] |
| B[0] B[1] B[2] B[3] | B[4] .. B[7] | ....| B[31] |
Open JTAG¶
This command is used to unlock the JTAG on a secure i.e. HS-SE device.
The command ID is 0x4968B2E9. This payload for this command is a
X.509 certificate with the debug extension and signed by one of the keys
trusted in the customer board configuration.
The certificate can be a maximum of 4 KB in size.
The fields of the certificate should be filled as specified in the @ref sec_x509_cert_doc_debug_extension.
This command has two responses.
- If JTAG unlock is successful, it returns
0xDEAD3A17. - If JTAG unlock is unsuccessful, it returns
0xDEADFA17.
If the command has failed, please review the settings in the certificate before resending.
System Firmware will perform the following checks on the certificate before attempting to apply the debug settings.
- The signature on the certificate is verified with the public key in the certificate.
- The public key used to sign the certificate must be present in the System Firmware Keystore.
- Various parameters in the certificate are within the specified range.
The command can be resent with a modified certificate if the JTAG unlock command has failed. However once JTAG unlock is successful, the same certificate needs to be used for subsequent unlock operations as well until the device is reset. This is because most of the registers controlling the debug operations can be written to only once after device reset. With a different certificate, it is likely that one of the debug registers need to be modified. The operation will fail as the register cannot be modified.