AM65X_SR2 PLL Defaults

PLL Defaults for AM65X_SR2 Device

This chapter provides information on the PLL defaults which the System firmware programs for AM65X_SR2 SoC.

This is what the system firmware programs after the PM board configuration is provided. The exact M and N values programmed are based on the crystal connected on the board. The crystal frequency is understood by the ROM from the BOOTPINS. This value is read by the System Firmware from the DEVSTAT register to determine which HFOSC is connected to the device

The System Firmware maintains a table of device clock frequency defaults at which the PLLs are programmed. This document is a reference that the users of System Firmware can look at to determine the default PLL configuration done during boot when PM board configuration message is sent.

Once the PM Init during board configuration is complete the bootloader or application can program individual clocks of individual modules to tweak the clocks based on the usecase which differ from the default. The APIs to refer to setting individual module clocks are TISCI_MSG_SET_FREQ, TISCI_MSG_QUERY_FREQ.

Use the below mentioned formula to calculate the output frequency of PLL HSDIVs:
  • HSDIV0 to HSDIV4: CLKOUT Freq * M2 / hsdiv
  • HSDIV5 to HSDIV9: CLKOUT Freq / hsdiv

Note

Any PLL configurations that are done before the PM board configuration is provided will be overwritten with the PLL defaults mentioned in the below tables. However, there are some PLLs that don’t get overwritten and the list can be found in the table PLL No Reinit Defaults for AM65X_SR2 Device

The following table gives the PLL configurations for the input crystal Frequency of 19.2 MHz:

PLL Name CLKOUT Freq (Hz) N+1 M Fractional M M2 HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) 400000000U 2 250 0 6 40 30 25 15
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) 250000000U 12 1250 0 8 10 10 15 6
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) 100000000U 12 1250 0 20 4 40 8 20
PER0 (ADPLLLJM_WRAP_MAIN_1) 960000000U 8 800 0 2 NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) 300000000U 8 750 0 6 8 18 9 4
DDR (ADPLLLJM_WRAP_MAIN_3) 333333333U 12 625 0 3 NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) 1155000000U 32 1925 0 1 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) 800000000U 3 250 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) 800000000U 3 250 0 2 NA NA NA NA

The following table gives the PLL configurations for the input crystal Frequency of 20.0 MHz:

PLL Name CLKOUT Freq (Hz) N+1 M Fractional M M2 HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) 400000000U 1 120 0 6 40 30 25 15
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) 250000000U 1 100 0 8 10 10 15 6
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) 100000000U 1 100 0 20 4 40 8 20
PER0 (ADPLLLJM_WRAP_MAIN_1) 960000000U 8 768 0 2 NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) 300000000U 8 720 0 6 8 18 9 4
DDR (ADPLLLJM_WRAP_MAIN_3) 333333333U 8 400 0 3 NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) 1155000000U 8 462 0 1 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) 800000000U 1 80 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) 800000000U 1 80 0 2 NA NA NA NA

The following table gives the PLL configurations for the input crystal Frequency of 24.0 MHz:

PLL Name CLKOUT Freq (Hz) N+1 M Fractional M M2 HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) 400000000U 1 100 0 6 40 30 25 15
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) 250000000U 3 250 0 8 10 10 15 6
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) 100000000U 12 1000 0 20 4 40 8 20
PER0 (ADPLLLJM_WRAP_MAIN_1) 960000000U 10 800 0 2 NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) 300000000U 10 750 0 6 8 18 9 4
DDR (ADPLLLJM_WRAP_MAIN_3) 333333333U 12 500 0 3 NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) 1155000000U 24 1155 0 1 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) 800000000U 3 200 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) 800000000U 3 200 0 2 NA NA NA NA

The following table gives the PLL configurations for the input crystal Frequency of 25.0 MHz:

PLL Name CLKOUT Freq (Hz) N+1 M Fractional M M2 HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) 400000000U 1 96 0 6 40 30 25 15
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) 250000000U 1 80 0 8 10 10 15 6
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) 100000000U 10 800 0 20 4 40 8 20
PER0 (ADPLLLJM_WRAP_MAIN_1) 960000000U 10 768 0 2 NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) 300000000U 10 720 0 6 8 18 9 4
DDR (ADPLLLJM_WRAP_MAIN_3) 333333333U 10 400 0 3 NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) 1155000000U 10 462 0 1 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) 800000000U 1 64 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) 800000000U 1 64 0 2 NA NA NA NA

The following table gives the PLL configurations for the input crystal Frequency of 26.0 MHz:

PLL Name CLKOUT Freq (Hz) N+1 M Fractional M M2 HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) 400000000U 13 1200 0 6 40 30 25 15
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) 250000000U 13 1000 0 8 10 10 15 6
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) 100000000U 13 1000 0 20 4 40 8 20
PER0 (ADPLLLJM_WRAP_MAIN_1) 960000000U 13 960 0 2 NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) 300000000U 13 900 0 6 8 18 9 4
DDR (ADPLLLJM_WRAP_MAIN_3) 333333333U 13 500 0 3 NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) 1155000000U 26 1155 0 1 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) 800000000U 13 800 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) 800000000U 13 800 0 2 NA NA NA NA

The following table gives the PLL configurations for the input crystal Frequency of 27.0 MHz:

PLL Name CLKOUT Freq (Hz) N+1 M Fractional M M2 HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) 400000000U 9 800 0 6 40 30 25 15
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) 250000000U 27 2000 0 8 10 10 15 6
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) 100000000U 27 2000 0 20 4 40 8 20
PER0 (ADPLLLJM_WRAP_MAIN_1) 960000000U 18 1280 0 2 NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) 300000000U 12 800 0 6 8 18 9 4
DDR (ADPLLLJM_WRAP_MAIN_3) 333333333U 27 1000 0 3 NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) 1155000000U 18 1540 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) 800000000U 27 1600 0 2 NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) 800000000U 27 1600 0 2 NA NA NA NA

PLL No Reinit Defaults for AM65X_SR2 Device

The following table gives details on PLLs (CLKOUT and HSDIVs) that are excluded from reinitializing when PM board configuration is received.

PLL Name CLKOUT HSDIV1 HSDIV2 HSDIV3 HSDIV4
MCU0 (ADPLLM_HSDIV_WRAP_MCU_0) – – – – –
CPSW (ADPLLM_HSDIV_WRAP_MCU_1) – – – – –
MAIN (ADPLLLJM_HSDIV_WRAP_MAIN_0) – – – – –
PER0 (ADPLLLJM_WRAP_MAIN_1) – NA NA NA NA
PER1 (ADPLLLJM_HSDIV_WRAP_MAIN_2) – – – – –
DDR (ADPLLLJM_WRAP_MAIN_3) – NA NA NA NA
DSS (ADPLLLJM_WRAP_MAIN_4) – NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_6) – NA NA NA NA
ARM (ADPLLM_WRAP_MAIN_7) – NA NA NA NA