Resource Management UDMAP TISCI Message Description

Introduction

This chapter provides information on usage of the RM UDMAP management TISCI message API parameters.

TISCI Message ID Message Name
0x1200 RESERVED, DO NOT (RE)USE
0x1201 RESERVED, DO NOT (RE)USE
0x1210 RESERVED, DO NOT (RE)USE
0x1211 RESERVED, DO NOT (RE)USE
0x1220 RESERVED, DO NOT (RE)USE
0x1221 RESERVED, DO NOT (RE)USE
0x1205 TISCI_MSG_RM_UDMAP_TX_CH_CFG
N/A TISCI_MSG_RM_UDMAP_TX_CH_CFG Response
0x1206 RESERVED, DO NOT (RE)USE
0x1207 TISCI_MSG_RM_UDMAP_TX_MULTI_CH_CFG
N/A TISCI_MSG_RM_UDMAP_TX_MULTI_CH_CFG Response
0x1215 TISCI_MSG_RM_UDMAP_RX_CH_CFG
N/A TISCI_MSG_RM_UDMAP_RX_CH_CFG Response
0x1216 RESERVED, DO NOT (RE)USE
0x1230 TISCI_MSG_RM_UDMAP_FLOW_CFG
N/A TISCI_MSG_RM_UDMAP_FLOW_CFG Response
0x1231 TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG
N/A TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG Response
0x1232 RESERVED, DO NOT (RE)USE
0x1233 RESERVED, DO NOT (RE)USE
0x1234 TISCI_MSG_RM_UDMAP_FLOW_DELEGATE
N/A TISCI_MSG_RM_UDMAP_FLOW_DELEGATE Response
0x1240 TISCI_MSG_RM_UDMAP_GCFG_CFG
N/A TISCI_MSG_RM_UDMAP_GCFG_CFG Response
0x1241 RESERVED, DO NOT (RE)USE

UDMAP Valid Parameters Field Usage

Some UDMAP TISCI message APIs make use of a valid_params bit field. Bits within the valid_params field define whether or not individual TISCI message parameters are valid. When a bit corresponding to a parameter is set (to 1) the parameter is considered valid and will be programmed into its corresponding register field, assuming validation of the parameter passes. When a valid_params bit is not set, i.e. a value of 0, the corresponding register field is read and used within the validation process of the request. The register field for a parameter is not programmed if the corresponding valid_params bit is not set.

TISCI_MSG_RM_UDMAP_TX_CH_CFG - UDMAP Transmit Channel Configure

UDMAP Transmit Channel Configure Request

The UDMAP tx channel cfg TISCI message API is used to configure SoC Navigator Subsystem UDMAP transmit channels. The API only allows configuration of a transmit channel by passing the tx channel index and the Navigator SoC device ID in which the channel is located. Only the non-real-time transmit channel registers are programmed as part of the channel configuration. The host is granted access to the transmit channel real-time registers via the SoC channelized firewalls based on the RM board configuration. The OS can access the channel real-time registers directly after transmit channel configuration is complete.

The UDMAP global invalid receive flow event and per transmit channel output event (OES) and error output event (EOES) registers are not programmed as part of the UDMAP tx channel cfg API. They’re programmed internally via the RM IRQ Set message.

The UDMAP tx channel cfg API can be used to configure transmit channels within any Navigator Subsystem UDMAP on the device.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_TX_CH_CFG          (0x1205U)

RM TISCI message to configure a Navigator Subsystem UDMAP transmit channel

UDMAP Transmit Channel Configure Message Parameters

struct tisci_msg_rm_udmap_tx_ch_cfg_req

Configures a Navigator Subsystem UDMAP transmit channel

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of tx channel configuration parameters. The tx channel configuration fields are not valid, and will not be used for ch configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_pause_on_err 1 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_atype 2 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_chan_type 3 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_fetch_size 4 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::txcq_qnum 5 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_priority 6 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_qos 7 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_orderid 8 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_sched_priority 9 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_filt_einfo 10 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_filt_pswords 11 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_supr_tdpkt 12 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_credit_count 13 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::fdepth 14 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_burst_size 15 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::tx_tdtype 16 - Valid bit for @ref tisci_msg_rm_udmap_tx_ch_cfg_req::extended_ch_type
nav_id u16 SoC device ID of Navigator Subsystem where tx channel is located
index u16 UDMAP transmit channel index.
tx_pause_on_err u8 UDMAP transmit channel pause on error configuration to be programmed into the tx_pause_on_err field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERROR_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERROR_ENABLED
tx_filt_einfo u8 UDMAP transmit channel extended packet information passing configuration to be programmed into the tx_filt_einfo field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_EINFO_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_EINFO_ENABLED
tx_filt_pswords u8 UDMAP transmit channel protocol specific word passing configuration to be programmed into the tx_filt_pswords field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_PSWORDS_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_PSWORDS_ENABLED
tx_atype u8 UDMAP transmit channel non Ring Accelerator access pointer interpretation configuration to be programmed into the tx_atype field of the channel’s TCHAN_TCFG register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_PHYS @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_INTERMEDIATE @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_VIRTUAL @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_NON_COHERENT
tx_chan_type u8 UDMAP transmit channel functional channel type and work passing mechanism configuration to be programmed into the tx_chan_type field of the channel’s TCHAN_TCFG register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_PACKET @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_DMA_REF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_DMA_VAL @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_BLOCK_REF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_BLOCK_VAL
tx_supr_tdpkt u8 UDMAP transmit channel teardown packet generation suppression configuration to be programmed into the tx_supr_tdpkt field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_SUPPRESS_TD_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_SUPPRESS_TD_ENABLED
tx_fetch_size u16 UDMAP transmit channel number of 32-bit descriptor words to fetch configuration to be programmed into the tx_fetch_size field of the channel’s TCHAN_TCFG register. The user must make sure to set the maximum word count that can pass through the channel for any allowed descriptor type. Cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_FETCH_SIZE_MAX
tx_credit_count u8 UDMAP transmit channel transfer request credit count configuration to be programmed into the count field of the TCHAN_TCREDIT register. Specifies how many credits for complete TRs are available. This field is only used when configuring a transmit channel of external type and cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_CREDIT_CNT_MAX
txcq_qnum u16 UDMAP transmit channel completion queue configuration to be programmed into the txcq_qnum field of the TCHAN_TCQ register. The specified completion queue must be assigned to the host, or a subordinate of the host, requesting configuration of the transmit channel.
tx_priority u8 UDMAP transmit channel transmit priority value to be programmed into the priority field of the channel’s TCHAN_TPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PRIORITY_MAX.
tx_qos u8 UDMAP transmit channel transmit qos value to be programmed into the qos field of the channel’s TCHAN_TPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_QOS_MAX.
tx_orderid u8 UDMAP transmit channel bus order id value to be programmed into the orderid field of the channel’s TCHAN_TPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ORDER_ID_MAX.
fdepth u16 UDMAP transmit channel FIFO depth configuration to be programmed into the fdepth field of the TCHAN_TFIFO_DEPTH register. Sets the number of Tx FIFO bytes which are allowed to be stored for the channel. This field is not supported for external channels. The TISCI message is rejected if a non-zero, valid, value is provided during external channel configuration. Check the UDMAP section of the TRM for restrictions regarding this parameter.
tx_sched_priority u8 UDMAP transmit channel tx scheduling priority configuration to be programmed into the priority field of the channel’s TCHAN_TST_SCHED register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_HIGH @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_MEDHIGH @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_MEDLOW @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_LOW
tx_burst_size u8 UDMAP transmit channel burst size configuration to be programmed into the tx_burst_size field of the TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_64_BYTES @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_128_BYTES @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_256_BYTES This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is not supported on some SoCs. On SoCs that do not support this field the input is quietly ignored even if the valid bit is set.
tx_tdtype u8 UDMAP transmit channel teardown type configuration to be programmed into the tdtype field of the TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_TDTYPE_IMMEDIATE @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_TDTYPE_WAIT This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_TDTYPE_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is not supported on some SoCs. On SoCs that do not support this field the input is quietly ignored even if the valid bit is set.
extended_ch_type u8 Extended Channel Type specific to BCDMA. A value of zero is the NULL extended_ch_type and applies UDMA and PKTDMA which dont have the MMR region layout that BCDMA does. BCDMA will have an extended_ch_type of value 1 assigned to block copy channels. So for BCDMA, supplying extended_ch_type value of 0 gets you access to the split TR TX channels. A value of 1 get you access to the block copy channels.

Configures the non-real-time registers of a Navigator Subsystem UDMAP transmit channel. The channel index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERR_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_FILT_EINFO_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_FILT_PSWORDS_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_CHAN_TYPE_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_SUPR_TDPKT_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_FETCH_SIZE_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_CREDIT_COUNT_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_CQ_QNUM_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PRIORITY_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_QOS_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ORDER_ID_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_FDEPTH_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIORITY_VALID is set in @ref tisci_msg_rm_udmap_tx_ch_cfg_req::valid_params.

UDMAP Transmit Channel Configuration Valid Parameters

The following table describes the valid bit mappings for the UDMAP transmit channel configure message optional parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_tx_ch_cfg_req Optional Parameter
0 tx_pause_on_err
1 tx_atype
2 tx_chan_type
3 tx_fetch_size
4 txcq_qnum
5 tx_priority
6 tx_qos
7 tx_orderid
8 tx_sched_priority
9 tx_filt_einfo
10 tx_filt_pswords
11 tx_supr_tdpkt
12 tx_credit_count
13 fdepth
14 tx_burst_size
15 tx_tdtype
16 extended_ch_type

UDMAP Transmit Channel Configure Response

The udmap tx channel cfg response message returns the result status of the processed udmap tx channel cfg message.

UDMAP Transmit Channel Configure Response Message Parameters

struct tisci_msg_rm_udmap_tx_ch_cfg_resp

Response to configuring a UDMAP transmit channel.

Parameter Type Description
hdr struct tisci_header Standard TISCI header

TISCI_MSG_RM_UDMAP_TX_MULTI_CH_CFG - UDMAP Multiple Transmit Channel Configure

UDMAP Multiple Transmit Channel Configure Request

The UDMAP tx multi channel cfg TISCI message API is used to configure multiple SoC Navigator Subsystem UDMAP transmit channels. The API only allows configuration of multiple transmit channels by passing the tx channel index and the Navigator SoC device ID in which the channel is located. Only the non-real-time transmit channel registers are programmed as part of the channel configuration. The host is granted access to the transmit channel real-time registers via the SoC channelized firewalls based on the RM board configuration. The OS can access the channel real-time registers directly after transmit channel configuration is complete.

The UDMAP global invalid receive flow event and per transmit channel output event (OES) and error output event (EOES) registers are not programmed as part of the UDMAP tx multi channel cfg API. They’re programmed internally via the RM IRQ Set message.

The UDMAP tx multi channel cfg API can be used to configure multiple transmit channels within any Navigator Subsystem UDMAP on the device.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_TX_MULTI_CH_CFG          (0x1207U)

RM TISCI message to configure multiple Navigator Subsystem UDMAP transmit channel

UDMAP Multiple Transmit Channel Configure Message Parameters

struct tisci_msg_rm_udmap_tx_multi_ch_cfg_req

Configures multiple Navigator Subsystem UDMAP transmit channels

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of tx channel configuration parameters. The tx channel configuration fields are not valid, and will not be used for ch configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_pause_on_err 1 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_atype 2 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_chan_type 3 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_fetch_size 4 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::start_txcq_qnum 5 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_priority 6 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_qos 7 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_orderid 8 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_sched_priority 9 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_filt_einfo 10 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_filt_pswords 11 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_supr_tdpkt 12 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_credit_count 13 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::fdepth 14 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_burst_size 15 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::tx_tdtype 16 - Valid bit for @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::extended_ch_type
nav_id u16 SoC device ID of Navigator Subsystem where tx channel is located
start_index u16 Start index of UDMAP transmit channel.
tx_pause_on_err u8 UDMAP transmit channel pause on error configuration to be programmed into the tx_pause_on_err field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERROR_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERROR_ENABLED
tx_filt_einfo u8 UDMAP transmit channel extended packet information passing configuration to be programmed into the tx_filt_einfo field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_EINFO_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_EINFO_ENABLED
tx_filt_pswords u8 UDMAP transmit channel protocol specific word passing configuration to be programmed into the tx_filt_pswords field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_PSWORDS_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_FILT_PSWORDS_ENABLED
tx_atype u8 UDMAP transmit channel non Ring Accelerator access pointer interpretation configuration to be programmed into the tx_atype field of the channel’s TCHAN_TCFG register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_PHYS @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_INTERMEDIATE @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_VIRTUAL @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_NON_COHERENT
tx_chan_type u8 UDMAP transmit channel functional channel type and work passing mechanism configuration to be programmed into the tx_chan_type field of the channel’s TCHAN_TCFG register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_PACKET @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_DMA_REF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_DMA_VAL @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_BLOCK_REF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_BLOCK_VAL
tx_supr_tdpkt u8 UDMAP transmit channel teardown packet generation suppression configuration to be programmed into the tx_supr_tdpkt field of the channel’s TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_SUPPRESS_TD_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_SUPPRESS_TD_ENABLED
tx_fetch_size u16 UDMAP transmit channel number of 32-bit descriptor words to fetch configuration to be programmed into the tx_fetch_size field of the channel’s TCHAN_TCFG register. The user must make sure to set the maximum word count that can pass through the channel for any allowed descriptor type. Cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_FETCH_SIZE_MAX
tx_credit_count u8 UDMAP transmit channel transfer request credit count configuration to be programmed into the count field of the TCHAN_TCREDIT register. Specifies how many credits for complete TRs are available. This field is only used when configuring a transmit channel of external type and cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_CREDIT_CNT_MAX
start_txcq_qnum u16 Starting index of UDMAP transmit channel completion queue configuration to be programmed into the txcq_qnum field of the TCHAN_TCQ register. The specified completion queue must be assigned to the host, or a subordinate of the host, requesting configuration of the transmit channel.
tx_priority u8 UDMAP transmit channel transmit priority value to be programmed into the priority field of the channel’s TCHAN_TPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PRIORITY_MAX.
tx_qos u8 UDMAP transmit channel transmit qos value to be programmed into the qos field of the channel’s TCHAN_TPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_QOS_MAX.
tx_orderid u8 UDMAP transmit channel bus order id value to be programmed into the orderid field of the channel’s TCHAN_TPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ORDER_ID_MAX.
fdepth u16 UDMAP transmit channel FIFO depth configuration to be programmed into the fdepth field of the TCHAN_TFIFO_DEPTH register. Sets the number of Tx FIFO bytes which are allowed to be stored for the channel. This field is not supported for external channels. The TISCI message is rejected if a non-zero, valid, value is provided during external channel configuration. Check the UDMAP section of the TRM for restrictions regarding this parameter.
tx_sched_priority u8 UDMAP transmit channel tx scheduling priority configuration to be programmed into the priority field of the channel’s TCHAN_TST_SCHED register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_HIGH @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_MEDHIGH @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_MEDLOW @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_LOW
tx_burst_size u8 UDMAP transmit channel burst size configuration to be programmed into the tx_burst_size field of the TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_64_BYTES @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_128_BYTES @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_256_BYTES This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is not supported on some SoCs. On SoCs that do not support this field the input is quietly ignored even if the valid bit is set.
tx_tdtype u8 UDMAP transmit channel teardown type configuration to be programmed into the tdtype field of the TCHAN_TCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_TDTYPE_IMMEDIATE @ref TISCI_MSG_VALUE_RM_UDMAP_TX_CH_TDTYPE_WAIT This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_TDTYPE_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is not supported on some SoCs. On SoCs that do not support this field the input is quietly ignored even if the valid bit is set.
extended_ch_type u8 Extended Channel Type specific to BCDMA. A value of zero is the NULL extended_ch_type and applies UDMA and PKTDMA which don’t have the MMR region layout that BCDMA does. BCDMA will have an extended_ch_type of value 1 assigned to block copy channels. So for BCDMA, supplying extended_ch_type value of 0 gets you access to the split TR TX channels. A value of 1 get you access to the block copy channels.
num_ch u8 The number of channels to which this particular configuration will be applied to.
ch_offset u8 Channel offset for each channel that needs to be configured. All channels that need to be configured should have a uniform offset.
txcq_offset u8 Offset for UDMAP transmit channel completion queue. All rings should have a uniform offset.

Configures the non-real-time registers of multiple Navigator Subsystem UDMAP transmit channels. The channels must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list. The same configuration will be applied to multiple channels. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERR_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_FILT_EINFO_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_FILT_PSWORDS_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_CHAN_TYPE_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_SUPR_TDPKT_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_FETCH_SIZE_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_CREDIT_COUNT_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_CQ_QNUM_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PRIORITY_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_QOS_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ORDER_ID_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TX_FDEPTH_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIORITY_VALID is set in @ref tisci_msg_rm_udmap_tx_multi_ch_cfg_req::valid_params.

UDMAP Multiple Transmit Channel Configuration Valid Parameters

The following table describes the valid bit mappings for the UDMAP multiple transmit channel configure message optional parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_tx_multi_ch_cfg_req Optional Parameter
0 tx_pause_on_err
1 tx_atype
2 tx_chan_type
3 tx_fetch_size
4 start_txcq_qnum
5 tx_priority
6 tx_qos
7 tx_orderid
8 tx_sched_priority
9 tx_filt_einfo
10 tx_filt_pswords
11 tx_supr_tdpkt
12 tx_credit_count
13 fdepth
14 tx_burst_size
15 tx_tdtype
16 extended_ch_type

UDMAP Multiple Transmit Channel Configure Response

The udmap tx multi channel cfg response message returns the result status of the processed udmap tx multi channel cfg message.

UDMAP Multiple Transmit Channel Configure Response Message Parameters

struct tisci_msg_rm_udmap_tx_multi_ch_cfg_resp

Response to configuring multiple UDMAP transmit channels.

Parameter Type Description
hdr struct tisci_header Standard TISCI header

Note

This API is not enabled for all SoCs. Use TISCI_MSG_QUERY_FW_CAPS to check if the TISCI_MSG_FLAG_FW_CAP_RM_UDMAP_MULTI_CH_CFG capability is supported on your SoC before using this message.

TISCI_MSG_RM_UDMAP_RX_CH_CFG - UDMAP Receive Channel Configure

UDMAP Receive Channel Configure

The UDMAP rx channel cfg TISCI message API is used to configure SoC Navigator Subsystem UDMAP receive channels. The API only allows configuration of a receive channel by passing the rx channel index and the Navigator SoC device ID in which the channel is located. Only the non-real-time receive channel registers are programmed as part of the channel configuration. The host is granted access to the receive channel real-time registers via the SoC channelized firewalls based on the RM board configuration. The OS can access the channel real-time registers directly after receive channel configuration is complete.

The UDMAP global invalid receive flow event and per receive channel output event (OES) and error output event (EOES) registers are not programmed as part of the UDMAP rx channel cfg API. They’re programmed internally via the RM IRQ Set message.

The UDMAP rx channel cfg API can be used to configure receive channels within any Navigator Subsystem UDMAP on the device.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_RX_CH_CFG          (0x1215U)

RM TISCI message to configure a Navigator Subsystem UDMAP receive channel

UDMAP Receive Channel Configure Message Parameters

struct tisci_msg_rm_udmap_rx_ch_cfg_req

Configures a Navigator Subsystem UDMAP receive channel

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of rx channel configuration parameters. The rx channel configuration fields are not valid, and will not be used for ch configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_pause_on_err 1 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_atype 2 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_chan_type 3 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_fetch_size 4 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rxcq_qnum 5 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_priority 6 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_qos 7 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_orderid 8 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_sched_priority 9 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::flowid_start 10 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::flowid_cnt 11 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_ignore_short 12 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_ignore_long 14 - Valid bit for @ref tisci_msg_rm_udmap_rx_ch_cfg_req::rx_burst_size
nav_id u16 SoC device ID of Navigator Subsystem where rx channel is located
index u16 UDMAP receive channel index.
rx_fetch_size u16 UDMAP receive channel number of 32-bit descriptor words to fetch configuration to be programmed into the rx_fetch_size field of the channel’s RCHAN_RCFG register. The user must make sure to set the maximum word count that can pass through the channel for any allowed descriptor type. Cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_FETCH_SIZE_MAX
rxcq_qnum u16 UDMAP receive channel completion queue configuration to be programmed into the rxcq_qnum field of the RCHAN_RCQ register. The specified completion queue must be assigned to the host, or a subordinate of the host, requesting configuration of the receive channel.
rx_priority u8 UDMAP receive channel receive priority value to be programmed into the priority field of the channel’s RCHAN_RPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PRIORITY_MAX.
rx_qos u8 UDMAP receive channel receive qos value to be programmed into the qos field of the channel’s RCHAN_RPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_QOS_MAX.
rx_orderid u8 UDMAP receive channel bus order id value to be programmed into the orderid field of the channel’s RCHAN_RPRI_CTRL register. This parameter cannot be greater than @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ORDER_ID_MAX.
rx_sched_priority u8 UDMAP receive channel rx scheduling priority configuration to be programmed into the priority field of the channel’s RCHAN_RST_SCHED register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_HIGH @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_MEDHIGH @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_MEDLOW @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIOR_LOW
flowid_start u16 UDMAP receive channel additional flows starting index configuration to program into the flow_start field of the RCHAN_RFLOW_RNG register. Specifies the starting index for flow IDs the receive channel is to make use of beyond the default flow. flowid_start and @ref flowid_cnt must be set as valid and configured together. The starting flow ID set by @ref flowid_cnt must be a flow index within the Navigator Subsystem’s subset of flows beyond the default flows statically mapped to receive channels. The additional flows must be assigned to the host, or a subordinate of the host, requesting configuration of the receive channel.
flowid_cnt u16 UDMAP receive channel additional flows count configuration to program into the flowid_cnt field of the RCHAN_RFLOW_RNG register. This field specifies how many flow IDs are in the additional contiguous range of legal flow IDs for the channel. @ref flowid_start and flowid_cnt must be set as valid and configured together. Disabling the valid_params field bit for flowid_cnt indicates no flow IDs other than the default are to be allocated and used by the receive channel. @ref flowid_start plus flowid_cnt cannot be greater than the number of receive flows in the receive channel’s Navigator Subsystem. The additional flows must be assigned to the host, or a subordinate of the host, requesting configuration of the receive channel.
rx_pause_on_err u8 UDMAP receive channel pause on error configuration to be programmed into the rx_pause_on_err field of the channel’s RCHAN_RCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERROR_DISABLED @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERROR_ENABLED
rx_atype u8 UDMAP receive channel non Ring Accelerator access pointer interpretation configuration to be programmed into the rx_atype field of the channel’s RCHAN_RCFG register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_PHYS @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_INTERMEDIATE @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_VIRTUAL @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_NON_COHERENT
rx_chan_type u8 UDMAP receive channel functional channel type and work passing mechanism configuration to be programmed into the rx_chan_type field of the channel’s RCHAN_RCFG register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_PACKET @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_PACKET_SINGLE_BUF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_DMA_REF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_DMA_VAL @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_BLOCK_REF @ref TISCI_MSG_VALUE_RM_UDMAP_CH_TYPE_3P_BLOCK_VAL
rx_ignore_short u8 UDMAP receive channel short packet treatment configuration to be programmed into the rx_ignore_short field of the RCHAN_RCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_RX_CH_PACKET_EXCEPTION @ref TISCI_MSG_VALUE_RM_UDMAP_RX_CH_PACKET_IGNORED
rx_ignore_long u8 UDMAP receive channel long packet treatment configuration to be programmed into the rx_ignore_long field of the RCHAN_RCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_RX_CH_PACKET_EXCEPTION @ref TISCI_MSG_VALUE_RM_UDMAP_RX_CH_PACKET_IGNORED
rx_burst_size u8 UDMAP receive channel burst size configuration to be programmed into the rx_burst_size field of the RCHAN_RCFG register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_64_BYTES @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_128_BYTES @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_256_BYTES This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_BURST_SIZE_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is not supported on some SoCs. On SoCs that do not support this field the input is quietly ignored even if the valid bit is set.

Configures the non-real-time registers of a Navigator Subsystem UDMAP receive channel. The channel index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_FETCH_SIZE_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_CQ_QNUM_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PRIORITY_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_QOS_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ORDER_ID_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_SCHED_PRIORITY_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_RX_FLOWID_START_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_RX_FLOWID_CNT_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_PAUSE_ON_ERR_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_ATYPE_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_CHAN_TYPE_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_RX_IGNORE_SHORT_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_CH_RX_IGNORE_LONG_VALID is set in @ref tisci_msg_rm_udmap_rx_ch_cfg_req::valid_params.

UDMAP Receive Channel Configuration Valid Parameters

The following table describes the valid bit mappings for the UDMAP receive channel configure message optional parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_rx_ch_cfg_req Optional Parameter
0 rx_pause_on_err
1 rx_atype
2 rx_chan_type
3 rx_fetch_size
4 rxcq_qnum
5 rx_priority
6 rx_qos
7 rx_orderid
8 rx_sched_priority
9 flowid_start
10 flowid_cnt
11 rx_ignore_short
12 rx_ignore_long
14 rx_burst_size

UDMAP Receive Channel Configure Response

The udmap rx channel cfg response message returns the result status of the processed udmap rx channel cfg message.

UDMAP Receive Channel Configure Response Message Parameters

struct tisci_msg_rm_udmap_rx_ch_cfg_resp

Response to configuring a UDMAP receive channel.

Parameter Type Description
hdr struct tisci_header Standard TISCI header

TISCI_MSG_RM_UDMAP_FLOW_CFG - UDMAP Receive Flow Configure

UDMAP Receive Flow Configure Request

The UDMAP flow cfg TISCI message API is used to configure a SoC Navigator Subsystem UDMAP receive flow’s standard, non-size threshold registers. The flow index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.

It’s the user’s responsibility to make sure any receive channels using the flow are disabled when changing the receive flow configuration. Otherwise, unknown operation may occur.

The UDMAP global invalid receive flow event register is not programmed as part of the UDMAP flow cfg API. It is programmed internally via the RM IRQ Set message.

The UDMAP flow cfg API can be used to configure receive flows within any Navigator Subsystem UDMAP on the device.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_FLOW_CFG          (0x1230U)

RM TISCI message to configure a Navigator Subsystem UDMAP receive flow

UDMAP Receive Flow Configure Message Parameters

struct tisci_msg_rm_udmap_flow_cfg_req

Configures a Navigator Subsystem UDMAP receive flow

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of rx flow configuration parameters. The rx flow configuration fields are not valid, and will not be used for flow configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_einfo_present 1 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_psinfo_present 2 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_error_handling 3 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_desc_type 4 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_sop_offset 5 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_dest_qnum 6 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_src_tag_hi 7 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_src_tag_lo 8 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_hi 9 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_lo 10 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_src_tag_hi_sel 11 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_src_tag_lo_sel 12 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_hi_sel 13 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_dest_tag_lo_sel 14 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_fdq0_sz0_qnum 15 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_fdq1_qnum 16 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_fdq2_qnum 17 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_fdq3_qnum 18 - Valid bit for @ref tisci_msg_rm_udmap_flow_cfg_req::rx_ps_location
nav_id u16 SoC device ID of Navigator Subsystem from which the receive flow is allocated
flow_index u16 UDMAP receive flow index for non-optional configuration.
rx_einfo_present u8 UDMAP receive flow extended packet info present configuration to be programmed into the rx_einfo_present field of the flow’s RFLOW_RFA register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_EINFO_NOT_PRESENT @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_EINFO_PRESENT
rx_psinfo_present u8 UDMAP receive flow PS words present configuration to be programmed into the rx_psinfo_present field of the flow’s RFLOW_RFA register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_PSINFO_NOT_PRESENT @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_PSINFO_PRESENT
rx_error_handling u8 UDMAP receive flow error handling configuration to be programmed into the rx_error_handling field of the flow’s RFLOW_RFA register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_ERR_DROP @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_ERR_RETRY
rx_desc_type u8 UDMAP receive flow descriptor type configuration to be programmed into the rx_desc_type field field of the flow’s RFLOW_RFA register. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DESC_HOST @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DESC_MONO
rx_sop_offset u16 UDMAP receive flow start of packet offset configuration to be programmed into the rx_sop_offset field of the RFLOW_RFA register. See the UDMAP section of the TRM for more information on this setting. Valid values for this field are 0-255 bytes. The allocation request will be NACK’d if specified offset is greater than @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SOP_MAX.
rx_dest_qnum u16 UDMAP receive flow destination queue configuration to be programmed into the rx_dest_qnum field of the flow’s RFLOW_RFA register. The specified destination queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
rx_src_tag_hi u8 UDMAP receive flow source tag high byte constant configuration to be programmed into the rx_src_tag_hi field of the flow’s RFLOW_RFB register. See the UDMAP section of the TRM for more information on this setting.
rx_src_tag_lo u8 UDMAP receive flow source tag low byte constant configuration to be programmed into the rx_src_tag_lo field of the flow’s RFLOW_RFB register. See the UDMAP section of the TRM for more information on this setting.
rx_dest_tag_hi u8 UDMAP receive flow destination tag high byte constant configuration to be programmed into the rx_dest_tag_hi field of the flow’s RFLOW_RFB register. See the UDMAP section of the TRM for more information on this setting.
rx_dest_tag_lo u8 UDMAP receive flow destination tag low byte constant configuration to be programmed into the rx_dest_tag_lo field of the flow’s RFLOW_RFB register. See the UDMAP section of the TRM for more information on this setting.
rx_src_tag_hi_sel u8 UDMAP receive flow source tag high byte selector configuration to be programmed into the rx_src_tag_hi_sel field of the RFLOW_RFC register. See the UDMAP section of the TRM for more information on this setting. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_NONE @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_CFG_TAG @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_FLOW_ID @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_SRC_TAG
rx_src_tag_lo_sel u8 UDMAP receive flow source tag low byte selector configuration to be programmed into the rx_src_tag_lo_sel field of the RFLOW_RFC register. See the UDMAP section of the TRM for more information on this setting. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_NONE @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_CFG_TAG @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_FLOW_ID @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SRC_SELECT_SRC_TAG
rx_dest_tag_hi_sel u8 UDMAP receive flow destination tag high byte selector configuration to be programmed into the rx_dest_tag_hi_sel field of the RFLOW_RFC register. See the UDMAP section of the TRM for more information on this setting. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_NONE @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_CFG_TAG @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_FLOW_ID @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_DEST_TAG_LO @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_DEST_TAG_HI
rx_dest_tag_lo_sel u8 UDMAP receive flow destination tag low byte selector configuration to be programmed into the rx_dest_tag_lo_sel field of the RFLOW_RFC register. See the UDMAP section of the TRM for more information on this setting. Can be set to @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_NONE @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_CFG_TAG @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_FLOW_ID @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_DEST_TAG_LO @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_DEST_SELECT_DEST_TAG_HI
rx_fdq0_sz0_qnum u16 UDMAP receive flow free descriptor queue 0 configuration to be programmed into the rx_fdq0_sz0_qnum field of the flow’s RFLOW_RFD register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
rx_fdq1_qnum u16 UDMAP receive flow free descriptor queue 1 configuration to be programmed into the rx_fdq1_qnum field of the flow’s RFLOW_RFD register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
rx_fdq2_qnum u16 UDMAP receive flow free descriptor queue 2 configuration to be programmed into the rx_fdq2_qnum field of the flow’s RFLOW_RFE register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
rx_fdq3_qnum u16 UDMAP receive flow free descriptor queue 3 configuration to be programmed into the rx_fdq3_qnum field of the flow’s RFLOW_RFE register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, requesting allocation and configuration of the receive flow.
rx_ps_location u8 UDMAP receive flow PS words location configuration to be programmed into the rx_ps_location field of the flow’s RFLOW_RFA register. Can be set to: @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_PS_END_PD @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_PS_BEGIN_DB

Configures a Navigator Subsystem UDMAP receive flow’s registers. Configuration does not include the flow registers which handle size-based free descriptor queue routing. The @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req message is used to configure register fields related to size based free descriptor queues. The flow index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list. It’s the user’s responsibility to make sure any receive channels using the flow are disabled when changing the receive flow configuration. Otherwise, unknown operation may occur. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_EINFO_PRESENT_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_PSINFO_PRESENT_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_ERROR_HANDLING_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DESC_TYPE_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SOP_OFFSET_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DEST_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SRC_TAG_HI_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SRC_TAG_LO_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DEST_TAG_HI_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DEST_TAG_LO_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SRC_TAG_HI_SEL_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SRC_TAG_LO_SEL_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DEST_TAG_HI_SEL_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DEST_TAG_LO_SEL_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ0_SZ0_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ1_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ2_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ3_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_PS_LOCATION_VALID is set in @ref tisci_msg_rm_udmap_flow_cfg_req::valid_params.

UDMAP Receive Flow Configure Valid Parameters

The following table describes the valid bit mappings for the UDMAP receive flow configure message parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_flow_cfg_req Parameter
0 rx_einfo_present
1 rx_psinfo_present
2 rx_error_handling
3 rx_desc_type
4 rx_sop_offset
5 rx_dest_qnum
6 rx_src_tag_hi
7 rx_src_tag_lo
8 rx_dest_tag_hi
9 rx_dest_tag_lo
10 rx_src_tag_hi_sel
11 rx_src_tag_lo_sel
12 rx_dest_tag_hi_sel
13 rx_dest_tag_lo_sel
14 rx_fdq0_sz0_qnum
15 rx_fdq1_sz0_qnum
16 rx_fdq2_sz0_qnum
17 rx_fdq3_sz0_qnum
18 rx_ps_location

UDMAP Receive Flow Configure Response

The udmap flow cfg response message returns the result status of the processed udmap flow cfg message.

UDMAP Receive Flow Configure Response Message Parameters

struct tisci_msg_rm_udmap_flow_cfg_resp

Response to configuring a Navigator Subsystem UDMAP receive flow

Parameter Type Description
hdr struct tisci_header Standard TISCI header

TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG - UDMAP Receive Flow Size Threshold Configure

UDMAP Receive Flow Size Threshold Configure Request

The UDMAP flow size threshold cfg TISCI message API is used to configure the size-based free descriptor queue routing registers for flow. The flow index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.

It’s the user’s responsibility to make sure any receive channels using the flow are disabled when changing the receive flow configuration. Otherwise, unknown operation may occur.

The UDMAP flow size threshold cfg API can be used to configure receive flows within any Navigator Subsystem UDMAP on the device.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_FLOW_SIZE_THRESH_CFG          (0x1231U)

RM TISCI message to configure a Navigator Subsystem UDMAP receive flow’s optional, size based free descriptor queue registers

UDMAP Receive Flow Size Threshold Configure Message Parameters

struct tisci_msg_rm_udmap_flow_size_thresh_cfg_req

Configures a Navigator Subsystem UDMAP receive flow’s size threshold fields.

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of rx flow configuration parameters. The rx flow configuration fields are not valid, and will not be used for flow configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_size_thresh0 1 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_size_thresh1 2 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_size_thresh2 3 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_fdq0_sz1_qnum 4 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_fdq0_sz2_qnum 5 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_fdq0_sz3_qnum 6 - Valid bit for @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::rx_size_thresh_en
nav_id u16 SoC device ID of Navigator Subsystem from which the receive flow is allocated
flow_index u16 UDMAP receive flow index for optional configuration.
rx_size_thresh0 u16 UDMAP receive flow packet size threshold 0 configuration to be programmed into the rx_size_thresh0 field of the flow’s RFLOW_RFF register. The value must be provided in 32-byte units due to a 5-bit left shift performed by the hardware prior to comparison to packet size. See the UDMAP section of the TRM for more information on this setting and the shift on comparison.
rx_size_thresh1 u16 UDMAP receive flow packet size threshold 1 configuration to be programmed into the rx_size_thresh1 field of the flow’s RFLOW_RFF register. The value must be provided in 32-byte units due to a 5-bit left shift performed by the hardware prior to comparison to packet size. See the UDMAP section of the TRM for more information on this setting and the shift on comparison.
rx_size_thresh2 u16 UDMAP receive flow packet size threshold 2 configuration to be programmed into the rx_size_thresh2 field of the flow’s RFLOW_RFG register. The value must be provided in 32-byte units due to a 5-bit left shift performed by the hardware prior to comparison to packet size. See the UDMAP section of the TRM for more information on this setting and the shift on comparison.
rx_fdq0_sz1_qnum u16 UDMAP receive flow free descriptor queue for size threshold 1 configuration to be programmed into the rx_fdq0_sz1_qnum field of the flow’s RFLOW_RFG register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, who owns the receive flow index and who is making the optional configuration request.
rx_fdq0_sz2_qnum u16 UDMAP receive flow free descriptor queue for size threshold 2 configuration to be programmed into the rx_fdq0_sz2_qnum field of the flow’s RFLOW_RFH register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, who owns the receive flow index and who is making the optional configuration request.
rx_fdq0_sz3_qnum u16 UDMAP receive flow free descriptor queue for size threshold 3 configuration to be programmed into the rx_fdq0_sz3_qnum field of the flow’s RFLOW_RFH register. See the UDMAP section of the TRM for more information on this setting. The specified free queue must be valid within the Navigator Subsystem and must be owned by the host, or a subordinate of the host, who owns the receive flow index and who is making the optional configuration request.
rx_size_thresh_en u8 UDMAP receive flow packet size based free buffer queue enable configuration to be programmed into the rx_size_thresh_en field of the RFLOW_RFC register. See the UDMAP section of the TRM for more information on this setting. This parameter can be no greater than @ref TISCI_MSG_VALUE_RM_UDMAP_RX_FLOW_SIZE_THRESH_MAX

Configures a Navigator Subsystem UDMAP receive flow’s size threshold fields The flow index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list. It’s the user’s responsibility to make sure any receive channels using the flow are disabled when changing the receive flow configuration. Otherwise, unknown operation may occur. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SIZE_THRESH0_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SIZE_THRESH1_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SIZE_THRESH2_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ0_SZ1_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ0_SZ2_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_FDQ0_SZ3_QNUM_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_SIZE_THRESH_EN_VALID is set in @ref tisci_msg_rm_udmap_flow_size_thresh_cfg_req::valid_params.

UDMAP Receive Flow Size Threshold Configure Valid Parameters

The following table describes the valid bit mappings for the UDMAP receive flow size threshold configure message parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_flow_size_thresh_cfg_req Parameter
0 rx_size_thresh0
1 rx_size_thresh1
2 rx_size_thresh2
3 rx_fdq0_sz1_qnum
4 rx_fdq0_sz2_qnum
5 rx_fdq0_sz3_qnum
6 rx_size_thresh_en

UDMAP Receive Flow Size Threshold Configure Response

The udmap flow size threshold cfg response message returns the result status of the processed udmap flow size threshold cfg message.

UDMAP Receive Flow Size Threshold Configure Response Message Parameters

struct tisci_msg_rm_udmap_flow_size_thresh_cfg_resp

Response to configuring a Navigator Subsystem UDMAP receive flow’s size threshold fields.

Parameter Type Description
hdr struct tisci_header Standard TISCI header

TISCI_MSG_RM_UDMAP_FLOW_DELEGATE - UDMAP Flow Delegate

UDMAP Flow Delegate Request

The UDMAP flow delegate TISCI message API is used by a host to delegate configuration of an owned, according to the RM board configuration, common DMA flow to another host. After delegation the host owning the flow and the delegated host are allowed to configure the flow via the flow configuration TISCI messages. The delegation can be cleared by the host who owns the flow by setting the clear parameter of the flow delegate message.

The flow index set for delegation must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_FLOW_DELEGATE          (0x1234U)

RM TISCI message to delegate a DMA flow to another host for configuration

UDMAP Flow Delegate Message Parameters

struct tisci_msg_rm_udmap_flow_delegate_req

Delegates the specified flow to another host for configuration. Only the original owner of the flow, as specified in the RM board configuration resource entries, can delegate an additional host as able to configure the flow. A flow’s delegation can be cleared by the original owner of the flow using the clear parameter.

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of flow delegation parameters. The flow delegation fields are not valid, and will not be used, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_flow_delegate_req::delegated_host 1 - Valid bit for @ref tisci_msg_rm_udmap_flow_delegate_req::clear
dev_id u16 SoC device ID of DMA in which the common flow exists.
flow_index u16 DMA common flow being delegated for configuration.
delegated_host u8 The host delegated configuration access to the flow. The host must be a valid host within the SoC. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DELEGATE_HOST_VALID is set in @ref tisci_msg_rm_udmap_flow_delegate_req::valid_params.
clear u8 Clears the flow delegation when enabled. Set this parameter to @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DELEGATE_CLEAR. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_FLOW_DELEGATE_CLEAR_VALID is set in @ref tisci_msg_rm_udmap_flow_delegate_req::valid_params.

UDMAP Flow Delegate Valid Parameters

The following table describes the valid bit mappings for the UDMAP flow delegate message parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_flow_delegate_req Parameter
0 delegated_host
1 clear

UDMAP Flow Delegate Response

The udmap flow delegate response message returns the result status of the processed udmap flow delegate message.

UDMAP Flow Delegate Response Message Parameters

struct tisci_msg_rm_udmap_flow_delegate_resp

Response to delegating a flow to another host for configuration.

Parameter Type Description
hdr struct tisci_header Standard TISCI header

TISCI_MSG_RM_UDMAP_GCFG_CFG - UDMAP Global Configuration Configure

UDMAP Global Configuration Configure Request

The udmap_gcfg_cfg TISCI message API is used to configure non-real-time registers in the UDMAP subsystem’s global configuration region. The host, or a supervisor of the host, who owns the global configuration region must be the requesting host. The API allows configuration of the global configuration region by passing the Navigator SoC device ID of the UDMAP subsystem in which the region is located.

Usage

Message Type Normal
Secure Queue Only? No

TISCI Message ID

TISCI_MSG_RM_UDMAP_GCFG_CFG          (0x1240U)

RM TISCI message to configure a Navigator Subsystem UDMAP global configuration

UDMAP Global Configuration Configure Message Parameters

struct tisci_msg_rm_udmap_gcfg_cfg_req

Configures a Navigator Subsystem UDMAP global configuration region. Configures the non-real-time registers of a Navigator Subsystem UDMAP global configuration region. The GCFG region being programmed must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment array. Individual fields for registers specified as valid are not checked for correctness. It is the application’s responsibility to verify if the register fields are being set according to the device specification.

Parameter Type Description
hdr struct tisci_header Standard TISCI header
valid_params u32 Bitfield defining validity of global configuration parameters. The configuration fields are not valid, and will not be used for global configuration, if their corresponding valid bit is zero. Valid bit usage: 0 - Valid bit for @ref tisci_msg_rm_udmap_gcfg_cfg_req::perf_ctrl 1 - Valid bit for @ref tisci_msg_rm_udmap_gcfg_cfg_req::emu_ctrl 2 - Valid bit for @ref tisci_msg_rm_udmap_gcfg_cfg_req::psil_to 3 - Valid bit for @ref tisci_msg_rm_udmap_gcfg_cfg_req::rflowfwstat
nav_id u16 SoC device ID of Navigator Subsystem where global configuration is located
perf_ctrl u32 Configures the performance control register. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_GCFG_PERF_CTRL_VALID is set in @ref tisci_msg_rm_udmap_gcfg_cfg_req::valid_params.
emu_ctrl u32 Configures the emulation control register. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_GCFG_EMU_CTRL_VALID is set in @ref tisci_msg_rm_udmap_gcfg_cfg_req::valid_params.
psil_to u32 Configures the PSI-L proxy timeout register. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_GCFG_PSIL_TO_VALID is set in @ref tisci_msg_rm_udmap_gcfg_cfg_req::valid_params.
rflowfwstat u32 Writes the rx flow ID firewall status register. This field is only valid if @ref TISCI_MSG_VALUE_RM_UDMAP_GCFG_RFLOWFWSTAT_VALID is set in @ref tisci_msg_rm_udmap_gcfg_cfg_req::valid_params.

UDMAP Global Configuration Configure Valid Parameters

The following table describes the valid bit mappings for the UDMAP global configuration configure parameters:

valid_params Bit Corresponding tisci_msg_rm_udmap_gcfg_cfg_req Parameter
0 perf_ctrl_timeout_cnt
1 emu_ctrl_soft
2 emu_ctrl_free
3 psil_to_tout
4 psil_to_tout_cnt
5 utc_chan_start
6 rflowfwstat_pend

UDMAP Global Configuration Configure Response

The udmap_gcfg_cfg_response message returns the result status of the processed udmap_gcfg_cfg message.

UDMAP Global Configuration Configure Response Message Parameters

struct tisci_msg_rm_udmap_gcfg_cfg_resp

Response to configuring UDMAP global configuration.

Parameter Type Description
hdr struct tisci_header Standard TISCI header