Cryptographic Services¶
Table of Contents
Introduction¶
The Cryptographic services allow tifs client to encrypt/decrypt data blobs using one of AES-ECB, AES-CBC or AES-GCM operations.
Functional Goals¶
Cryptographic Service System provides the following functionality:
- API to encrypt a data blob.
 - API to decrypt a data blob.
 
Design¶
The to-be encrypted/decrypted blob must be preceded by a context. The blob starts immediately after the context blob ends. The context blob contains information like the algorithm to use, key, key size, iv, data length etc.
The response contains calculated tag when the mode is AES-GCM and operation type is ‘encryption’.
The context also contains a revision field that denotes the context version. The revision field has been added to support different variations of the service in the future. Currently, just one version is supported which is version 0.
The structure of the context v0 is given below.
struct csp_aes_ctx_v0 {
  uint8_t     mode;
  uint8_t     key_size;
  uint8_t     ctr_width;
  uint8_t     resv0;
  uint64_t    data_len;
  uint64_t    dest_addr;
  uint32_t    key[8];
  uint32_t    iv[4];
  uint32_t    tag[4];
}