Mailbox IPC¶
Introduction to mailbox ipc channels¶
This chapter provides information about various mailbox ipc channels configured by tifs. Every mailbox ipc channel can be used for unidirectional communication between two cores. Every mailbox ipc channel is comprised of a mailbox fifo and a memory segment. While the memory segment is used for storing the actual TISCI messages the mailbox fifo is used for storing 32-bit pointers to the messages.
Note:
- Every mailbox fifo has space for 4 32-bit message pointers which means that one channel can hold at-most 4 tisci messages at a time.
 - Every mailbox ipc memory segment has space for 5 tisci messages.
 - The size of every message slot is 64 bytes though all are not used.