J7200 Proxy Device Descriptions¶
Introduction¶
This chapter provides information on the Proxy devices in the J7200 SoC. Some System Firmware TISCI messages take device specific inputs. This chapter provides information on the valid values for Proxy TISCI message parameters.
Proxy Device IDs¶
Some System Firmware TISCI message APIs require the Proxy device ID be provided as part of the request. Based on J7200 Device IDs these are the valid Proxy device IDs.
| Proxy Device Name | Proxy Device ID |
|---|---|
| J7200_DEV_NAVSS0_PROXY_0 | 210 |
| J7200_DEV_MCU_NAVSS0_PROXY0 | 234 |
Proxy Indices¶
This section describes Proxy indices. The proxy index is used in some Proxy based TISCI messages.
Warning
Resources marked as reserved for use by DMSC cannot be assigned to a host within the RM Board Configuration resource assignment array. The RM Board Configuration is rejected if an overlap with a reserved resource is detected.
| Proxy Name | Proxy Range |
|---|---|
| J7200_DEV_NAVSS0_PROXY_0 | 0 to 63 |
| J7200_DEV_MCU_NAVSS0_PROXY0 (RESERVED BY SYSTEM FIRMWARE) | 0 to 0 |
| J7200_DEV_MCU_NAVSS0_PROXY0 | 1 to 63 |