OTP Keywriter TISCI Description¶
This chapter provides information on TISCI message for programming customer keys into eFuse array on K3 devices.
| TISCI Message ID | Message Name |
|---|---|
| 0x9031 | TISCI_MSG_KEY_WRITER |
This document must be read alongside Key Writer
API Description¶
TISCI_MSG_KEY_WRITER - Key writer¶
Usage¶
| Message Type | Secure |
| Secure Queue Only? | Yes |
TISCI Message ID¶
TISCI_MSG_KEY_WRITER (0x9031U)
struct tisci_msg_keywriter_req
Request message for keywriter
| Parameter | Type | Description |
|---|---|---|
| hdr | struct tisci_header | standard TISCI header |
| image_addr_lo | u32 | Lower 32 bit address (in LE format) of the certificate |
| image_addr_hi | u32 | Higher 32 bit address (in LE format) of the certificate |
| key_prog_mask | u32 | Reserved for future use |
The address of the certificate containing customer key information is given as an input to the API.
struct tisci_msg_keywriter_resp
Response message for keywriter
| Parameter | Type | Description |
|---|---|---|
| hdr | struct tisci_header | standard TISCI header |
| debug_response | u32 | debug code for success/failure |
A debug_response of 0x0 means the key programming was successful, other
response codes indicate the point of failure, which can be referred from PDK documentation
for OTP Keywriter.
OTP KEY WRITER ERROR CODES¶
Note
For example a debug_response 0x00000004 would mean that (KEYWR_ERR_DECRYPT_BMPKH) there was an error in decrypting BMPKH extension field
enum keywriter_error_codes
OTP Keywriter error code bit indices
| Enum | Value | Description |
|---|---|---|
| KEYWR_ERR_DECRYPT_AES256_KEY | 0 | Error in Decrypting AES256 key randomly generated by customer |
| KEYWR_ERR_DECRYPT_BMEK | 1 | Error in Decrypting BMEK extension field |
| KEYWR_ERR_DECRYPT_BMPKH | 2 | Error in Decrypting BMPKH extension field |
| KEYWR_ERR_DECRYPT_SMEK | 3 | Error in Decrypting SMEK extension field |
| KEYWR_ERR_DECRYPT_SMPKH | 4 | Error in Decrypting SMPKH extension field |
| KEYWR_ERR_INTERAL_OP | 5 | Internal Operation Error |
| KEYWR_ERR_INVALID_EXT_COUNT | 6 | Invalid extension count in x509 certificate. Either SMPKH, SMEK pair or BMPKH, BMEK, SMPKH, SMEK should be used. Any other combination will trigger error |
| KEYWR_ERR_PARSE_CERT | 7 | Error in parsing certificate |
| KEYWR_ERR_PARSE_FEK | 8 | Error in parsing TI FEK (appended to TIFS binary, before encryption) |
| KEYWR_ERR_PARSE_SMPK_CERT | 9 | Error in parsing SMPK signed certificate (certificate that contains customer key data) |
| KEYWR_ERR_PROGR_BMEK | 10 | Error in programming BMEK into SoC eFuses |
| KEYWR_ERR_PROGR_BMPKH_PART_1 | 11 | Error in programming BMPKH part 1 into SoC eFuses |
| KEYWR_ERR_PROGR_BMPKH_PART_2 | 12 | Error in programming BMPKH part 2 into SoC eFuses |
| KEYWR_ERR_PROGR_KEYCOUNT | 13 | Error in programming KEY COUNT into SoC eFuses |
| KEYWR_ERR_PROGR_KEYREV | 14 | Error in programming KEY REV into SoC eFuses |
| KEYWR_ERR_PROGR_SMEK | 15 | Error in programming SMEK into SoC eFuses |
| KEYWR_ERR_PROGR_SMPKH_PART_1 | 16 | Error in programming SMPKH part 1 into SoC eFuses |
| KEYWR_ERR_PROGR_SMPKH_PART_2 | 17 | Error in programming SMPKH part 2 into SoC eFuses |
| KEYWR_ERR_VALIDATION_CERT | 18 | Error validating certificate |
| KEYWR_ERR_VALIDATION_SMPK_CERT | 19 | Error validating SMPK signed certificate |
| KEYWR_ERR_VALIDATION_BMPK_KEY | 20 | Error validating BMPK key |
| KEYWR_ERR_VALIDATION_SMPK_KEY | 21 | Error validating SMPK key |
| KEYWR_ERR_WRITE_PROT_KEYCOUNT | 22 | Error write protecting key count row |
| KEYWR_ERR_WRITE_PROT_KEYREV | 23 | Error write protecting key revision row |
| KEYWR_ERR_IMG_INTEG_SMPK_CERT | 24 | SMPK signed certificate image integrity failed |
| KEYWR_ERR_PROGR_MSV | 25 | Error in programming MSV into SoC eFuses |
| KEYWR_ERR_PROGR_SWREV | 26 | Error in programming SWREV into SoC eFuses |
| KEYWR_ERR_PROGR_FW_CFG_REV | 27 | Error in programming FW CFG REV into SoC eFuses |
| KEYWR_ERR_DECRYPT_EXT_OTP | 28 | Error in Decrypting EXT OTP extension field |
| KEYWR_ERR_PROGR_EXT_OTP | 29 | Error in programming EXT OTP extension field |
| KEYWR_ERR_PROGR_OVERRIDE | 30 | Error in programming existing field without override specified |
| KEYWR_ERR_JTAG_DISABLE | 31 | Error in programming JTAG DISABLE field |