Trace Layer

Trace Layer Overview

The ability to output human readable trace messages is necessary to be able to properly debug firmware operation. However, due to the potential for huge amounts of messages due to fast transitions in firewalls, clocks, etc, a compact trace format that can be easily machine parsed is required as well. A global ‘trace’ layer is provided so that any sub-system present in the firmware has the ability to output information in a common way over a user configured interface.

Trace Configuration

All built-in trace options can be selectively enabled during runtime as described in Design details for System Firmware Debug Console. The trace destinations are configurable as build options but by default are built in and usage of them is left up to the aforementioned board configuration.

In the interest of allowing debug of early boot within System Firmware the default state of all Board Config Debug configurable trace sources and destinations is enabled. Once the TISCI_MSG_BOARD_CONFIG message is received, the values within boardcfg_dbg_cfg immediately take effect and only the configured trace sources and destinations will be in use until reboot. However, this means that the earliest boot messages before TISCI_MSG_BOARD_CONFIG from System Firmware will always be printed.

Warning

Keeping trace enabled will have considerable impact on performance. While useful for debug, there are many trace points throughout the code and waiting for each print to occur, especially if all trace destinations are enabled, can add considerable to each subsystem init and TISCI message response. If performance is a system requirement trace should be disabled.

All trace debug and trace print messages will be routed as strings over the UART or memory buffer as there is only a single resource for each of these. ITM (JTAG) has multiple channels available that will be partitioned as described below:

ITM Channel Number Usage
0 Trace print strings.
1 Baseport Trace debug.
2 Security Trace debug.
3 Resource Management Trace debug.
4 Power Management Trace debug.

Trace Memory Buffer Location

The trace memory buffer is located within the firmware memory. Information about the location and size can be found below.

SoC Base Address Size
AM65x 0x44083000 0x1000
J721e 0x44083000 0x1000
AM64x 0x44043000 0x0FE0
J7200 0x44083000 0x1000
AM62x 0x4405F000 0x1000
AM62Ax 0x4405F000 0x1000
J721S2 0x4406B000 0x1000
J784S4 0x4406B000 0x1000
AM62Px 0x4405F000 0x1000
J722S 0x4405F000 0x1000

Trace UART Allocation

The table below shows the UART instances used for routing TIFS trace messages over the UART.

SoC UART Instance
AM65x WKUP UART0
J721e WKUP UART0
AM64x MAIN UART1
J7200 WKUP UART0
AM62x MAIN UART1
AM62Ax MAIN UART1
J721S2 WKUP UART0
J784S4 WKUP UART0
AM62Px MAIN UART1
J722S MAIN UART5

Trace Debug Data Format

The Trace Debug API supports the sending of arbitrary u32’s to the various Trace destinations. By defining a common convention for these u32’s to represent data they can be used to describe events within the system. The below format describes the standard meaning of each bit inside the u32.

Note

The trace version for this release is 0x03007

Type Bit Index Use
Domain ID 31 - 29 Identifies which domain this debug code belongs to.
Action ID 28 - 22 Identifies the action this code represents, domain specific.
Message Specific Data 21 - 0 Additional data specific to the domain and action ID.

Optionally, a sub-action ID can be specified as part of the standard message data field in order to provide more granular trace data per subsystem. The below format describes the meaning for each bit inside the u32 when the optional sub-action ID is utilized.

Type Bit Index Use
Domain ID 31 - 29 Identifies which domain this debug code belongs to.
Action ID 28 - 22 Identifies the action this code represents, domain specific.
Sub-Action ID 21 - 16 Identifies the sub-action this code represents, domain specific.
Message Specific Data 15 - 0 Additional data specific to the domain and action ID.

Domain ID

Domain Name Value Use
Baseport 0 Debug trace is from Baseport Domain.
Security 1 Debug trace is from Security Domain
RM 2 Debug trace is from Resource Management Domain
PM 3 Debug trace is from Power Management Domain.
Reserved 4 Reserved for future use.
Reserved 5 Reserved for future use.
Reserved 6 Reserved for future use.
Reserved 7 Reserved for future use.

Messages sent using any reserved Domain IDs will be ignored.

Action & Optional Sub-Action IDs

Below is a listing of the Action IDs and Sub-Action IDs for each domain along with how the Message Specific Data (MSD) is to be interpreted.

The Sub-Action IDs are optionally used by domain owners to provide more granular data for each Action ID. Use of Sub-Action IDs restricts the action data per trace to 16-bits wide.

Baseport Action IDs

Action ID Value Use MSD Use Notes
BP_INIT_COMPLETE 0 OSAL/Baseport init complete Unused  
TISCI_MSG_RECEIVED 1 TISCI Message received (21-16) Queue ID (15-0) TISCI ID When TISCI_MSG_RECEIVED is followed by TISCI_MSG_SENDER_HOST_ID with the same Queue ID, the reported TISCI ID and HOST ID are guaranteed to have come from the same received TISCI message. Queue ID is an arbitrary value used for this purpose.
TISCI_MSG_SENDER_HOST_ID 2 Host ID of sent Message (21-16) Queue ID (15-0) Host ID of request See note above for TISCI_MSG_RECEIVED.
RESERVED 10 N/A N/A  
TRACE_DATA_VERSION 16 OSAL/Baseport trace data version. (19-12) Version major (11-0) Version minor Any System Firmware trace parsing utilities should be able to comprehend the trace version when decoding trace logs
SYSFW_VERSION 17 System Firmware version (15-8) Version (7-4) Subversion (3-0) Patch  
GENERIC_DEBUG 127 Generic Debug Message Any use.  

Security Action IDs

Action ID Value Use MSD Use
RESERVED 0x1 RESERVED NA
Security Init 0x2 Indicates progress of post-boardconfig security initialization Bit [0] - 0 => start, 1 => end
Authentication 0x3 This is the authentication operation and indicates failures seen during authentication, such as with TISCI_MSG_PROC_AUTH_BOOT 0x1 => Certificate too large (>4KB) 0x2 => Issue fetching certificate 0x3 => Issue with Hash operation 0x4 => Hash comparison fails
Read/Write OTP revision 0x4 This indicates failures during run time read/write to OTP revision (swrev, keyrev) 0x1 => Host ID invalid (write APIs)
0x2 => Error in OTP revision identifier
0x3 => Error in value (write APIs)
0x4 => Failure during eFuse programming
0x5 => Failure to validate dual signed certificate (write keyrev API)
FAIL (modifier) 0x40 Action failed when action bit set N/A
Generic Debug 127 Generic Debug message Any use.

Resource Management Action IDs & Sub-Action IDs

Action ID Value Use Sub-Action ID Value MSD Use
RM_INIT 0 RM init complete N/A N/A N/A
RM_CORE_INIT 1 RM core init complete N/A N/A N/A
RA_INIT 3 RA driver init complete N/A N/A N/A
RING_CONFIGURE 4 NavSS ring configuration DEVICE_ID 0 Ring accelerator Device ID
INDEX 1 Ring index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
RING_VIRTID 10 ring Virt ID
RING_MODE 11 ring mode
RING_SIZE 12 ring size
RING_BA_LO_HI 13 Upper 16-bits of base address lo
RING_BA_LO_LO 14 Lower 16-bits of base address lo
RING_COUNT_HI 15 Upper 4-bits of count
RING_COUNT_LO 16 Lower 16-bits of count
RING_ORDERID 17 ring Order ID
RING_GET_CFG 5 Get NavSS ring configuration DEVICE_ID 0 Ring accelerator Device ID
INDEX 1 Ring index
GET_RESET_CFG 2 Configuration retrieval type
RING_VALIDATE_INDEX 6 NavSS ring index validation INDEX 1 Ring index
SS_DEVICE_ID 5 NavSS subsystem device ID
RING_MON_CFG 7 NavSS ring monitor configuration DEVICE_ID 0 Ring accelerator Device ID
INDEX 1 Ring monitor index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
RING_MONITOR_SOURCE 18 Monitor source
RING_MONITOR_MODE 19 Monitor mode
RING_MONITOR_QUEUE 20 Queue, or ring, to monitor
RING_OES_SET 8 Set OES register in NavSS ring accelerator DEVICE_ID 0 Ring accelerator Device ID
INDEX 1 Ring index
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
RING_OES_GET 9 Get OES register in NavSS ring accelerator DEVICE_ID 0 Ring accelerator Device ID
INDEX 1 Ring index
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
UDMAP_INIT 12 UDMAP driver init complete N/A N/A N/A
UDMAP_TX_CH_SET_THRD_ID 13 Set NavSS UDMAP transmit channel thread ID INDEX 1 Transmit channel index
SS_DEVICE_ID 5 NavSS subsystem device ID
UDMA_CH_THREAD_ID 30 PSI-L thread ID
UDMAP_TX_CH_CFG 14 NavSS UDMAP transmit channel configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 transmit channel index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
UDMA_CH_PAUSE_ON_ERR 10 Pause on error
UDMA_CH_ATYPE 11 Channel atype
UDMA_CH_TYPE 12 Channel type
UDMA_CH_FETCH_SIZE 13 Fetch size
UDMA_CH_CQ_QNUM 14 Completion queue number
UDMA_CH_PRIORITY 15 Priority
UDMA_CH_QOS 16 QoS
UDMA_CH_ORDERID 17 Order ID
UDMA_CH_SCHED_PRIORITY 18 Scheduling priority
UDMA_CH_BURST_SIZE 31 Burst size
UDMA_TX_CH_FILT_EINFO 32 Filter extended info
UDMA_TX_CH_FILT_PSWORDS 33 Filter PS words
UDMA_TX_CH_SUPR_TDPKT 34 Teardown packet suppression
UDMA_TX_CH_CREDIT_COUNT 35 Channel credit count
UDMA_TX_CH_FDEPTH 36 Channel fdepth
UDMA_TX_CH_TDTYPE 37 Channel teardown type
UDMAP_TX_CH_GET_CFG 15 Get NavSS UDMAP transmit channel configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 UDMAP transmit channel index
GET_RESET_CFG 2 Configuration retrieval type
UDMAP_GCFG_CFG 16 NavSS UDMAP GCFG region configuration DEVICE_ID 0 UDMAP Device ID
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
UDMAP_RX_CH_SET_THRD_ID 20 Set NavSS UDMAP receive channel thread ID INDEX 1 Receive channel index
SS_DEVICE_ID 5 NavSS subsystem device ID
UDMA_CH_THREAD_ID 30 PSI-L thread ID
UDMAP_RX_CH_CFG 21 NavSS UDMAP receive channel configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 receive channel index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
UDMA_CH_PAUSE_ON_ERR 10 Pause on error
UDMA_CH_ATYPE 11 Channel atype
UDMA_CH_TYPE 12 Channel type
UDMA_CH_FETCH_SIZE 13 Fetch size
UDMA_CH_CQ_QNUM 14 Completion queue number
UDMA_CH_PRIORITY 15 Priority
UDMA_CH_QOS 16 QoS
UDMA_CH_ORDERID 17 Order ID
UDMA_CH_SCHED_PRIORITY 18 Scheduling priority
UDMA_CH_BURST_SIZE 31 Burst size
UDMA_RX_CH_FLOW_ID_START 32 Flow ID start
UDMA_RX_CH_FLOW_ID_COUNT 33 Flow ID count
UDMA_RX_CH_IGNORE_SHORT 34 Ignore long
UDMA_RX_CH_IGNORE_LONG 35 Ignore short
UDMAP_RX_CH_GET_CFG 22 Get NavSS UDMAP receive channel configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 UDMAP receive channel index
GET_RESET_CFG 2 Configuration retrieval type
UDMAP_GCFG_GET_CFG 23 Get NavSS UDMAP GCFG region configuration DEVICE_ID 0 UDMAP Device ID
GET_RESET_CFG 2 Configuration retrieval type
PROXY_INIT 24 Proxy driver init complete N/A N/A N/A
PROXY_CFG 25 NavSS proxy configuration DEVICE_ID 0 Proxy Device ID
INDEX 1 Proxy index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
PROXY_OES_SET 26 Set OES register in NavSS Proxy DEVICE_ID 0 Proxy Device ID
INDEX 1 Proxy index
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
PROXY_OES_GET 27 Get OES register in NavSS Proxy DEVICE_ID 0 Proxy Device ID
INDEX 1 Proxy index
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
UDMAP_FLOW_CFG 29 NavSS UDMAP receive flow configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 receive flow index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
UDMA_FLOW_RX_EINFO_PRESENT 10 extended info present
UDMA_FLOW_RX_PSINFO_PRESENT 11 psinfo present
UDMA_FLOW_RX_ERROR_HANDLING 12 error handling
UDMA_FLOW_DESC_TYPE 13 descriptor type
UDMA_FLOW_RX_SOP_OFFSET 14 SOP offset
UDMA_FLOW_RX_PS_LOCATION 15 PS location
UDMA_FLOW_SRC_TAG_SEL 16 Source tag selector
UDMA_FLOW_DEST_TAG_SEL 17 Destination tag selector
UDMA_FLOW_RX_DEST_QNUM 18 Destination queue number
UDMA_FLOW_RX_FDQ0_SZ0_QNUM 19 FDQ0 SZ0 queue number
UDMA_FLOW_RX_FDQ1_QNUM 20 FDQ1 queue number
UDMA_FLOW_RX_FDQ2_QNUM 21 FDQ2 queue number
UDMA_FLOW_RX_FDQ3_QNUM 22 FDQ3 queue number
UDMAP_FLOW_SZ_CFG 30 NavSS UDMAP receive flow size threshold configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 receive flow index
VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
UDMA_FLOW_RX_FDQ0_SZ1_QNUM 23 FDQ0 SZ1 queue number
UDMA_FLOW_RX_FDQ0_SZ2_QNUM 24 FDQ0 SZ2 queue number
UDMA_FLOW_RX_FDQ0_SZ3_QNUM 25 FDQ0 SZ3 queue number
UDMA_FLOW_RX_SIZE_THRESH_EN 26 size threshold routing enable
UDMAP_OES_SET 31 Set OES register in NavSS UDMAP DEVICE_ID 0 UDMAP Device ID
INDEX 1 Channel index
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
UDMAP_OES_GET 32 Get OES register in NavSS UDMAP DEVICE_ID 0 UDMAP Device ID
INDEX 1 Channel index
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
UDMAP_FLOW_GET_CFG 33 Get NavSS UDMAP receive flow configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 UDMAP receive flow index
GET_RESET_CFG 2 Configuration retrieval type
UDMAP_FLOW_SZ_GET_CFG 34 Get NavSS UDMAP receive flow size threshold configuration DEVICE_ID 0 UDMAP Device ID
INDEX 1 UDMAP receive flow index
GET_RESET_CFG 2 Configuration retrieval type
PSIL_INIT 35 PSI-L driver init complete N/A N/A N/A
PSIL_PAIR 36 Pair NavSS PSI-L threads DEVICE_ID 0 PSI-L proxy device ID
PSIL_SRC_THREAD 10 PSI-L source thread
PSIL_DST_THREAD 11 PSI-L destination thread
PSIL_THREAD_ENABLED 12 PSI-L thread enabled prior to pairing
PSIL_READ 38 Read NavSS PSI-L thread configuration register DEVICE_ID 0 PSI-L proxy device ID
PSIL_THREAD 15 PSI-L thread
PSIL_THREAD_CFG_REG_ADDR 16 Thread configuration register addr
PSIL_THREAD_CFG_REG_VAL_HI 17 Upper 16-bits of register value
PSIL_THREAD_CFG_REG_VAL_LO 18 Lower 16-bits of register value
PSIL_WRITE 39 Write NavSS PSI-L thread configuration register DEVICE_ID 0 PSI-L proxy device ID
PSIL_THREAD 15 PSI-L thread
PSIL_THREAD_CFG_REG_ADDR 16 Thread configuration register addr
PSIL_THREAD_CFG_REG_VAL_HI 17 Upper 16-bits of written value
PSIL_THREAD_CFG_REG_VAL_LO 18 Lower 16-bits of written value
PSIL_UNPAIR 40 Unpair NavSS PSI-L threads DEVICE_ID 0 PSI-L proxy device ID
PSIL_SRC_THREAD 10 PSI-L source thread
PSIL_DST_THREAD 11 PSI-L destination thread
PSIL_THREAD_DISABLED 13 PSI-L thread disabled prior to unpairing
PSIL_SRC_THREAD_PEER 14 Source thread peer register thread value
PSIL_HOST_ID_CHECK 41 Verify message host ID matches resource host ID PSIL_HOST_ID_BCFG 19 Resource host ID in RM boardcfg
PSIL_MSG_HOST_ID 20 Message host ID
IRQ_INIT 43 IRQ driver init complete N/A N/A N/A
IRQ_SET 44 Program interrupt route VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
IRQ_IA_ID 10 IA device ID
IRQ_GLOBAL_EVENT 11 Global event
IRQ_DST_HOST_IRQ 12 Destination host IRQ input index
IRQ_SECONDARY_HOST 13 Secondary host ID
IRQ_SRC_ID 14 Interrupt source device ID
IRQ_SRC_INDEX 15 Interrupt source index
IRQ_DST_ID 16 Interrupt destination device ID
IRQ_VINT 17 Virtual interrupt
IRQ_VINT_STATUS_BIT_INDEX 18 Virtual interrupt status bit
IRQ_RELEASE 45 Clear interrupt route VALID_PARAM_HI 7 Upper 16-bits of valid_params
VALID_PARAM_LO 8 Lower 16-bits of valid_params
IRQ_IA_ID 10 IA device ID
IRQ_GLOBAL_EVENT 11 Global event
IRQ_DST_HOST_IRQ 12 Destination host IRQ input index
IRQ_SECONDARY_HOST 13 Secondary host ID
IRQ_SRC_ID 14 Interrupt source device ID
IRQ_SRC_INDEX 15 Interrupt source index
IRQ_DST_ID 16 Interrupt destination device ID
IRQ_VINT 17 Virtual interrupt
IRQ_VINT_STATUS_BIT_INDEX 18 Virtual interrupt status bit
IRQ_IA_OES_SET 46 Set OES register in Interrupt Aggregator DEVICE_ID 0 IA Device ID
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
IRQ_IA_OES_GET 47 Get OES register in Interrupt Aggregator DEVICE_ID 0 UDMAP Device ID
EVENT 3 Global event
OES_REG_INDEX 4 OES register index
IRQ_IA_INIT 48 IA driver init complete N/A N/A N/A
IRQ_IA_MAP_VINT 49 Map an event to an IA virtual interrupt DEVICE_ID 0 IA device ID
IA_VINT 10 Virtual interrupt
IA_GLOBAL_EVENT 11 Global event
IA_VINT_STATUS_BIT 12 Virtual interrupt status bit
IRQ_IA_UNMAP_VINT 50 Unmap an event from an IA virtual interrupt DEVICE_ID 0 IA device ID
IA_VINT 10 Virtual interrupt
IA_GLOBAL_EVENT 11 Global event
IA_VINT_STATUS_BIT 12 Virtual interrupt status bit
IRQ_IR_INIT 52 IR driver init complete N/A N/A N/A
IRQ_IR_CFG 53 Configured IR input to output mapping DEVICE_ID 0 IR device ID
IR_INPUT 10 IR input index
IR_OUTPUT 11 IR output index
IRQ_IR_CLR 54 Cleared IR input to output mapping DEVICE_ID 0 IR device ID
IR_INPUT 10 IR input index
IR_OUTPUT 11 IR output index
RESASG_FIREWALL_CFG 59 RM resource assignment firewall configuration INDEX 1 Resource index
RESASG_UTYPE 6 Resource assignment unique type
RESASG_FWL_ID 13 Channelized firewall ID
RESASG_FWL_CH 14 Channelized firewall channel
RESASG_VALIDATE_RESOURCE 60 RM validate resource against board configuration INDEX 1 Resource index
RESASG_UTYPE 6 Resource assignment unique type
RESASG_VALIDATE_HOST 10 host ID
RESOURCE_GET 61 Retrieve a resource range for a host RESASG_UTYPE 6 Resource assignment unique type
RESOURCE_GET_TYPE 10 Resource type
RESOURCE_GET_SUBTYPE 11 Resource subtype
RESOURCE_GET_RANGE_START 12 Resource range start
RESOURCE_GET_RANGE_NUM 13 Resource range number
RESOURCE_GET_SECONDARY_HOST 14 Secondary host
DEVGRP_VALIDATE 62 Validate device against current RM device group DEVICE_ID 0 Device ID
DEVGRP_BOARDCFG 10 RM Board configuration devgrp
DEVGRP_DEVICE 11 RM managed device devgrp
FAIL (modifier) 0x40 Action failed when action bit set N/A N/A N/A
GENERIC_DEBUG 127 Generic Debug Message N/A N/A Any use.

Power Management Action IDs

Action ID Value Use MSD Use
DEVICE_ON 0 Device has been turned on . Device ID
DEVICE_OFF 1 Device has been turned off. Device ID
CLOCK_ENABLE 2 Clock has been enabled. Clock ID
CLOCK_DISABLE 3 Clock has been disabled. Clock ID
CLOCK_SET_RATE 4 Clock frequency has been changed. [21:17] - Clock frequency, exponent [16:10] - Clock frequency, significand [9:0] - Clock ID
CLOCK_SET_PARENT 5 Clock parent has been changed. [21:10] - New parent ID [9:0] - Clock ID
MSG_RECEIVED 6 TI-SCI message received Message ID
MSG_PARAM_DEV_CLK_ID 7 TI-SCI message content: dev/clk-ids [10:21] - Clock ID [9:0] - Device ID
MSG_PARAM_VAL 8 TI-SCI message content: value Target value
WAKE_ARM 9 ARM wakeup event received Host ID
WAKE_HANDLER 10 Wakeup handler executed Interrupt ID
PD_GET 11 Powerdomain get [21:20] - PSC ID [19:14] - Powerdomain ID [13:0] - PD Use count
PD_PUT 12 Powerdomain put [21:20] - PSC ID [19:14] - Powerdomain ID [13:0] - PD Use count
SET_LOCAL_RESET 13 Set local reset [21:20] - PSC ID [19:14] - Powerdomain ID [0] - Enable (1) / Disable (0)
MODULE_GET 14 Module get [21:20] - PSC ID [19:14] - LPSC ID [13:0] - Module Use count
MODULE_PUT 15 Module put [21:20] - PSC ID [19:14] - LPSC ID [13:0] - Module Use count
RETENTION_GET 16 Retention put [21:20] - LPSC ID [19:14] - Powerdomain ID [13:0] - Module Retention count
RETENTION_PUT 17 Retention put [21:20] - LPSC ID [19:14] - Powerdomain ID [13:0] - Module Retention count
PD_INIT 18 Powerdomain init [19:14] - Powerdomain ID [21:20] - PSC ID
PSC_INV_DATA 19 Invalid PSC Data N/A
PD_TRANS_TIMEOUT 20 Powerdomain Transition timeout [21:20] - PSC ID [19:14] - Powerdomain ID [2:0] - Priv Position information
PD_INV_DEP_DATA 21 Powerdomain Invalid Dep Data [21:20] - Dependent PD ID [19:14] - Powerdomain ID [2:0] - Priv Position information
PD_RSTDNE_TIMEOUT 22 Powerdomain resetdone timeout [21:20] - PSC ID [19:14] - Powerdomain ID [2:0] - Priv Position information
SET_MODULE_RESET 23 Set module Reset [21:20] - PSC ID [19:14] - Powerdomain ID [0] - Enable (1) / Disable (0)
PM_INIT 32 Power Management Init [20] - Power Init result [19] - Modules defer result [18:16] - Index of start module [15:0] - Error value
PM_DEV_INIT 33 Power Management device init [21:12] - Device ID [11:0] - Error value
PM_SYS_RESET 34 Power Management system reset [21:14] - Domain [13:0] - Error value
FAIL (modifier) 0x40 Action failed when action bit set N/A
LPM_SEQ 48 Low power mode sequence [21:8] - Sequence number [7:0] - Value
EXCLUSIVE_BUSY 123 Other hosts have enabled the device which exclusive access has been requested [21:12] - Device ID [11:6] - Requesting host ID [5:0] - One of other host IDs
EXCLUSIVE_DEVICE 124 Another host has exclusive access to the requested device [21:8] - Device ID [7:0] - Requesting host ID
INVALID_STATE 125 API attempted to set invalid state Target state
BAD_DEVICE 126 API received bad device ID Device ID
GENERIC_DEBUG 127 Generic Debug Message Any use.