From RTSC-Pedia
![]() | [printable version] [offline version] | offline version generated on 23-Mar-2009 01:03 UTC | ![]() |
XDCspec Language Reference
Elements of the RTSC specification language
Contents |
Grammar
XDCspec - config-specification | under construction |
XDCspec - const-specification | under construction |
XDCspec - enum-specification | under construction |
XDCspec - extern-specification | under construction |
XDCspec - function-specification | under construction |
XDCspec - package-specification | Package specification syntax |
XDCspec - proxy-specification | under construction |
XDCspec - struct-specification | under construction |
XDCspec - typedef-specification | under construction |
XDCspec - unit-specification | under construction |
XDCspec - declaration | under construction |
XDCspec - initializer | under construction |
Attributes
Attributes are additional properties that can be associated with elements of the XDCspec language. Attributes are always prefixed with '@' and must appear immediately before the element to which they apply.
For example, it is possible to declare that a module is "gated" by adding the @Gated attribute just before the module statement in the module's spec file.
| @Gated module System { ...} |
The following list enumerates the complete set of currently supported attributes.
XDCspec - @Annex | This parameter or method has been added |
XDCspec - @CommandOption | under construction |
XDCspec - @CustomHeader | This module's header includes handcrafted headers |
XDCspec - @DirectCall | Always generate a direct call to this function |
XDCspec - @Encoded | This type has custom encoding |
XDCspec - @Factory | This proxy is a factory |
XDCspec - @Gated | This module has a gate |
XDCspec - @GlobalNames | This module defines "unprefixed" identifiers |
XDCspec - @InstanceFinalize | This module's instances require finalization |
XDCspec - @InstanceInitError | This module's instance initialization can fail |
XDCspec - @Macro | This function is a macro |
XDCspec - @ModuleStartup | This module has a startup initialization function |
XDCspec - @NoRuntime | This module does not use xdc.runtime |
XDCspec - @Opaque | under construction |
XDCspec - @Prefix | This module defines a custom prefix |
XDCspec - @Proxy | under construction |
XDCspec - @System | under construction |
XDCspec - @TargetHeader | This metaonly module generates a header |
XDCspec - @Template | This module contributes configuration C code |
XDCspec - @XmlDtd | This structure can be serialized as XML |
Module Attributes
Module Attributes. The following list enumerates the attributes applicable to modules and interfaces.
XDCspec - @CustomHeader | This module's header includes handcrafted headers |
XDCspec - @Gated | This module has a gate |
XDCspec - @GlobalNames | This module defines "unprefixed" identifiers |
XDCspec - @InstanceFinalize | This module's instances require finalization |
XDCspec - @InstanceInitError | This module's instance initialization can fail |
XDCspec - @ModuleStartup | This module has a startup initialization function |
XDCspec - @NoRuntime | This module does not use xdc.runtime |
XDCspec - @Prefix | This module defines a custom prefix |
XDCspec - @TargetHeader | This metaonly module generates a header |
XDCspec - @Template | This module contributes configuration C code |
Method Attributes
Method Attributes. The following list enumerates the attributes applicable to methods.
XDCspec - @Annex | This parameter or method has been added |
XDCspec - @DirectCall | Always generate a direct call to this function |
XDCspec - @Macro | This function is a macro |
XDCspec - @System | under construction |
Type Attributes
Type Attributes. The following list enumerates the attributes applicable to types defined in a module or interface.
XDCspec - @Encoded | This type has custom encoding |
XDCspec - @XmlDtd | This structure can be serialized as XML |
Configuration Attributes
Configuration Attributes. The following list enumerates the attributes applicable to configuration parameters defined in a module or interface.
XDCspec - @CommandOption | under construction |
XDCspec - @Factory | This proxy is a factory |
XDCspec - @Proxy | under construction |
XDoc tags
XDCspec - @_nodoc | under construction |
XDCspec - @a | under construction |
XDCspec - @b | under construction |
XDCspec - @c | under construction |
XDCspec - @details | under construction |
XDCspec - @field | under construction |
XDCspec - @link | under construction |
XDCspec - @param | under construction |
XDCspec - @p | under construction |
XDCspec - @p(blist) | under construction |
XDCspec - @p(code) | under construction |
XDCspec - @p(dlist) | under construction |
XDCspec - @p(html) | under construction |
XDCspec - @p(nlist) | under construction |
XDCspec - @p(text) | under construction |
XDCspec - @see | under construction |
XDCspec - @summary | under construction |
XDCspec - @value | under construction |
See also
NOTE: The following documents are obsolete but contain information that has yet to be moved to the current document
XDCspec Language Summary | XDCspec language quick reference |
![]() | [printable version] [offline version] | offline version generated on 23-Mar-2009 01:03 UTC | ![]() |