package xdc.tools.repoman

Repository Manager tool

This tool creates and manages package repositories. It displays information about archived packages, extracts archived packages, extracts repositories from bundles and deletes packages from repositories. [ more ... ]
XDCspec declarations sourced in xdc/tools/repoman/package.xdc
requires xdc.tools;
requires xdc.shelf;
 
package xdc.tools.repoman [1, 0, 0, 0] {
 
    module Main;
    // Command implementation
}
USAGE
xs xdc.tools.repoman [--help]
    -t [-v] [-p pathname] [packagename...|packagefile...]
    -n [-v] [-p pathname] [packagename...|packagefile...]
    -x [-v] [-D] [-R] [-F] [-r destrepo] [-p path] [-b bundlerepository] [packagename...|packagefile...]
    -d [-v] [-r destrepo] packagename...
    -c [-v] [-r destrepo] [-p pathname] packagename...
    --rsave -f file [-p searchpath] repository...
    --rrestore -f file [-p searchpath] [index-spec]
    --rcreate -f file [-p searchpath] [index-spec] destrepository...
OPTIONS
-t
Display package info
-n
Display package names only
-x
Extract package(s)
-d
Delete package(s)
-p
Path arg
-r
Repository arg
-D
Include package dependencies
-R
Recursive include package dependencies
-a
Return an array of strings
-X
Return a Results struct as XML
-v
Print informative messages during execution
-b
Bundle repository arg
-F
Force incompatible packages
-c
Copy package(s)
-f
file arg to save/restore repository
-rsave
Save a repository's information to file
-rrestore
Restore one or more repositories from information in file
-rcreate
Create one or more repositories from information in file
DETAILS
This tool creates and manages package repositories. It displays information about archived packages, extracts archived packages, extracts repositories from bundles and deletes packages from repositories.
Information about archived packages can be displayed with the '-t' and '-n' options. The '-p' argument is used to specify a directory to search in. If the '-p' arg is omitted, the current directory is searched. Specific packages can searched for by specifying one or more package names, or one or more package archives at the end of the command line. If no packages are specified, information on all packages found in the search directory will be displayed.
Archived packages can be extracted to a repository with the '-x' option. '-x -D' will extract dependent packages, too. '-x -R' will recursively extract dependent packages. If any of the packages in the specified package list are not compatible, the operation will be aborted. '-F' can be used to force all packages to be extracted, regardles of compatibility. The '-p' arg is used to specify a directory to search in. If not specified, the current directory will be searched. The '-x' option also extracts repositories from a bundle. In this case, the last argumnet specifies the bundle file to extract from. The repositories to be extracted are be specified with the '-b' arg.
Packages can be deleted from a repository with '-d'. If the package has any subdirectores that contain packages, they will be left intact. After the package is deleted, if the package has no subdirectories with packages, empty directories that are part of the fully qualified package will be deleted, too.
Packages can be copied between repositories with '-c'. If the package being copied already exists in the destination repository, it will be deleted prior to being replaced.
The '-r' argument specifies a destination repository. If '-r' is omitted, the repository of the current package is used. If there is no current package, the current directory is used.
When a package name is given, it can be specified in full, such as 'ti.platforms.sim6xxx', or the wildcard characters '*' and '?' may be used, as in 'ti.platforms.*' or 'ti.catalog.c??00'. A version/key can also be attached to a package name in the following manner: 'ti.platforms.c6000[1,0,0,0,313835]'. A prefix of the full version/key may also be used: 'ti.platforms.c6000[1,0]'.
If a package name has multiple matches either with or without a version/key specified, the most recent will be selected. Wildcards may also be used when naming a package archive file.
EXAMPLES
xs xdc.tools.repoman -t
Displays all info on all archived packages in the current directory
xs xdc.tools.repoman -t -p C:\xdc-o19\exports
Displays all info on all archived packages in C:\xdc-o19\exports
xs xdc.tools.repoman -t -p C:\xdc-o19\exports ti.platforms.*
Displays all info on archived packages whose names begin with ti.platforms. in C:\xdc-o19\exports
xs xdc.tools.repoman -t -p C:\xdc-o19\exports ti_platforms*.tar
Displays all info on packages in files that match ti_platforms*.tar in C:\xdc-o19\exports
xs xdc.tools.repoman -t -p C:\xdc-o19\exports ti.catalog.c6000 ti.catalog.sim6xxx
Displays all info on archived packages ti.catalog.c6000 and ti.catalog.sim6xxx in C:\xdc-o19\exports
xs xdc.tools.repoman -x
Extracts all archived packages in the current directory to the current repository
xs xdc.tools.repoman -x -r C:\myrepo\packages -p C:\exports
Extracts all archived packages in C:\exports to C:\myrepo\packages repository
xs xdc.tools.repoman -x -r C:\myrepo\packages -p C:\exports ti.catalog.*
Extracts packages matching ti.catalog.* from c:\exports to c:\myrepo\packages
xs xdc.tools.repoman -x -r C:\myrepo\packages C:\exports\ti_catalog*.tar
Extracts packages from files matching C:\exports\ti_catalog*.tar to c:\myrepo\packages
xs xdc.tools.repoman -x -r C:\myrepo\packages C:\exports\ti_catalog*.tar
Extracts packages from files matching C:\exports\ti_catalog*.tar to c:\myrepo\packages
xs xdc.tools.repoman -x -R -r C:\myrepo -p C:\xdc-o19\exports ti.platforms.sim6xxx
Extracts the package ti.platforms.sim6xxx and all recursively dependent packages from C:\xdc-o19\exports to C:\myrepo
xs xdc.tools.repoman -x -r C:\ -b packages C:\exports\xdc_core.tar.gz
Extracts the repository 'packages' from bundle C:\exports\xdc_core.tar.gz to C:\
xs xdc.tools.repoman -c -r C:\destdir\packages -p C:\srcdir\packages ti.catalog.c6000
Copies the package ti.catalog.c6000 from C:\srcdir\packages to C:\destdir\packages
xs xdc.tools.repoman --rsave -f c:/repoinfo.rmn -p c:/pkgarchives;c:/testpkgs c:/myrepo
Saves package information for repository c:/myrepo to file c:/repoinfo.rmn. Also saves the search path c:/pkgarchives;c:/testpkgs
xs xdc.tools.repoman --rrestore -f c:/repoinfo.rmn -p c:/pkgarchives;c:/testpkgs
Restores all of the packages in the repository referenced in c:/repoinfo.rmn. Uses the search path c:/pkgarchives;c:/testpkgs to find and copy packages. Will create the repository if it doesn't exist.
xs xdc.tools.repoman --rcreate -f c:/repoinfo.rmn -p c:/pkgarchives;c:/testpkgs c:/mynewrepo
Creates the new repository c:/mynewrepo from the repository referenced in the file c:/repoinfo.rmn. Uses the search path c:/pkgarchives;c:/testpkgs to find and copy packages. If successful, the newly created repository will be identical to its predecessor referenced in c:/repoinfo.rmn.
generated on Sat, 01 Nov 2008 10:29:21 GMT