package xdc

Core interfaces and modules necessary for the XDC runtime

In addition to the interfaces specified below, this package also supplies a C/C++ header, std.h that facilitates the creation of portable sources. This header defines a set of "base" types that enable the creation of C-code that is portable between any two targets. C source code that relies exclusively on these types is portable to all targets and platforms. Where appropriate, the types defined below are related to the types defined in the library headers perscribed by the C99 standard (ISO/IEC 9899:1999). [ more ... ]
XDCspec declarations sourced in xdc/package.xdc
package xdc [1, 1, 1, 0] {
 
    interface IPackage;
    // Base interface implemented by all packages
}
DETAILS
In addition to the interfaces specified below, this package also supplies a C/C++ header, std.h that facilitates the creation of portable sources. This header defines a set of "base" types that enable the creation of C-code that is portable between any two targets. C source code that relies exclusively on these types is portable to all targets and platforms. Where appropriate, the types defined below are related to the types defined in the library headers perscribed by the C99 standard (ISO/IEC 9899:1999).
Why not simply use the C99 types? Having a unique set of names provides a layer of insulation between a portable code base and a particular compiler; e.g., even if a compiler does not support the C99 types or defines them inappropriately for a particular device, it is possible to use the compiler without changing the code base. Thus, the developer is not forced to choose the lesser of two evils: waiting for a change to the compiler or forking the code base for a particular compiler device combination.
There are several situations where a small separate set of portable types can help the maintainability of a code base.
  • not all of the types described in the C99 standard are required to be defined by conformant implementations nor is it possible for all devices to implement some of the types specified (e.g., int8_t is not implemented on C54 devices); so it is difficult to identify non-portable source code.
  • not all compilers provide C99 type support; if XDC supplies the type definition and the compiler is updated to include C99 types, a compilation error will occur if the source includes the C99 headers.
  • not all compiler and device combinations are conformant; even high quality compilers may not properly define the types for each device supported by compiler.
USAGE
      #include <xdc/std.h>
To compile sources that include xdc/std.h, two symbols must be defined before including this header:
xdc_target_types__
the package qualified path of the target's standard types header; e.g., ti/targets/std.h. This value is specified in the target's stdInclude config parameter; see xdc.bld.ITarget.stdInclude
xdc_target_name__
the target's module name without the package prefix; e.g., C64 rather than ti.targets.C64.
For example, to compile sources for the ti.targets.C64 target using TI's cl6x compiler, the following command line is sufficient:
      cl6x -Dxdc_target_types__=ti/targets/std.h -Dxdc_target_name__=C64
Each of the type names below has an equivalent "long name"; i.e., a name that has an "xdc_" prefix. For example, the type Bool can also be written as "xdc_Bool". Long names exist to avoid conflicts with names defined or used by existing code bases.
In the event that one of the short type names below conflicts with another type name (that can not be changed), it is possble to disable the short names by defining the symbol xdc__nolocalnames before including xdc/std.h.
      #define xdc__nolocalnames
      #include <xdc/std.h>
STANDARD TYPES
This header may be included multiple times and defines the following target-dependent types:
Bool
this type is large enough to hold the values 0 or 1. The constants TRUE and FALSE are of this type; see below.
String
this type is defined to be a char * and exists to allow code to distinguish between pointers to buffers of raw data and '\0' terminated strings.
Intn, where n = 8, 16, or 32
signed integer type that is large enough to hold n bits; the actual target type may by be larger than n. This type is equivalent to one of the C99 types int_leastn_t or int_fastn_t; see Section 7.18.
UIntn, where n = 8, 16, or 32
unsigned integer type that is large enough to hold n bits; the actual target type may by be larger than n. This type is equivalent to one of the C99 types uint_leastn_t or uint_fastn_t; see ISO/IEC 9899:1999 Section 7.18.
Bitsn, where n = 8, 16, or 32
unsigned integer type that is precisely n bits. Not all targets support all values of n; if the target does not support an exact size the corresponding type is not defined. This type is equivalent to the corresponding C99 type uintn_t; see ISO/IEC 9899:1999 Section 7.18.
Fxn
this type is a pointer to code; it can hold a pointer to any function.
Ptr
this type is a pointer to data; it can hold a pointer to any data structure.
IArg
this integer type is large enough to hold a Fxn, Ptr, or Int.
UArg
this unsigned integer type is large enough to hold a Fxn, Ptr, or Int.
LLong
this long integer type is large enough to hold a Long and is defined as a 'long long' type on targets that support this type; otherwise, it is simply a Long. Note that C99 requires the long long type to be at least 64-bits wide (See ISO/IEC 9899:1999 Section 5.2.4.2.1). But some compilers do not support 64-bit integral types and some don't support the long long even though they do support 64-bit integral types. Since these variations limit the portability of valid C sources, the LLong type is always defined, is always at least as wide as the Long type, and is at least 64-bits wide for targets that support 64-bit integral types.
ULLong
this unsigned long integer type is large enough to hold a ULong and is defined as a 'unsigned long long' type on targets that support this type; otherwise, it is simply a ULong.
The xdc/std.h header also defines the following aliases for the base C types. These aliases exist so that C sources can consistently follow a naming convention in which all type names are written in camel-case.
Char and UChar
aliases for char and unsigned char, respectively
Short and UShort
aliases for short and unsigned short, respectively
Int and UInt
aliases for int and unsigned int, respectively
Long and ULong
aliases for long and unsigned long, respectively
Double and LDouble
aliases for double and long double, respectively
SizeT
alias for size_t
VaList
alias for va_list
The types above are defined for all targets. Some targets can support the following additional types. Since these types are not always supported by a target, these types should only be used when no other type sufficies.
Bitsn, where n = 8, 16, or 32
this unsigned integer type is precisely n-bits wide. This type is equivalent to the optional C99 type uintn_t; see ISO/IEC 9899:1999 Section 7.18.1.1. This type is defined if and only if the preprocessor macro xdc__BITSn__ is defined.
(64-Bit Types) Although the C99 standard requires support for 64-bit types, not all compiler/device combinations can usefully support them. As a result, the 64-bit types described here may not be defined for all targets. For each type there is a corresponding pre-processor macro which is defined if and only if the type is supported.
Int64
signed integer type that is large enough to hold 64 bits; the actual target type may by be wider than 64 bits. This type is equivalent to one of the C99 types int_least64_t or int_fast64_t; see Section 7.18. This type is defined if and only if the preprocessor macro xdc__INT64__ is defined.
UInt64
unsigned integer type that is large enough to hold n bits; the actual target type may by be wider than 64 bits. This type is equivalent to one of the C99 types uint_least64_t or uint_fast64_t; see ISO/IEC 9899:1999 Section 7.18. This type is defined if and only if the preprocessor macro xdc__INT64__ is defined.
Bits64
unsigned integer type that is precisely 64 bits wide. If the target does not support an exact 64-bit size, this type is not defined. This type is equivalent to the corresponding C99 type uint64_t; see ISO/IEC 9899:1999 Section 7.18. This type is defined if and only if the preprocessor macro xdc__BITS64__ is defined.
PREDEFINED MACROS
In addition to the type definitions above, xdc/std.h also defines the following commonly used constants
NULL
defined as 0
TRUE
defined as ((Bool)1)
FALSE
defined as ((Bool)0)
Finally, xdc/std.h defines the following target-independent symbols that have target-dependent values; these predefined macros enable conditional compilation of source files based on target-specific attributes.
{c_target_name}
this symbol (the target's fully qualified name with all '.'s replaced with '_') is always defined and allows one to easily include target-specific headers or define symbols with target-specific values.
xdc_target__isaCompatible_{isa_name}
for every ISA named in the array returned by this target's xdc.bld.ITarget.getISAChain() method, a symbol of this name is defined. In addition to enabling one to create code specific to a particular ISA, this allows one to create code that depends on TI's C6x architecture without being dependent on a particular member of the C6x family, for example.
xdc_target__isa_{isa}
this symbol is always defined and {isa} is the target's isa (see xdc.bld.ITarget.isa).
xdc_target__{little,big}Endian
if this target's xdc.bld.ITarget.model.endian property is specified, this symbol is defined and {little,big} is replaced by model.endian.
xdc_target__{code_model_name}Code
if this target's xdc.bld.ITarget.model.codeModel is specified, this symbol is defined and {code_model_name} is replaced by model.codeModel.
xdc_target__{data_model_name}Data
if this target's xdc.bld.ITarget.model.dataModel is specified, this symbol is defined and {data_model_name} is replaced by model.dataModel.
xdc_target__os_{os_name}
this symbol is always defined and {os_name} is the target's os name (see xdc.bld.ITarget.os).
xdc_target__sizeof_{type_name}
this symbol is defined for each type name supported in the target's xdc.bld.ITarget.stdTypes structure, {type_name} is the name of one of the standard types supported above, and the value is sizeof(type_name).
xdc_target__alignof_{type_name}
this symbol is defined for each type name supported in the target's xdc.bld.ITarget.stdTypes structure, {type_name} is the name of one of the standard types supported above, and the value is the alignment required by the compiler for {type_name}.
xdc_target__bitPerChar
this symbol is always defined and specifies the number of bits in the target's char. This value combined with the xdc_target__sizeof_ values allows C code to determine the precise number of bits in any of the standard types.
SEE
THROWS
XDCException exceptions are thrown for fatal errors. The following error codes are reported in the exception message:
xdc.PACKAGE_NOT_FOUND
This error is reported whenever a specified package is not found This may happen for the following reasons:
  • Ensure that the package in question is contained in one of the repositories named in the package path.
  • The package has not been built by the xdc tool even though the physical package directory may be present along the package path
xdc.FILE_NOT_FOUND
This error is reported when a specified file is not found. Ensure that any directory name prefix in the name is a package directory contained in one of the repositories named in the package path. For example, if "ti/targets/linkcmd.xdt" can't be found, make sure the directory ti/targets/ is contained in at least one repository named in the package path.
xdc.MODULE_NOT_FOUND
This error is reported when a specified module can't be found. Ensure that the package containing the module in question is contained in at least one repository named in the package path. Also ensure that the module name is qualified with the package name. For example, to refer to the module Engine in the package ti.sdo.ce, the module name should be specified as ti.sdo.ce.Engine.
xdc.TOOL_USAGE_ERROR
This error may happen when the xs tool is not passed the expected command line arguments.
xdc.MODULE_UNDEFINED_MAIN_FUNCTION
This error is reported when the xs tool is passed a module that does not define a main function. Ensure that the meta-domain implementation of the module has a main function.
xdc.SPEC_FILE_ERROR
This error is reported when there is a parsing error in a specification file. Check the spec. file for syntax errors.
xdc.DEPRECATED_FUNCTION
This error is reported whenever a deprecated function is called.
generated on Sat, 01 Nov 2008 10:29:30 GMT