Installation and Setup for DSP/BIOS 5.31

 

This version of DSP/BIOS is delivered independent of Code Composer Studio (CCStudio). It is available for Linux, Solaris, and Microsoft Windows. It includes support for all DSP families supported by DSP/BIOS: C28x, C54x, C55x, and C6000.

 

Quick Start: If you want to quickly try DSP/BIOS with command-line/makefile builds (and not use Code Composer Studio), follow the steps in the Installing DSP/BIOS, Setting System Variables, and the Building Examples from the Command Line sections.

 

IMPORTANT: The BIOS_INSTALL_DIR environment variable must be set in order for you to use BIOS 5.31, see Setting System Variables.

 

For the latest information about what’s new in this release and any known issues, see the release notes (which, in turn, has links to the release notes of the sub-components that make up the DSP/BIOS product).

 

This document describes how to perform the following tasks:

·        Installing DSP/BIOS

·         Setting System Variables

·        Coordinating with CCStudio

o       Selecting the DSP/BIOS Version for CCStudio

o       Testing the Installation

·        Updating DSP/BIOS Applications

o        Converting CDB Files to TCF Files
(For the CCStudio message about converting CDB files, read this section.)

o       Modifying CCStudio Projects to Use TCF Files

o       Makefiles for DSP/BIOS Applications

o       Running the Tconf Debugger

·        DSP/BIOS Examples

o       Building Examples from the Command Line

o       Porting Examples to a New Platform

·        How to make one DSP/BIOS installation accessible to multiple CCStudio installations via the BIOS Selector

·        More Information About DSP/BIOS

Installing DSP/BIOS

To install this version of DSP/BIOS, follow these steps:

1.     Copy or download the distribution file for your operating system to a temporary location. There is a different distribution file for each supported OS; make sure to install the proper one. They can be installed either via the GUI or the command line (-console option). The Linux/Solaris file can be installed only via the command-line.

2.     Choose an install directory anywhere on your system; if Windows it is recommended to be at the top of a CCS 3.3 (or higher) installation (e.g. C:\CCStudio_v3.3). The directory must not have any spaces in its path. Make sure you have at least 200 MB available, or the install will fail with a Java error.

The rest of this document uses <install_dir> to refer to the location you choose. Most examples in this document are for Windows.

3.     Run the self-extracting installation file you downloaded. For command-line installations, use the –console flag on the command line. For example:

./dsp_bios_setuplinux_5_31_00_xx.bin -console

4.     During the installation, accept the End User License Agreement, and specify the directory you chose above as the destination directory.

5.  If CCS 3.3 is already installed, then during the BIOS 5.31 installation a utility runs that updates the CCS version of TConfCmdObject.ocx (a hidden plugin responsible for Tconf integration and updating from 4.90 to 5.31).  If BIOS 5.31 is installed prior to CCS 3.3, then the BIOS 5.31 UpdateTConfCmdObject.exe utility needs to be run manually after CCS 3.3 is installed.  To do this, open a command window, change to the <install_dir>/packages/ti/bios/bti/bin directory, and type "UpdateTconfCmdObject -f".

 

If you ever need to uninstall DSP/BIOS, an uninstaller is provided for Windows (e.g. Control Panel -> Add/Remove Programs). For Linux and Solaris, go to the <install_dir> and remove all the files with the “rm –rf <install_dir>/bios_5_31” command.

Setting System Variables

To setup this version of DSP/BIOS, these steps must be followed:

1.     Create the BIOS_INSTALL_DIR system environment variable, and set it to <install_dir>\bios_5_31.

 

     On Windows XP, you create system environment variables by opening System Properties from the Control Panel. In the Advanced tab, click the Environment Variables button. Use the System variables area to edit existing variables and create new variables.
 

2.     If building outside of CCS, Insert the following location at the beginning of your PATH system environment variable. (Remove any that were put in for a DSP/BIOS 5.10 or 5.20 installation.) 

     For Windows use back slashes (“\”):

%BIOS_INSTALL_DIR%\xdctools
(Windows requires a semicolon ; between each system environment variable you add to the PATH)
 

     For Solaris/Linux use forward slashes (“/”):

 

       If you are using bash on Linux, change the PATH with the following command:

export PATH=$BIOS_INSTALL_DIR/xdctools:$PATH

  If you are using csh on Solaris, change the PATH with the following command:

Set PATH =($BIOS_INSTALL_DIR/xdctools $PATH)

Coordinating with CCStudio

In order to correctly build and communicate via Run-Time Analysis (RTA) with a DSP/BIOS application, CCStudio needs to be configured with the version of the tools and DLLs that matches the DSP/BIOS version of the applications.  This is setup via the BIOS Selector.

 

If you are using Linux/Solaris, you can copy applications you have built to a Windows system with CCStudio for debugging.

Selecting the DSP/BIOS Version for CCStudio

For CCStudio 3.3 or higher, you can choose which version of DSP/BIOS to use with CCStudio. This choice is on a per DSP family basis. To do this, follow these steps:

1.     Open the Component Manager, by choosing Help->About in CCStudio and clicking the Component Manager button. You can also open the Component Manger from the Start->Programs->Texas Instruments menu.

2.     Expand the Target Content (DSP/BIOS) folder to see a list of targets. For your target platform, expand the list to see the available DSP/BIOS versions. Put a checkmark next to the version of DSP/BIOS you want to use. Information about the selected version of DSP/BIOS is shown to the right.

 

 



3.     You may see a message that says the combination you have selected is untested. This message is informational only, and does not necessarily indicate that the combination will not work correctly.  Please check the release notes for CCS and DSP/BIOS.

4.     Save your change and exit from the Component Manager. Then, restart CCStudio.  CCStudio uses a field in the project file (*.pjt), CPUFamily, to determine which BIOS is selected.  

IMPORTANT: Make sure when you are switching BIOS versions that the BIOS_INSTALL_DIR variable is updated to match and if you are using DosRun.bat that it is updated as well for both BIOS and RTDX.

Testing the Installation

The hello example comes with all the files generated for a number of platforms. You can run the example without rebuilding to test the installation and your selection of the DSP/BIOS version.

1.     Open CCStudio.

2.     Load the hello.out executable for the platform you are using. These are in <install_dir>\bios_5_31\packages\ti\bios\examples\basic\hello\<target>.

3.     Choose DSP/BIOS->Message Log to open the log.

4.     Run the program.

5.     View the log and you should see the hello message.

Updating DSP/BIOS Applications

DSP/BIOS 5.31 now uses Tconf for DSP/BIOS configuration instead of a CDB file. If you have a DSP/BIOS 4.90 application or older, you first convert your CDB file to TCF, and then use CCStudio as you would normally to build projects, or build from the command line.

 

NOTE:  The CDB file created by the DSP/BIOS Configuration Tool (gconf) is now generated when you run gconf or a TCF Tconf script and no longer considered a source file. You can still view CDB files with the gconf DSP/BIOS Configuration Tool in read-only mode. However, to change a DSP/BIOS configuration, you must now edit the TCF file with gconf or a text editor.

Converting CDB Files to TCF Files

 

Unless you already have a TCF file, you need to follow one of these procedures to convert your CDB file to a TCF file.  In both cases you must have access to your previous version of DSP/BIOS that you were using CDB with.

CCS Automated Procedure:

1.     From within CCS, open your project file.

2.     You will see a popup box indicating that your CDB file and project need to be updated; click OK which will then do the conversion. 

NOTE:  If you are using CCS 3.3 or later this step will fail, but a script file (cdb2tcf.bat) which automates the procedure below is generated in the same directory as your project file.  This file can then be modified to point to your old BIOS version and then run manually to complete the conversion.  If there happens to be another kind of failure in the automated conversion, then this same script file can be corrected to fix the issue.

Command Line Procedure:

1.     From a command prompt, move to the directory that contains your project’s CDB file.

2.     If you added the %BIOS_INSTALL_DIR%\xdctools directory to your PATH definition, run the cdb2tcf utility as follows:

cdb2tcf <seedpath> <project>.cdb.

For example:

cdb2tcf c:\CCStudio_v3.3\c6000\bios\include hello.cdb.

The <seedpath> should point to the directory containing CDB seed files. That directory is usually c:\CCStudio_v3.3\<ISA>\bios\include, where <ISA> is c6000.

3.     Make sure BIOS_INSTALL_DIR is set as described in the section on Setting System Variables.

4.     The cdb2tcf utility provides messages about the steps it performs. If the original seed file specified inside your CDB file exists in the location specified, the conversion should be successful.

5.     If your configuration made any CSL (Chip Support Library) settings, cdb2tcf generates two files: <project>_csl.c and <project>_csl.h. If these files were generated, follow these steps:

o       Add <project>_csl.c to your project.

o       Add a call to cslCfgInit() to your main() function. The function is in the generated <project>_csl.c file. DSP/BIOS no longer calls this function for you.

o       You may need to modify source files that #include <project>cfg.h to also #include <project>_csl.h. You need only modify files that use CSL configuration structures defined in these two files.

o       If you have device driver code that makes CSL calls, make sure that code calls CSL_init() before calling any other CSL API. Alternately, you may want to create a function that calls CSL_init() and reference that function in your DSP/BIOS configuration by adding the following lines to the Tconf script:

bios.GBL.CALLUSERINITFXN = true;
bios.GBL.USERINITFXN = prog.extern(“your_function_name”);

o       Add the appropriate CSL library for your target to the project or to a linker command file that is separate from the one generated by Tconf (<project>cfg.cmd). For example:

-lcsl6416.lib

o       You may see some CSL related warnings when you build your project. If you see a warning that says “Creating output section .csldata:SYS_data without SECTIONS specification”, you need to add the .csldata section to the memory section of your linker command file. (If you are using the generated linker command file, then you will need to create (and add to your project) your own that includes the BIOS generated linker command file and then adds this .csldata section.)  For example:

SECTIONS {
   .csldata > IDATA
}

o       Add the CSL include directory to your project build’s include path.

o       You are now responsible for managing and updating <project>_csl.c and <project>_csl.h as source files. DSP/BIOS no longer supports configuring CSL. See the CSL documentation for details.

6.     Follow the steps in the next section to add the TCF file to your project and make other project modifications.

Modifying CCStudio Projects to Use TCF Files

For CCStudio 3.3 and newer, your BIOS 5.31 projects must use a TCF file for DSP/BIOS configuration. The previous section tells how to convert a CDB file to a TCF file. To use that file in a CCStudio project that previously used cdb-based BIOS 4.90, follow these steps unless it was already done via the automated procedure.

1.     Open CCStudio and your project. Click OK in the popup box that indicating that it will convert the CDB file. (If you attempt to build without converting, the build procedure attempts to run the CDB file as a TCF file, which generates errors.)

2.     In CCStudio, remove the CDB file from your project.

3.     Add the <project>.tcf file to your CCStudio project.

4.     If you use a custom platform configuration file, you might need to specify the config.importPath. (If you use only TI-supplied platform configuration files, you can skip this step.) For example, if the directory containing your platform configuration file is D:\work\platforms, choose the Project->Build Options menu item in CCStudio. In the DspBiosBuilder tab, select the Basic category and specify the config.importPath as follows: (Note that forward slashes are required.)

    D:/work/platforms

If you have more than one directory containing custom platform configuration files, separate them with semicolons:

    D:/work/platforms;D:/morework/platforms

See the DSP/BIOS Textual Configuration (Tconf) User’s Guide (SPRU007H) for details on defining config.importPath.

5.     If your TCF file requires other parameters or arguments to be passed in, choose Project->Build Options menu item in CCStudio. In the DspBiosBuilder tab, enter the -D<name>=<value> options directly in the top edit box.  For example:
   
-Dconfig.platform = “Dsk6416”

6.     If you are creating a new CCStudio project, in most cases you should add the generated <project>cfg.cmd linker command file to the project. The generated linker command file is not added automatically by CCStudio.    Note: If the generated linker command file is not available, then add the tcf file to the project, right-click and 'compile' the tcf file to generate it.

If, however, your project has its own linker command file, make sure that the <project>cfg.cmd is either not included by your own linker command file or that it is excluded from the project. (That is, make sure it only gets into the project once, rather than twice.) To remove the generated file from the project if your own linker file includes it, right-click the <project>cfg.cmd file in the Generated Files folder of the project view. Select File-Specific Options. Check the Exclude File from Build option.

7.     Run Project->Build.

Makefiles for DSP/BIOS Applications

If you do not use CCStudio to build your application, you can build from the command line using gmake and makefiles.

 

The best way to create build files for your application is to copy and revise the files used to build a DSP/BIOS example. The relevant files for the examples shipped with DSP/BIOS 5.31 are:

·        makefile in a specific example directory

·        config.mak in <install_dir>\bios_5_31\packages\ti\bios\examples\common

·        cNNrules.mak in <install_dir>\bios_5_31\packages\ti\bios\examples\common
   (NN is the DSP family)

 

NOTE: When a single example is copied, it is still using the common directory from the installation.  You must change the makefile and TCF file to reference a different location for the items in common.

 

IMPORTANT: Only use forward slashes (“/”) in all makefiles and files included by makefiles regardless of the OS you are using.

 

Typical things you might need to change in config.mak are:

·        INSTALL_ROOT and COMPONENT_ROOT should point to the location where you installed DSP/BIOS. Currently, they are set to use the BIOS_INSTALL_DIR environment variable.

·        If you want to use a version of RTDX or PSL other than the version provided with the DSP/BIOS installation, change the variable for that component. For example, you might set PSL_ROOT to C:/ti/c5500/psl.

·        The CnnX_CODEGEN_ROOT variable for your DSP platform should point to the location of the codegen tools you want to use. For example, C6X_CODEGEN_ROOT = C:/CCStudio/c6000/cgtools. (If you use multiple operating systems, note that the codegen tools are OS-specific.)

·        If you are using UNIX, comment out the REMOVE definition for Windows and uncomment the corresponding definitions for UNIX.

 

Typical things you might need to change in cNNrules.mak are:

·        Currently all examples are built for debug (-g). To change this, remove the “-g” from the CCNNOPTS line.

·        Change or add any compiler, assembler, or linker options as needed in the definitions of CCNNOPTS, ASNNOPTS, and LDNNOPTS.

 

Typical things you might need to change in the makefile are:

·        COMMON_DIR should point to the location of config.mak and CNNrules.mak.

·        TCONFOPTS should be the –D option for use on the tconf command line. See the instructions for defining the config.importPath for CCStudio and the DSP/BIOS Textual Configuration (Tconf) User’s Guide (SPRU007H).

·        CCNNFLAGS, ASNNFLAGS, and LDNNFLAGS allow you to specify any additional compiler, assembler, and linker flags specific to this application.

For example, to have a map file created for the bigTime example, add “-m bigtime.map” to LD55FLAGS. To build with the C55x large model, first change the configuration in the tcf file, and then add the “-ml” flag to the C55FLAGS and AS55FLAGS definitions in the makefile.

·        PROG, OBJS, and CMDS should reference your source files, object files, and linker command files.

·        If the application uses CSL directly, add the “-i” option to CCNNFLAGS to point to the directory that contains the CSL header files.

 

IMPORTANT: If your application includes CSL header and library files from CCStudio 2.21, 2.3, or 3.0, first copy these files from their DSP/BIOS directory to a corresponding new CSL directory. Then, reference the new directory in the makefile. For example, for ‘C6x CSL header files, copy the <CCStudio_install_dir>\C6000\bios\include\csl*.h files to <CCStudio_install_dir>\C6000\csl\include. For ‘C6x CSL library files, copy the <CCStudio_install_dir>\C6000\bios\lib\csl*.lib files to <CCStudio_install_dir>\C6000\csl\lib.

Running the Tconf Debugger

Tconf comes with the Rhino javascript debugger for use with Tconf scripts.   To invoke the debugger, pass '-g' to Tconf.   Three options are shown:

 

1) CCS Project:  When you are using CCStudio 3.3 or higher, you can launch the debugger when Tconf is invoked from the project, in Project->Build Options, DspBiosBuilder tab, select the 'Debug' Category and change Graphical debugger option from 'none' to 'run the *.tcf in the graphical debugger'.

 

2) Command Line:  Another method for running the debugger is In a command prompt, invoke Tconf with the '-g' option.   For example, here is a sample tconf command line that runs the debugger:

 

    tconf -g -Dconfig.importPath=c:\CCStudio_v3.3\bios_5_31\packages hello.tcf

 

3) Makefile:  If you are building from a makefile, a special build target has been added to makefiles shipped with the bios examples to support using the Tconf debugger. To use this build target, type:

 

gmake .tconfdebug .

 

See the section on modifying CCStudio projects to use Tconf and the DSP/BIOS Textual Configuration (Tconf) User’s Guide (SPRU007H) for information on setting command line arguments for Tconf.

DSP/BIOS Examples

You can use the following sources for example DSP/BIOS applications:

·        DSP/BIOS Examples. A number of DSP/BIOS example applications are provided with this installation in the <install_dir>\bios_5_31\packages\ti\bios\examples directory. The examples have been reorganized into basic and advanced directories and renamed to make them easier to reference. The README file in the top-level examples directory describes the examples. The directory for each example contains a README file that further describes the example and its expected output. The following section tells how to build these examples from the command line.  The CCS tutorial has also been updated to work with these examples.

·        Reference Frameworks. Design-ready, reusable, C language source code for TMS320 'C5000 and 'C6000 DSPs. You can build on top of the framework, confident that the underlying pieces are robust and appropriate for the characteristics of the target application. Levels 1, 3, and 5 support differing application complexity needs. Go to www.dspvillage.com and choose Software->Reference Frameworks from the left-side menus.

·        Application Notes. A number of application notes have been provided about various aspects of DSP/BIOS. Go to www.dspvillage.com and choose Technical Documents->Application Notes. Choose the View by Software tab and select the Real-Time OS – DSP/BIOS item.

·        Device Driver Developer’s Kit. This kit comes with examples of how to develop drivers and how to integrate third-party drivers.

Building Examples from the Command Line

All DSP/BIOS examples can be built with CCStudio with the provided pjt files, but to build the examples provided with DSP/BIOS from the command line, follow these steps. You can use the makefiles for the examples as a basis for creating your own makefiles.

1.     You can copy the entire example tree to a directory with write access, or at a minimum, copy the directory that contains the individual example (see note).

2.     In the ../examples/common directory, edit the "config.mak" file. Make changes as described in the section on building with gmake.

3.     At the command prompt, go to your example directory and the platform of interest. For example:
   cd
E:\BiosWorkarea\examples\basic\bigtime\sim64P

4.     Run gmake.

Note:
To build examples, go to ..\examples and run one of the following:
  gmake –f makefile,6x
  gmake –f makefile,64P  (If using codegen from CCS 3.3)
  gmake –f makefile,67P  (If using codegen from CCS 3.3)
 

Porting Examples to a New Platform

All DSP/BIOS examples come preconfigured for a specific set of platforms, but to build these examples for your own board, follow these steps. You can use the existing board specific configuration files for the examples as a basis for creating your own versions.

1.     Create a custom platform file (Platform.tci) for your board <new_board> by following the steps in the TextConf User's Guide, section 4.3.

2.     Create a <new_board>_common.tci file in the <install_dir>/packages/ti/bios/examples/common directory (see note).  Refer to the README in the examples directory for what goes in this file.

3.     Make a new platform subdirectory for the example you wish to port, i.e. <install_dir>/packages/ti/bios/examples/basic/mailbox/<new_board>.

4.     Copy the makefile and <example>.tcf files from a similar architecture platform for this example to this new platform directory.

5.     Make any necessary changes to the makefile and update the <example>.tcf to reference your new platform created in step 1.

6.     Copy over and update the <example>_<new_board>_custom.tci file if necessary (only needed for a few examples).

7.     Create a CCS project for this example platform or build using the command line with gmake.

How to make one DSP/BIOS installation accessible to multiple CCStudio installations via the BIOS Selector

1.    On a PC with Code Composer Studio installed, map a network drive to the remote network where DSP/BIOS 5.31 is to be installed. Choose a drive letter that can be used on all other PCs with CCS installations that need to access DSP/BIOS 5.31 remotely.

2.    From the PC with the CCStudio installation, install DSP/BIOS 5.31 on the remote drive that you just mapped.

3.    On the remote PC with the DSP/BIOS 5.31 installation, run regedit.

4.    Right click on the key “HKEY_LOCAL_MACHINE\SOFTWARE\Texas Instruments\DBT_<mapped_drive>:|bios_5_31|” and select the “Export” menu item.

5.    Save the selected branch as “bios_5_31.reg”

6.    On a different PC with CCStudio installed, run regedit. Select the menu item “File->Import”, and import the “bios_5_31.reg” that you previously exported.

7.    On the different PC, follow the directions in <bios_5_31 install_dir>\SetupGuide.html, sections “Setting System Variables” and “Coordinating with CCStudio”. When selecting the DSP/BIOS version for CCStudio, select the DSP/BIOS 5.31 that is installed on the remote PC.

8.    For all other PCs that will be running the remote DSP/BIOS 5.31, follow steps 1, 6 and 7.

More Information About DSP/BIOS

See the following documents available with this release and also on www.dspvillage.com to learn about DSP/BIOS:

·        TMS320 DSP/BIOS User’s Guide (SPRU423)

·        TMS320C5000 DSP/BIOS API Reference Guide (SPRU404)

·        TMS320C6000 DSP/BIOS API Reference Guide (SPRU403)

·        DSP/BIOS Textual Configuration (Tconf) User’s Guide (SPRU007H)

·        DSP/BIOS Driver Developer’s Guide (SPRU616)

·        DSP/BIOS online help

·        Release notes

·        Application notes

·        Reference Frameworks

·        DSP/BIOS Link documentation and application notes (for multiprocessor or OMAP applications)

 

 

Copyright © 2006, Texas Instruments Incorporated

 

Code Composer Studio, DSP/BIOS, eXpressDSP, and TMS320 are among the trademarks of Texas Instruments. See www.ti.com for a list of trademarks and registered trademarks belonging to Texas Instruments.