Contact Us     Buy      About TI      TI Worldwide     my.TI  
Texas Instruments
Real World Signal Processing
  Search TI > Advanced Search 
  
  
Update Advisor: DSP Target Content Product Releases

XDAIS Framework Components

XDAIS Framework Components enable faster implementation of application frameworks that use codecs that comply to the TMS320 DSP Algorithm Standard (XDAIS). XDAIS defines standards that prevent codecs from hard-coding ownership of system resources such as memory and DMA channels. An XDAIS-compliant codec must enable the application framework to query it and provide the specific memory and DMA resources it needs. This makes integration of algorithms from multiple sources much easier. The Framework Components include the following three modules:

DSKT2: DSKT2 uses the IALG interface to determine what system memory resources they require and then allocates the memory while instantiating the codec.

DMAN3: DMAN3 uses the IDMA3 interface to determine which DMA resources are required by a codec. DMAN3 includes several enhancements to take full advantage of the DMA (including QDMA and EDMA 3.0) capabilities offered by the 64+ core.

ACPY3: ACPY3 performs fast DMA-based memory-to-memory copies using DMA resources acquired through DMAN. ACPY3 is highly optimized to deliver maximum performance for 64+ devices.

Download Information

Click on the links in the table below if you wish to download or to view more detailed information, including the product release notes. The product release notes and documentation are included in the product installation but are also made available separately here to enable review prior to download.

Note that you will be prompted to accept a license and then send an e-mail when downloading a releases. This e-mail is stored in a list used solely for the purpose of informing you of any patch releases, upgrades, updates, or emergency releases (for problems we regard as especially critical) associated with the release you have downloaded.

To view a detailed list of defects that were fixed in this release, a list of known problems, or to understand which CCS, code generation, and host and target OS versions this version was tested with, please refer to the product release notes.

Framework Components Product Downloads
Version Download Online Docs Features / Device Support
Framework Components 2.24.01 Framework Components 2.24.01 Release Notes See release notes
Framework Components 2.24 Framework Components 2.24 Release Notes See release notes
Framework Components 2.23.01 Framework Components 2.23.01 Release Notes See release notes
Framework Components 2.22.01 Framework Components 2.22.01 Release Notes New Features & device support: See release notes
Framework Components 2.21 Framework Components 2.21 Release Notes New Features & device support: See release notes
Framework Components 2.20.01 Framework Components 2.20.01 Release Notes New Features & device support: See release notes
Framework Components 2.20 Framework Components 2.20 Release Notes New Features & device support: See release notes
Framework Components 2.10.02 Framework Components 2.10.02 Release Notes New Features & device support: See release notes
Framework Components 2.10.01 Framework Components 2.10.01 Release Notes New Features & device support: See release notes
Framework Components 2.10 Framework Components 2.10 Release Notes New Features & device support: See release notes
Framework Components 2.00.01 Framework Components 2.00.01 Release Notes New Features & device support: See release notes
Framework Components 2.00 Framework Components 2.00 Release Notes New Features & device support: See release notes
Framework Components 1.20.03 Framework Components 1.20.03 Release Notes New Features: DSKT2 critical bug fix

Device Support: 64x+, 55x

Framework Components 1.20.02
Framework Components 1.20.02 Release Notes New Features: Defect fixes and new DSKT2 user manual

Device Support: 64x+, 55x
Framework Components 1.10.04 Framework Components 1.10.04 Release Notes New Features: DSKT2 critical bug fix

Device Support: 64x+, 55x

Framework Components 1.10.01
Framework Components 1.10.01
Release Notes
New Features: DMAN3 and EDMA3 usage application note

Device Support: 64x+, 55x
Framework Components 1.02 Framework Components 1.02
Release Notes
Device Support: 64x+ only
Framework Components 1.00.01 Framework Components 1.00 Release Notes

Device Support: 64x+

For additional information, contact support@ti.com

 
Products  |  Applications  |  Support  |  Site Map
© Copyright 1995-2009 Texas Instruments Incorporated. All rights reserved. Trademarks  |  Privacy Policy  |  Terms of Use