Engine.h File Reference


Detailed Description

The Codec Engine Runtime. Provides the user an inteface to open and manipulate an engine which can instantiate and communicate with xDAIS algorithms that run either on the local CPU or on a "remote" DSP Server.

#include <ti/sdo/ce/Server.h>
#include <ti/sdo/ce/ipc/Comm.h>
#include <ti/xdais/ialg.h>
#include <ti/sdo/ce/node/node.h>
#include <stddef.h>
#include <stdio.h>

Include dependency graph for Engine.h:

This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  Engine_Attrs
 Attributes of an Engine. More...
struct  Engine_AlgInfo
 Properties of an Engine algorithm. More...

Defines

#define Engine_GTNAME   "CE"
 Trace name for the Engine module.
#define Engine_EOK   0
#define Engine_EEXIST   1
#define Engine_ENOMEM   2
#define Engine_EDSPLOAD   3
#define Engine_ENOCOMM   4
#define Engine_ENOSERVER   5
#define Engine_ECOMALLOC   6
#define Engine_ERUNTIME   7
#define Engine_ECODECCREATE   8
#define Engine_ECODECSTART   9
#define Engine_EINVAL   10
#define Engine_EBADSERVER   11
#define Engine_ENOTAVAIL   12
#define Engine_EWRONGSTATE   13
#define Engine_EINUSE   14
#define Engine_ENOTFOUND   15
#define Engine_ETIMEOUT   16

Typedefs

typedef Engine_Obj * Engine_Handle
 Opaque handle to an engine.
typedef Int Engine_Error
 Engine error code.

Functions

Void Engine_close (Engine_Handle engine)
 Close an Engine.
Engine_Handle Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec)
 Open an Engine.
Int Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out)
 Write Server's trace buffer to specifed file stream.
Engine_Error Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index)
 Get details of an algorithm configured into an engine.
Int Engine_getCpuLoad (Engine_Handle engine)
 Get Server's cpu usage in percent.
Engine_Error Engine_getLastError (Engine_Handle engine)
 Get error code of the last failed operation.
Engine_Error Engine_getNumAlgs (String name, Int *numAlgs)
 Get the number of algorithms configured into an engine.
Server_Handle Engine_getServer (Engine_Handle engine)
 Get handle to an Engine's server.
UInt32 Engine_getUsedMem (Engine_Handle engine)
 Get Server's total memory usage.
Int Engine_setTrace (Engine_Handle engine, String mask)
 Set Server's trace mask.

Variables

Engine_Attrs Engine_ATTRS
 Default engine attributes.


Copyright 2008, Texas Instruments Incorporated