Quick Start Guide¶
Introduction¶
This guide is intended to assist users in the initial setup and demonstration of a CC32XX Azure IoT application using the CC32XX Plugin for Azure IoT, which augments the Azure IoT C SDK by providing support on TI CC32XX devices. The guide explains how to configure the boards, compile the software artifacts, program the CC32XX device, set up your Azure account and run an Azure application.
Hardware Requirements¶
One of the following LaunchPads:
Software Requirements¶
- SimpleLink CC32XX SDK 4.10
- A computer running a supported operating system listed in the Release Notes
- At least one of the following IDEs supported by the SimpleLink CC32XX SDK:
- Uniflash Tool 5.3.1 or compatible for flashing the application binary and the service pack
- FreeRTOSv10.2.1 (Optional)
- If the User wants to use FreeRTOS with the Plugin, the user is expected to download the FreeRTOS sources from www.freertos.org
Installing CC32XX Plugin for Azure IoT¶
- Download and open the CC32XX Plugin for Azure IoT Installer (replace x’s with version number):
- Windows: azure_cc32xx_x_xx_xx_xx.exe
- Linux: azure_cc32xx_x_xx_xx_xx.run
- macOS: azure_cc32xx_x_xx_xx_xx.app
- Select an installation directory. This will be referred to as
<AZURE_INSTALL_DIR>in the rest of this document. It’s recommended that you install it in your CCS installation directory (defaultC:\tion Windows) so it can be discovered automatically - Click Next > and finish the installation
Hardware Setup¶
Jumper Settings¶
The CC32XX device implements a sense-on-power scheme to determine the device operation mode upon power up. The encoding of these pins determines the boot flow and the default mapping for some of the pins (UART, JTAG, etc.) The SOP pins are connected to jumper J13 on the CC32XX LaunchPad, which is shipped in flash and functional mode (010) as shown in the image below.
SOP[2…0] mode (100) is used for programming the serial flash with the application binary and/or the service pack. After flashing, the board should be reset and the mode set to (000) (no jumpers in place) to run/execute the contents of flash
SOP[2…0] mode (010) is the flash and execute mode which is similar to the (100) mode except that after flashing, the contents of flash are executed immediately without having to reset or remove all jumpers. This mode is also used when using CCS (or IAR) to connect to the device for loading and debugging
Setting Up a Serial Terminal¶
Plug the CC32XX LaunchPad into a USB port on your PC.
Open a serial session to the appropriate COM port with the following settings:
Baudrate: 115200 Data bits: 8 Stop bits: 1 Parity: None Flow Control: None
The output of the examples will be displayed in the terminal.
Azure IoT Developer Setup¶
In order to run the example applications, it is necessary to complete the following steps:
Building and Running Examples in CCS¶
Several examples are provided in the Plugin and can be found in the examples/ subdirectory.
These steps refer to the simplesample_http application for the CC3220SF device, but the same procedure applies to any CC32XX device and to other examples as well.
It is assumed that the SimpleLink CC32XX SDK has already been installed in a directory we will refer to as
<SIMPLELINK_CC32XX_SDK_INSTALL_DIR>. You should install it if you have not already done so, as the CC32XX Plugin for Azure IoT depends on the CC32XX SDK.Open Code Composer Studio (close and re-open if already running before Plugin or SDK installation).
In CCS, import the
simplesample_httpexample by first selecting Project > Import CCS Projects…In the Import CCS Projects window, hit the browse button to browse to the location corresponding to
<AZURE_INSTALL_DIR>\examples. Select the checkbox next to thesimplesample_httpexample for tirtos (or freertos) for CCS and hit the Finish button.
Two projects should appear in the Project Explorer tab in CCS: one for the
simplesample_httpexample itself (i.e.simplesample_http_CC3220SF_LAUNCHXL_tirtos_ccs), and the other is a project corresponding to the OS chosen (e.g.tirtos_builds_CC3220SF_LAUNCHXL_release_ccs).The example comes with a README.html file that contains more details specific to the example. Be sure to take a look as it may contain additional instructions.
Update the example to use your Azure connection string and WiFi Access Point information, as specified in the section Example Pre-Build Steps
If you are using FreeRTOS, you need to set the installation directory of FreeRTOS before building:
- In CCS, select Window > Preferences
- Navigate to Code Composer Studio > Build > Variables
- Click Add
- For Variable name, enter
FREERTOS_INSTALL_DIR - For Type, select directory
- For Value, enter the installation directory of FreeRTOS
- Hit OK until you get back to the main window in CCS
Right-click on the
simplesample_httpproject, and select Build Project to build.
Load and Run the Example¶
- Plug the LaunchPad into a USB port on your PC.
- Right-click on the
simplesample_httpproject, and select Debug As > Code Composer Debug Session. Note the SOP[2..0] jumper setting on the board must be (010) in order for the CCS debugger to connect. - Run the application by pressing F8. The output will appear in your serial terminal session.
Example Output¶
```
Starting the simplesample_http example
Current time: Mon Jul 23 23:52:04 2018
CC32XX has connected to AP and acquired an IP address.
IP Address: 192.168.1.128
Flashing certificate file ...successfully wrote file /cert/ms.pem to flash
IoTHubClient accepted the message for delivery
Message Id: 1 Received.
Result Call Back Called! Result is: IOTHUB_CLIENT_CONFIRMATION_OK
```
Building and Running Examples in IAR¶
Download and Installation¶
For instructions on downloading and setting up IAR properly for use with the SimpleLink CC32XX SDK and its Plugins, please refer to the CC32XX SDK’s Quick Start Guide document. As part of the procedure, make sure to configure the custom argument variables for the SDK.
Configuring Custom Argument Variables Specific to the Plugin¶
Before starting to work with any of the Azure IoT example projects in the Plugin, you need to load a set of environment variables that will be set for your current workspace, in addition to the ones from the SimpleLink SDK.
The custom argvars can be found at
<AZURE_INSTALL_DIR>/tools/iar/AZURE_CC32XX_SDK.custom_argvars, if you need to modify the default path argument variables, edit the variables with the correct path.Open the IAR IDE
Choose Tools > Configure Custom Argument Variables
Click Global > Import
Browse to
<AZURE_INSTALL_DIR>/tools/iar. Import the custom argvars from the Plugin.
Importing Your First Project¶
These steps refer to the simplesample_http application for the CC3220SF device, but the same procedure applies to any CC32XX device and to other examples as well.
You can choose to open an Example Project by either directly accessing the Example workspace (by double clicking on its *.eww file), or by importing the Example from the Example List in the IDE.
Directly Accessing an Example From the Example Folder¶
All Code Examples that are shipped with the plugin come with an IAR workspace (*.eww file). Double-Clicking the specific workspace allows you to open the project on disk and build it.
Each example comes with a README.html file. Be sure to take a look in case it has additional instruction specific to the example you wish to run. Update the example to use your Azure connection string and WiFi Access Point information, as specified in the section Example Pre-Build Steps
Importing an Example in the Example List¶
In the IAR-IDE, select File > Open File… from the menu and open
<AZURE_INSTALL_DIR>/tools/iar/Examples.htmlAll the Plugin for Azure IoT example projects that are available in IAR are listed in the html page.
Scroll through the page and click on the project you are interested in. In this guide we choose to work with
simplesample_httpfor the CC3220SF based on TI-RTOS.
When prompted, click
Yesto save a copy of the project workspace in a specific folder,Nowill save the workspace in a default folder.After clicking
Yes, browse to the location where you want to save this workspace. ClickChoose
Building the Project¶
- Two projects should appear in the Workspace tab in IAR: one for the
simplesample_httpexample itself (i.e.simplesample_http_CC3220SF_LAUNCHXL_tirtos_iar), and the other is a project corresponding to the OS chosen (e.g.tirtos_builds_CC3220SF_LAUNCHXL_release). - The example comes with a README.html file that contains more details specific to the example. Be sure to take a look as it may contain additional instructions.
- Update the example to use your Azure connection string and WiFi Access Point information, as specified in the section Example Pre-Build Steps
- Make/Build the Example Project by first selecting the OS project tab on the Workspace window and select Project > Make. Once done, select the
simplesample_httptab on the Workspace window and select Project > Make.
Start a Debug Session¶
To start an IAR debug session follow the steps outlined in the Run a debug session section in the QuickStart for IAR IDE chapter of the CC32XX SDK’s Quick Start Guide document.
Load and Run the Example¶
- Plug the LaunchPad into a USB port on your PC.
- Select Project > Download and Debug Note the SOP[2..0] jumper setting on the board must be (010) in order for the IAR debugger to connect.
- Run the application by pressing F5.
- The Example output is displayed in the serial terminal, as shown here.
Building with Makefiles¶
These steps refer to the simplesample_http application, but the same procedure applies to other examples as well.
- It is assumed that the SimpleLink CC32XX SDK has already been installed in a directory we will refer to as
<SIMPLELINK_CC32XX_SDK_INSTALL_DIR>. You should install it if you have not already done so, as the CC32XX Plugin for Azure IoT depends on the CC32XX SDK. - Update the
imports.makfile in the<AZURE_INSTALL_DIR>root folder with the appropriate path(s). This file relies on the settings in theimports.makfile of the SimpleLink CC32XX SDK, so please ensure you have updated the latter with the appropriate paths as well if you have not done so previously. - Navigate to the directory corresponding to your OS, board and toolchain of choice. For example,
<SIMPLELINK_CC32XX_SDK_INSTALL_DIR>/kernel/tirtos/builds/CC3220SF_LAUNCHXL/release/ccsfor tirtos and TI (CCS) toolchain on the CC3220SF LaunchPad. - Run ‘make’ to build the OS. If you develop on a Windows machine and do not have the ‘make’ utility, you can alternatively run ‘gmake’ from your TI XDCTOOLS installation (e.g.
C:\ti\xdctools_x_xx_xx_xx_core\gmake.exe). Normally XDCTOOLS are installed along with the CC32XX SDK, but if you need to download it, it is available here. - Navigate to the example folder specific to your board(replace
CC3220SF_LAUNCHXLwith your board name):<AZURE_INSTALL_DIR>/examples/rtos/CC3220SF_LAUNCHXL/azure/simplesample_http - Read the README.html file of the example, and follow any additional instructions specific to the example if present.
- Update the example to use your Azure connection string and WiFi Access Point information, as specified in the section Example Pre-Build Steps
- Navigate to the example folder specific to your OS and toolchain
<AZURE_INSTALL_DIR>/examples/rtos/CC3220SF_LAUNCHXL/azure/simplesample_http/tirtos/ccs - To build, run ‘make’ to generate
simplesample_http.out - You can load and debug the generated
simplesample_http.outin CCS (or IAR) - The Example output is displayed in the serial terminal, as shown here.
Building the Azure PAL and SDK Libraries¶
The libraries for the Azure Platform Adaptation Layer (PAL) and the Azure IoT C SDK are shipped pre-built as part of the plugin. If for some reason, you would like to rebuild them, follow these steps:
Fill out
imports.makfile from the CC32XX SDK with the paths to your XDC tools installation (XDC_INSTALL_DIR) and the compiler toolchain(s) of your choice. Leave empty the*_ARMCOMPILERvariables for the toolchains you don’t wish to build for.Update the
imports.makfile in the<AZURE_INSTALL_DIR>root folder with the appropriate path(s)Open a Windows command prompt or Linux terminal.
In the terminal window, run the following commands (be sure to replace
<AZURE_INSTALL_DIR>with your installation path, and usegmake.exefrom your XDC tools installation in<XDC_INSTALL_DIR>instead ofmakeif you are a Windows user).cd <AZURE_INSTALL_DIR>\source\third_party\azure-iot-pal-simplelink\build_all make clean make all
Viewing Data from the Cloud¶
You can view the data that has been received on the cloud side in various ways, for example using the Device Explorer or the iothub-explorer from Microsoft, or creating an Azure Function App on the Azure portal itself. Please refer to online documentation from Microsoft to learn about the various ways to interact with the IoT Hub.
Example Pre-Build Steps¶
Before building a specific application, you must complete the following steps in order to successfully connect to Azure (these steps refer to the simplesample_http application, but the same procedure applies to other examples as well):
Update the Example with Your Wi-Fi Access Point Information¶
Open the file wificonfig.h, found in the simplesample_http project. Search for “USER STEP” and update the Wi-Fi SSID and SECURITY_KEY macros.
Update the Azure Connection String¶
Open the file simplesample_http.c in a text editor and replace the value of the “connectionString” variable with the device connection string you noted when you registered your device with the IoT hub. (Other examples similarly have a source file named <example_name>.c or NetMgr.c where the connection string can be set.)
This step does not apply to the examples that use the Device Provisioning Service (DPS), which obtains the device credentials through a registration process.
Update the Service Pack¶
To update the CC32XX’s service pack complete the sections titled Launching ImageCreator from UniFlash, Creating a New Project and Adding the Latest Service Pack from UniFlash ImageCreator Basics.
Update the Certificate Catalog¶
In order for the Azure examples to run successfully the CC32XX must be updated with a certificate catalog that contains the Baltimore CyberTrust Root CA (i.e. NOT the default playground catalog). When connecting securely using TLS with Azure servers, this root CA is validated against the certificate catalog, and a connection error would result if the catalog does not contain this particular root CA. To do this complete the section titled Changing the Trusted Root-Certificate Catalog from UniFlash ImageCreator Basics to flash the Certificate Catalog found in <SIMPLELINK_CC32XX_SDK_INSTALL_DIR>/tools/cc32xx_tools/certificate-catalog/.
Flash the Root Certificate¶
Note: In the examples, the root CA certificate - “Baltimore CyberTrust Root” is flashed to the location/cert/ms.pem. This location must matchSL_SSL_CA_CERTin<AZURE_INSTALL_DIR>\source\third_party\azure-iot-pal-simplelink\pal\inc\cert_sl.h, and has been setup correctly for you by default.
The Baltimore root CA certificate is needed as it’s the root CA for *.azure-devices.net, the IoT Hub endpoint, and it’s the only way for the device to verify the chain of trust.
The default behavior of the example is to automatically write the certificate to flash if it does not exist. This prevents the file from being written unnecessarily to the file system each time the program is run. If you wish to override this behavior, or if you wish to use a new certificate file, you can force the certificate to be flashed by passing “-DOVERWRITE_CERTS” to the compiler in the makefile. Otherwise it is best to not change anything here.