SimpleLink CC32XX SDK Azure IoT Plugin 3.30.00.02 Release Notes
Table of Contents
Introduction
The Azure IoT Plugin enables users to create Azure IoT applications. It includes the necessary Azure IoT sources, as well as documentation and examples.
Documentation
The following documentation is provided with this release.
What’s New
3.30.00.02
Defects
The following Defects were resolved
ID | Summary |
---|---|
None | None |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
AZUREIOT-59 | Support the SimpleLink 3.30 (Q3 2019) SDKs |
AZUREIOT-35 | Add sysconfig support to examples |
Upgrade and Compatibility Information
Example/SysConfig Updates
All examples in this release have been updated to use SysConfig. SysConfig generates .c and .h files with the various configuration data structures and constants. These files were previously written by hand. Check the SimpleLink SDK’s User’s Guide for more information about SysConfig.
Here is a short summary of the changes to each example:
Previous Release | This release |
---|---|
Hand written files with #defines and C structures | example.syscfg (generates files with #defines and C structures) |
Board.h, CCXXXX_LAUNCHXL.h | ti_drivers_config.h |
CCXXXX_LAUNCHXL.c | ti_drivers_config.c |
#defines are named Board_GPIO_LED0, etc. | #defines are named CONFIG_GPIO_LED_0, etc. |
pin settings common to all examples are shown in Board.html | pin settings unique to each example are commented in ti_drivers_config.h |
See the SimpleLink CC32XX SDK documentation for its compatibility breaks.
Host Support
- Windows
- macOS
- Linux
Dependencies
This release requires the following software components and tools versions to successfully function:
- CC32XX SDK 3.30.00.04
See the CC32XX SDK documentation for IDE and toolchain dependencies
Device Support
This release supports the following devices:
- CC3220S
- CC3220SF
- CC3235S
- CC3235SF
Validation Information
This release was validated using the following software components. Please use the versions below, or compatible:
- CC32XX SDK 3.30.00.04
- Azure IoT PAL: git reference azure-iot-pal-simplelink-3.30.00.02 in repository https://github.com/TexasInstruments/azure-iot-pal-simplelink
- Microsoft Azure IoT C SDK: git reference b03cc5e0afb647934e45d4530d3e993476db3d3e from branch lts_07_2019 in repository https://github.com/Azure/azure-iot-sdk-c
Known Issues
- All examples that call printf() send their output to the IDE console window, hence cannot be run independently without the IDE (unless these printf() calls are removed).
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases. Pre-releases are denoted with a suffix (e.g. 1.00.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. azure_cc32xx_3_30_00_02.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Last updated: 2019-10-25