SimpleLink CC32XX SDK Azure IoT Plugin 2.20.00.05 Release Notes
Table of Contents
Introduction
The Azure IoT Plugin enables users to create Azure IoT applications. It includes the necessary Azure IoT sources, as well as documentation and examples.
Documentation
The following documentation is provided with this release.
What’s New
2.20.00.05
Defects
The following Defects were resolved
ID | Summary |
---|---|
AZUREIOT-49 | Setting x509 certificates using IoTHubClient_LL_SetOption() results in unauthorized connection |
AZUREIOT-46 | Build warnings in prov_dev_client_ll_sample for GCC + TIRTOS |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
AZUREIOT-44 | Support the SimpleLink 2.40 (Q4 2018) SDKs |
AZUREIOT-37 | Add support for CC3235 |
Upgrade and Compatibility Information
See the CC32XX SDK documentation for compatibility breaks.
In this release, there is a change in the certificate file that contains the certificate used for connecting to Azure. If you have run examples from previous releases of the plugin, please use TI Uniflash to delete the old ms.pem file from the cert/ directory on the device’s filesystem (Select Advanced -> Connect -> Online User Files after picking your device in Uniflash to interact with the filesystem). When you run examples from this new plugin release, they would automatically flash the new file if the old one had been removed.
Some examples would fail during their TLS connection if the old file remains in place.
Host Support
- Windows
- Linux
Dependencies
This release requires the following software components and tools versions to successfully function:
- CC32XX SDK 2.40.01.01
See the CC32XX SDK documentation for IDE and toolchain dependencies
Device Support
This release supports the following devices:
- CC3220
- CC3235
Validation Information
This release was validated using the following software components. Please use the versions below, or compatible:
- CC32XX SDK 2.40.01.01
- Azure IoT PAL: git reference azure-iot-pal-simplelink-2.20.00.05 in repository https://github.com/TexasInstruments/azure-iot-pal-simplelink
- Microsoft Azure IoT C SDK: git reference abacd2311a1b6d9fabc0743acf494d418fac8a30 from branch lts_10_2018 in repository https://github.com/Azure/azure-iot-sdk-c
Known Issues
- All examples that call printf() send their output to the IDE console window, hence cannot be run independently without the IDE (unless these printf() calls are removed).
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases. Pre-releases are denoted with a suffix (e.g. 1.00.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
To support multiple side-by-side installations of the product, the product version is encoded in the top level directory, ex. azure_cc32xx_2_20_00_05.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Last updated: 2019-03-05