Azure IoT Plugin Change Log
Table of Contents
2.10
New Features
Bugs Resolved
2.00
New Features
AZUREIOT-21 |
Support the SimpleLink 2.20 (Q2 2018) SDKs |
AZUREIOT-19 |
Update to Jan 2018 LTS release |
AZUREIOT-16 |
add support for X509 authentication |
AZUREIOT-12 |
Add MSP432E4 support |
AZUREIOT-6 |
Add FreeRTOS support |
Bugs Resolved
AZUREIOT-25 |
printf() output should follow toolchain behavior rather than build on UARTUtils |
AZUREIOT-17 |
Memory leak in tlsio_sl_destroy() in tlsio_sl.c |
AZUREIOT-15 |
Examples should honor user configured SECURITY_TYPE |
AZUREIOT-13 |
HTTPAPI_CreateConnection() can cause memory corruption on server connection failures |
AZUREIOT-8 |
Remove .git files in azure-iot-sdk-c created by git submodule cloning |
Compatibility Notes
This release uses a new directory structure for the Platform Adaptation Layer (PAL) so that it is cleanly separated from the rest of the Microsoft Azure IoT C SDK. This makes it easier to distinguish TI-modified content in the PAL versus the code directly obtained from Microsoft, which is helpful when updating the latter.