Users Guide
Table of Contents
Introduction
The CC3220 Azure IoT Plugin is a companion software package that enables development of Azure IoT applications on TI’s CC3220 SimpleLink platform.
SimpleLink Plugins are designed to work in tandem with the microprocessor specific SimpleLink SDKs. This Plugin is designed to work alongside the SimpleLink CC3220 SDK and relies heavily on several core elements within this SDK. Without a prior installation of the SimpleLink CC3220 SDK, this Plugin will not work. Be sure to review and become familiar with the SimpleLink CC3220 SDK’s documentation, and all those features apply when using this Plugin.
This Plugin also assumes a general familiarity with the Azure IoT ecosystem. Be sure to consult that documentation as well.
Documentation and Support
Links to documentation for this Plugin and the Components it includes are provided in the Documentation Overview.
This Plugin is supported on the TI E2E Community.
Examples
The Azure IoT Plugin contains several examples. Each example contains its own README.
Importing, Building and Running the Examples
Refer to the Quick Start Guide for detailed instructions on importing, building and running the examples.