Platform Support Package (PSP) Software Manifest


Legend

Package Name

The name of the application or files

Version

Version of the application or files

License

Name of the license or licenses that apply to the Package.

Location

The directory name and path on the media (or in an archive) where the Package is located.

Delivered As

This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in.  If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided.

Modified

This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes.

Obtained from[1]

This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded.

  

Manifest

Note: Replace MM.mm.pp.bb in the directory path below with the PSP release version you are using.

Package Name

Version

License

Delivered As

Modified

 

ARM NOR/NAND/SPI User Boot Loader    

 NA 

GPLv2

Source and Binary

NA

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/boot-strap/armubl 

 

DA850/OMAP-L138/AM18xx Pre-built binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x8/arm-nand-ais.bin

DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x8/arm-spi-ais.bin and DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x8/arm-nor-ais.bin

 

DA830/OMAP-L137 Pre-built binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x7/ubl-nand.bin

DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x7/ubl-spi.bin 

 

AM17xx Pre-built binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/am17xx/arm-nand-ais.bin

DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/am17xx/arm-spi-ais.bin

Obtained from[1]

TI

DSP NAND/SPI User Boot Loader

NA

GPLv2

Source and Binary

NA

Location

 

 

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/boot-strap/dspubl 

 

DA830/OMAP-L137 Pre-built binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x7/dsp-nand-ais.bin

DaVinci-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omapl1x7/dsp-spi-ais.bin

Obtained from[1]

TI

SPI Flash Writer  

 NA   

GPLv2

Source and Binary

YES

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/utils/spiflash_writer

 

DA830/OMAP-L137/AM17xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/utils/omapl1x7/spiflash_writer.out

 

DA850/OMAP-L138/AM18xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/utils/omapl1x8/spiflash-writer.out

Obtained from[1]

SPI flash code in U-Boot obtained from  http://git.denx.de/?p=u-boot.git;a=summary.

Commit ID 3d1c46b2efcf4c56226d6bc5b8a3c2372e7ab517.

NAND Flash Writer   

 NA

GPLv2    

Source and Binary

NA

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/utils/nand_writer.

 

DA830/OMAP-L137/AM17xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/utils/omapl1x7/nand_writer.out

 

DA850/OMAP-L138/AM18xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/utils/omapl1x8/nand-writer.out

Obtained from[1]

TI

NOR Flash Writer   

 NA

GPLv2    

Source and Binary

NA

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/utils/norflash_writer.

 

DA850/OMAP-L138/AM18xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/utils/omapl1x8/norflash-writer.out

Obtained from[1]

TI

 U-Boot  

 2009.11

 GPLv2

Source and Binary

YES

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/u-boot

 

DA830/OMAP-L137/AM17xx SPI Boot mode Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/u-boot/omapl1x7/u-boot.bin

 

DA850/OMAP-L138/AM18xx SPI Boot mode Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/u-boot/omapl1x8/u-boot.bin

Obtained from[1]

U-Boot 2009.11 obtained from http://git.denx.de/?p=u-boot.git;a=commit;

h=bb3bcfa2426cc6a0aecec7270e3ee67ca843a125.

Video Sample Code

 NA

 BSD

Source and binary

NA

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/examples/examples.tar.gz

 

Binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/vpif_test_display, DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/vpif_test_mmap_loopback and

DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/vpif_test_userptr_loopback

Obtained from[1]

TI

GPIO/EDMA/McBSP Sample Code

 NA

 GPLv2

Source and binary

NA

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/src/examples/examples.tar.gz

 

Binaries at DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/edma_test.ko, DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/gpio_test.ko and

DaVinci-PSP-SDK-MM.mm.pp.bb/images/examples/mcbsp_test.ko

Linux Functional Testbench(LFTB)

01.00.00.13

TI  New BSD (user space) & GPLV2 for kernel space

Source and Binary

NA

Location

Source at DaVinci-PSP-SDK-MM.mm.pp.bb/test-suite

Obtained from[1]

TI

Open source Linux (based on DaVinci GIT)

 2.6.33-rc4

 GPLv2

Source and Binary

YES

Location

Source at  DaVinci-PSP-SDK-MM.mm.pp.bb/src/kernel  

 

DA830/OMAP-L137/AM17xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/kernel/omapl1x7/uImage

 

DA850/OMAP-L138/AM18xx Binary at DaVinci-PSP-SDK-MM.mm.pp.bb/images/kernel/omapl1x8/uImage

Obtained from[1]

Linux 2.6.33-rc4 obtained from http://git.kernel.org/?p=linux/kernel/git/khilman/linux-davinci.git;a=commit;

h=887f8d18de5efbeafc76e5c509fd53f9018992fa.

 


[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.