Build System¶
Building the Applications From Source¶
There are various ways to build the applications in the TI 15.4-Stack Linux SDK Installer.
Using Top-Level Script¶
The script file build_all.sh can be used to build all the example
applications. Table 4. lists the available options and
their effect when using this script.
| Options | Description |
|---|---|
| $bash ./build_all.sh clean | Delete all compiled object and executable files |
| $bash ./build_all.sh | Builds for host machine |
| $bash ./build_all.sh host | Builds for host machine |
| $bash ./build_all.sh bbb | Builds for BBB (when building from the x86 machine requires the BBB cross-compiler, as mentioned in Linux® Development Host) |
| $bash ./build_all.sh remake | Delete all compiled object and executable files and then build for the host machine |
Using the Makefile Within Each Directory¶
Each component (library or application) directory contains a makefile to build that component.
Change to the specific directory (either application or library).
Type make.
Table 5. lists the general targets supported by each makefile.
| Options | Description |
|---|---|
| bash$ make | Builds the host |
| bash$ make host | Builds the host |
| bash$ make bbb | Builds the BBB variant |
| bash$ make clean | Removes all generated files |
| bash$ make remake | Make clean followed by make |
Makefile System¶
Note
The cc13xx-sbl (bootloader) is a simple self-contained application that uses one self- contained makefile. The cc13xx-sbl does not use the fragment-based system described in the discussion that follows.
Generally, there are two types of builds:
- A static library
- An application
The makefile method used in the example application is a makefile-fragment scheme. There are three parts to this fragment-based system:
- The primary Makefile (located with the source code [typically in a parent directory])
- The front_matter.mak make-fragment (in the scripts directory)
- The app.mak or library.mak make-fragment (in the scripts directory)
The various components are shown in Figure 19. and discussed in more detail in the rest of this chapter. In Figure 19., the outer box represents an example makefile and the inner shaded boxes represent the fragments.
Figure 19. Makefile Structure
Primary Makefile¶
The primary makefile is at the top level of each item (that is, the top directory of a library, or an application). The top portion of the Makefile does the following:
- Set a pseudo default target, typically named _default
- Set various ${CFLAGS}
- Include the ${scripts}/front_matter.mak
Included ${scripts}/front_matter.mak¶
The included ${scripts}/front_matter.mak file is in the following:
${root}/scripts/front_matter.mak
This is a common-boiler-plate file that determines the following:
- The key variable${ARCH} specifies the type of build (host or BBB).
- The various compile (transformation) rules are listed.
- The compiler-generated dependency files are created and included.
Makefile (Between the Includes)¶
The makefile (between the includes) is not a separate file; it is the portion of the original makefile between the two include statements. In this section, the following items are listed:
- Source Files, that is ${C_SOURCES}
- Libraries that are used
- Any additional required rules (for example, using the protobuf compiler)
Included ${scripts}/library.mak or ${scripts}/app.mak¶
This file is either ${root}/scripts/library.mak or ${root}/scripts/app.mak These files do one of the following:
- Create the library
- Create the executable
Makefile (Final Portion)¶
The makefile (final portion) is not a separate file but is the final portion of the makefile after the include statements. The final portion contains a directory, an application, or library-specific rules.