This section provides information on the OSPI Module Instance within this product. Each of the registers within the Module Instance is described separately below.
|
Register Name |
Type |
Register Width (Bits) |
Register Reset |
Address Offset |
|
RW |
32 |
0x8208 0081 |
0x0000 0000 |
|
|
RW |
32 |
0x0000 0003 |
0x0000 0004 |
|
|
RW |
32 |
0x0000 0002 |
0x0000 0008 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 000C |
|
|
RW |
32 |
0x0000 0001 |
0x0000 0010 |
|
|
RW |
32 |
0x0010 1002 |
0x0000 0014 |
|
|
RW |
32 |
0x0000 0080 |
0x0000 0018 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 001C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0020 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0024 |
|
|
RW |
32 |
0x0000 0200 |
0x0000 0028 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 002C |
|
|
RW |
32 |
0x0000 0001 |
0x0000 0030 |
|
|
RW |
32 |
0x0000 0001 |
0x0000 0034 |
|
|
RW |
32 |
0x0004 0005 |
0x0000 0038 |
|
|
RW |
32 |
0xFFFF FFFF |
0x0000 003C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0040 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0044 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0050 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0054 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0058 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0060 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0064 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0068 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 006C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0070 |
|
|
RW |
32 |
0xFFFF FFFF |
0x0000 0074 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0078 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 007C |
|
|
RW |
32 |
0x0000 0004 |
0x0000 0080 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 008C |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0090 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 0094 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00A0 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00A4 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 00A8 |
|
|
RW |
32 |
0x0000 0000 |
0x0000 00AC |
|
|
RW |
32 |
0x0000 0000 |
0x0000 00B0 |
|
|
RW |
32 |
0x4000 0000 |
0x0000 00B4 |
|
|
RW |
32 |
0x0080 0000 |
0x0000 00B8 |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00BC |
|
|
RO |
32 |
0x0000 0000 |
0x0000 00C0 |
|
|
RW |
32 |
0x13ED FA00 |
0x0000 00E0 |
|
|
RW |
32 |
0x06F9 0000 |
0x0000 00E4 |
|
|
RO |
32 |
0x0400 0300 |
0x0000 00FC |
|
Address offset |
0x0000 0000 |
||
|
Description |
Octal-SPI Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31 |
IDLE |
Serial interface and low level SPI pipeline is IDLE: This is a STAUS read-only bit. Note this is a retimed signal, so there will be some inherent delay on the generation of this status signal. |
RO |
1 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
30 |
DUAL_BYTE_OPCODE_EN |
Dual-byte Opcode Mode enable bit This bit is to be set in case the target Flash Device supports dual byte opcode (i.e. Macronix MX25). It is applicable for Octal I/O Mode or Protocol only so should be set back to low if the device is configured to work in another SPI Mode. If enabled, the supplementing bytes are taken from Opcode Extension Register (Lower) and from Opcode Extension Register (Upper). |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
29 |
CRC_EN |
CRC enable bit This bit is to be set in case the target Flash Device supports CRC (Macronix MX25). It is applicable for Octal DDR Protocol only so should be set back to low if the device is configured to work in another SPI Mode. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
28:26 |
RESERVED |
|
RO |
0x0 |
||
|
25 |
PIPELINE_PHY |
Pipeline PHY Mode enable: This bit is relevant only for configuration with PHY Module. It should be asserted to '1' between consecutive PHY pipeline reads transfers and de-asserted to '0' otherwise. |
RW |
1 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
24 |
EN_DTR_PROTOCOL |
Enable DTR Protocol: This bit should be set if device is configured to work in DTR protocol. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
23 |
EN_AHB_DECODER |
Enable AHB Decoder: Value=0 : Active slave is selected based on Peripheral Chip Select Lines (bits [13:10]). Value=1 Active slave is selected based on actual AHB address (the partition for each device is calculated with respect to bits [28:21] of Device Size Configuration Register) |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
22:19 |
MSTR_BAUD_DIV |
Master Mode Baud Rate Divisor: SPI baud rate = (master reference clock) baud_rate_divisor. The baud rate is the clock rate divided by 2 multiplied by (Divisor + 1). Meaning, when Divisor Value is set to 0,1,2,..15 it sets the baud rate is the clock rate divided by 2, 4, 6,..32 respectively |
RW |
0x1 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
18 |
ENTER_XIP_MODE_IMM |
Enter XIP Mode immediately: Value=0 : If XIP is enabled, then setting to 0 will cause the controller to exit XIP mode on the next READ instruction. Value=1 : Operate the device in XIP mode immediately Use this register when the external device wakes up in XIP mode (as per the contents of its non- volatile configuration register). The controller will assume the next READ instruction will be passed to the device as an XIP instruction, and therefore will not require the READ opcode to be transferred. Note: To exit XIP mode, this bit should be set to 0. This will take effect in the attached device only after the next READ instruction is executed. Software therefore should ensure that at least one READ instruction is requested after resetting this bit in order to be sure that XIP mode is exited. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
17 |
ENTER_XIP_MODE |
Enter XIP Mode on next READ: Value=0 : If XIP is enabled, then setting to 0 will cause the controller to exit XIP mode on the next READ instruction. Value=1 : If XIP is disabled, then setting to ?1? will inform the controller that the device is ready to enter XIP on the next READ instruction. The controller will therefore send the appropriate command sequence, including mode bits to cause the device to enter XIP mode. Use this register after the controller has ensured the FLASH device has been configured to be ready to enter XIP mode. Note : To exit XIP mode, this bit should be set to 0. This will take effect in the attached device only AFTER the next READ instruction is executed. Software should therefore ensure that at least one READ instruction is requested after resetting this bit before it can be sure XIP mode in the device is exited. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
16 |
ENB_AHB_ADDR_REMAP |
Enable AHB Address Re-mapping: (Direct Access Mode Only) When set to 1, the incoming AHB address will be adapted and sent to the FLASH device as (address + N), where N is the value stored in the remap address register. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
15 |
ENB_DMA_IF |
Enable DMA Peripheral Interface: Set to 1 to enable the DMA handshaking logic. When enabled the controller will trigger DMA transfer requests via the DMA peripheral interface. Set to 0 to disable |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
14 |
WR_PROT_FLASH |
Write Protect Flash Pin: Set to drive the Write Protect pin of the FLASH device. This is resynchronized to the generated memory clock as necessary. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
13:10 |
PERIPH_CS_LINES |
Peripheral Chip Select Lines: Peripheral chip select lines If pdec = 0, ss[3:0] are output thus: ss[3:0] n_ss_out[3:0] xxx0 1110 xx01 1101 x011 1011 0111 0111 1111 1111 (no peripheral selected) else ss[3:0] directly drives n_ss_out[3:0] |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
9 |
PERIPH_SEL_DEC |
Peripheral select decode: |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
8 |
ENB_LEGACY_IP_MODE |
Legacy IP Mode Enable: |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
7 |
ENB_DIR_ACC_CTLR |
Enable Direct Access Controller: |
RW |
1 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
6 |
RESET_CFG |
RESET pin configuration: 0 = RESET feature on DQ3 pin of the device 1 = RESET feature on dedicated pin of the device (controlling of 5th bit influences on reset_out output) |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
5 |
RESET_PIN |
Set to drive the RESET pin of the FLASH device and reset for de-activation of the RESET pin feature |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
4 |
HOLD_PIN |
Set to drive the HOLD pin of the FLASH device and reset for de-activation of the HOLD pin feature |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
3 |
PHY_MODE_EN |
PHY mode enable: When enabled, the controller is informed that PHY Module is to be used for handling SPI transfers. This bit is relevant only for configuration with PHY Module. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
2 |
SEL_CLK_PHASE |
Select Clock Phase: Selects whether the clock is in an active or inactive phase outside the SPI word. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
1 |
SEL_CLK_POL |
Clock polarity outside SPI word: |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
0 |
ENB_SPI |
Octal-SPI Enable: |
RW |
1 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
Address offset |
0x0000 0004 |
||
|
Description |
Device Read Instruction Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:29 |
RESERVED_4 |
|
RO |
0x0 |
||
|
28:24 |
DUMMY_RD_CLK_CYCLES |
Dummy Read Clock Cycles: Number of dummy clock cycles required by device for read instruction. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
23:21 |
RESERVED_3 |
|
RO |
0x0 |
||
|
20 |
MODE_BIT_EN |
Mode Bit Enable: Set this field to 1 to ensure that the mode bits as defined in the Mode Bit Configuration register are sent following the address bytes. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
19:18 |
RESERVED_2 |
|
RO |
0x0 |
||
|
17:16 |
DATA_XFER_TYPE_EXT_MODE |
Data Transfer Type for Standard SPI modes: 0 : SIO mode data is shifted to the device on DQ0 only and from the device on DQ1 only 1 : Used for Dual Input/Output instructions. For data transfers, DQ0 and DQ1 are used as both inputs and outputs. 2 : Used for Quad Input/Output instructions. For data transfers, DQ0,DQ1,DQ2 and DQ3 are used as both inputs and outputs. 3 : Used for Quad Input/Output instructions. For data transfers, DQ[7:0] are used as both inputs and outputs. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
15:14 |
RESERVED |
|
RO |
0x0 |
||
|
13:12 |
ADDR_XFER_TYPE_STD_MODE |
Address Transfer Type for Standard SPI modes: 0 : Addresses can be shifted to the device on DQ0 only 1 : Addresses can be shifted to the device on DQ0 and DQ1 only 2 : Addresses can be shifted to the device on DQ0, DQ1, DQ2 and DQ3 3 : Addresses can be shifted to the device on DQ[7:0] |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
11 |
PRED_DIS |
Predicted Read Disable Bit: Disable generation of predicted read when doing read accesses using Direct Mode |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
10 |
DDR_EN |
DDR Enable: This is to inform that opcode from rd_opcode_non_xip_fld is compliant with one of the DDR READ Commands |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
9:8 |
INSTR_TYPE |
Instruction Type: |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
7:0 |
RD_OPCODE_NON_XIP |
Read Opcode in non-XIP mode: Read Opcode to use when not in XIP mode |
RW |
0x03 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 0008 |
||
|
Description |
Device Write Instruction Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:29 |
RESERVED_4 |
|
RO |
0x0 |
||
|
28:24 |
DUMMY_WR_CLK_CYCLES |
Dummy Write Clock Cycles: Number of dummy clock cycles required by device for write instruction. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
23:18 |
RESERVED_3 |
|
RO |
0x00 |
||
|
17:16 |
DATA_XFER_TYPE_EXT_MODE |
Data Transfer Type for Standard SPI modes: 0 : SIO mode data is shifted to the device on DQ0 only and from the device on DQ1 only 1 : Used for Dual Input/Output instructions. For data transfers, DQ0 and DQ1 are used as both inputs and outputs. 2 : Used for Quad Input/Output instructions. For data transfers, DQ0,DQ1,DQ2 and DQ3 are used as both inputs and outputs. 3 : Used for Quad Input/Output instructions. For data transfers, DQ[7:0] are used as both inputs and outputs. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
15:14 |
RESERVED_2 |
|
RO |
0x0 |
||
|
13:12 |
ADDR_XFER_TYPE_STD_MODE |
Address Transfer Type for Standard SPI modes: 0 : Addresses can be shifted to the device on DQ0 only 1 : Addresses can be shifted to the device on DQ0 and DQ1 only 2 : Addresses can be shifted to the device on DQ0, DQ1, DQ2 and DQ3 3 : Addresses can be shifted to the device on DQ[7:0] |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
11:9 |
RESERVED |
|
RO |
0x0 |
||
|
8 |
WEL_DIS |
WEL Disable: This is to turn off automatic issuing of WEL Command before write operation for DAC or INDAC |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
7:0 |
WR_OPCODE |
Write Opcode |
RW |
0x02 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 000C |
||
|
Description |
Octal-SPI Device Delay Register: This register is used to introduce relative delays into the generation of the master output signals. All timings are defined in cycles of the SPI REFERENCE CLOCK/ext_clk, defined in this table as SPI master ref clock. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
D_NSS |
Clock Delay for Chip Select Deassert: Delay in master reference clocks for the length that the master mode chip select outputs are de-asserted between transactions. The minimum delay is always SCLK period to ensure the chip select is never re-asserted within an SCLK period. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
23:16 |
D_BTWN |
Clock Delay for Chip Select Deactivation: Delay in master reference clocks between one chip select being de-activated and the activation of another. This is used to ensure a quiet period between the selection of two different slaves and requires the transmit FIFO to be empty. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
15:8 |
D_AFTER |
Clock Delay for Last Transaction Bit: Delay in master reference clocks between last bit of current transaction and deasserting the device chip select (n_ss_out). By default, the chip select will be deasserted on the cycle following the completion of the current transaction. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
7:0 |
D_INIT |
Clock Delay with n_ss_out: Delay in master reference clocks between setting n_ss_out low and first bit transfer. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 0010 |
||
|
Description |
Read Data Capture Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:20 |
RESERVED_3 |
|
RO |
0x000 |
||
|
19:16 |
DDR_READ_DELAY |
DDR read delay: Delay the transmitted data by the programmed number of ref_clk cycles.This field is only relevant when DDR Read Command is executed. Otherwise can be ignored. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
15:9 |
RESERVED_2 |
|
RO |
0x00 |
||
|
8 |
DQS_EN |
DQS enable bit: If enabled, signal from DQS input is driven into RX DLL and is used for data capturing in PHY Mode rather than internally generated gated ref_clk.. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
7:6 |
RESERVED |
|
RO |
0x0 |
||
|
5 |
SAMPLE_EDGE_SEL |
Sample edge selection: Choose edge on which data outputs from flash memory will be sampled |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
4:1 |
DELAY |
Read Delay: Delay the read data capturing logic by the programmed number of ref_clk cycles |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
0 |
BYPASS |
Bypass the adapted loopback clock circuit |
RW |
1 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
Address offset |
0x0000 0014 |
||
|
Description |
Device Size Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:29 |
RESERVED |
|
RO |
0x0 |
||
|
28:27 |
MEM_SIZE_ON_CS3 |
Size of Flash Device connected to CS[3] pin: Value=00 : size of 512Mb. Value=01 : size of 1Gb. Value=10 : size of 2Gb. Value=11 : size of 4Gb. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
26:25 |
MEM_SIZE_ON_CS2 |
Size of Flash Device connected to CS[2] pin: Value=00 : size of 512Mb. Value=01 : size of 1Gb. Value=10 : size of 2Gb. Value=11 : size of 4Gb. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
24:23 |
MEM_SIZE_ON_CS1 |
Size of Flash Device connected to CS[1] pin: Value=00 : size of 512Mb. Value=01 : size of 1Gb. Value=10 : size of 2Gb. Value=11 : size of 4Gb. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
22:21 |
MEM_SIZE_ON_CS0 |
Size of Flash Device connected to CS[0] pin: Value=00 : size of 512Mb. Value=01 : size of 1Gb. Value=10 : size of 2Gb. Value=11 : size of 4Gb. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
20:16 |
BYTES_PER_SUBSECTOR |
Number of bytes per Block. This is required by the controller for performing the write protection logic. The number of bytes per block must be a power of 2 number. |
RW |
0x10 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
15:4 |
BYTES_PER_DEVICE_PAGE |
Number of bytes per device page. This is required by the controller for performing FLASH writes up to and across page boundaries. |
RW |
0x100 |
||
|
|
|
0x000 |
MINIMUM |
|
||
|
|
|
0xFFF |
MAXIMUM |
|
||
|
3:0 |
NUM_ADDR_BYTES |
Number of address bytes. A value of 0 indicates 1 byte. |
RW |
0x2 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
Address offset |
0x0000 0018 |
||
|
Description |
SRAM Partition Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:8 |
RESERVED |
|
RO |
0x00 0000 |
||
|
7:0 |
THRESHOLD |
Defines the size of the indirect read partition in the SRAM, |
RW |
0x80 |
||
|
Address offset |
0x0000 001C |
||
|
Description |
Indirect AHB Address Trigger Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ADDR |
This is the base address that will be used by the AHB controller. When the incoming AHB read access address matches a range of addresses from this trigger address to the trigger address + 15, then the AHB request will be completed by fetching data from the Indirect Controllers SRAM. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0020 |
||
|
Description |
DMA Peripheral Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:12 |
RESERVED_2 |
|
RO |
0x0 0000 |
||
|
11:8 |
NUM_BURST_REQ_BYTES |
Number of Burst Bytes: Number of bytes in a burst type request on the DMA peripheral request. A programmed value of 0 represents a single byte. This should be setup before starting the indirect read or write operation. The actual number of bytes used is 2**(value in this register) which will simplify implementation. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
7:4 |
RESERVED |
|
RO |
0x0 |
||
|
3:0 |
NUM_SINGLE_REQ_BYTES |
Number of Single Bytes: Number of bytes in a single type request on the DMA peripheral request. A programmed value of 0 represents a single byte. This should be setup before starting the indirect read or write operation. The actual number of bytes used is 2**(value in this register) which will simplify implementation. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
Address offset |
0x0000 0024 |
||
|
Description |
Remap Address Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
VALUE |
This register is used to remap an incoming AHB address to a different address used by the FLASH device. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0028 |
||
|
Description |
Mode Bit Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
RX_CRC_DATA_LOW |
RX CRC data (lower) The first CRC byte returned after RX data chunk. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
23:16 |
RX_CRC_DATA_UP |
RX CRC data (upper) The second CRC byte returned after RX data chunk. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
15 |
CRC_OUT_EN |
CRC# output enable bit When enabled, the controller expects the Flash Device to toggle CRC data on both SPI clock edges in CRC->CRC# sequence and calculates CRC compliance accordingly. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
14:11 |
RESERVED |
|
RO |
0x0 |
||
|
10:8 |
CHUNK_SIZE |
It defines size of chunk after which CRC data is expected to show up on the SPI interface for write and read data transfers. |
RW |
0x2 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
7:0 |
MODE |
These are the 8 mode bits that are sent to the device following the address bytes if mode bit transmission has been enabled. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 002C |
||
|
Description |
SRAM Fill Register |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:16 |
SRAM_FILL_INDAC_WRITE |
SRAM Fill Level (Indirect Write Partition): Identifies the current fill level of the SRAM Indirect Write partition |
RO |
0x0000 |
||
|
|
|
Read 0x0000 |
MINIMUM |
|
||
|
|
|
Read 0xFFFF |
MAXIMUM |
|
||
|
15:0 |
SRAM_FILL_INDAC_READ |
SRAM Fill Level (Indirect Read Partition): Identifies the current fill level of the SRAM Indirect Read partition |
RO |
0x0000 |
||
|
|
|
Read 0x0000 |
MINIMUM |
|
||
|
|
|
Read 0xFFFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 0030 |
||
|
Description |
TX Threshold Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:5 |
RESERVED |
|
RO |
0x000 0000 |
||
|
4:0 |
LEVEL |
Defines the level at which the small TX FIFO not full interrupt is generated |
RW |
0x01 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
Address offset |
0x0000 0034 |
||
|
Description |
RX Threshold Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:5 |
RESERVED |
|
RO |
0x000 0000 |
||
|
4:0 |
LEVEL |
Defines the level at which the small RX FIFO not empty interrupt is generated |
RW |
0x01 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
Address offset |
0x0000 0038 |
||
|
Description |
Write Completion Control Register: This register defines how the controller will poll the device following a write transfer |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
POLL_REP_DELAY |
Defines additional delay for maintain Chip Select de-asserted during auto-polling phase |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
23:16 |
POLL_COUNT |
Defines the number of times the controller should expect to see a true result from the polling in successive reads of the device register. |
RW |
0x04 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
15 |
EN_POLLING_EXP |
Set to '1' for enabling auto-polling expiration. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
14 |
DISABLE_POLLING |
This switches off the automatic polling function |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
13 |
POLLING_POLARITY |
Defines the polling polarity. If '1', then the write transfer to the device will be complete if the polled bit is equal to '1'. If '0', then the write transfer to the device will be complete if the polled bit is equal to '0'. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
12 |
RESERVED |
|
RO |
0 |
||
|
11 |
POLLING_ADDR_EN |
Enables address phase of auto-polling (Read Status) command. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
10:8 |
POLLING_BIT_INDEX |
Defines the bit index that should be polled. A value of 010 means that bit 2 of the returned data will be polled for.A value of 111 means that bit 7 of the returned data will be polled for. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
7:0 |
OPCODE |
Defines the opcode that should be issued by the controller when it is automatically polling for device program completion. This command is issued followed all device write operations. By default, this will poll the standard device STAUS register using opcode 0x05 |
RW |
0x05 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 003C |
||
|
Description |
Polling Expiration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
NO_OF_POLLS_BEF_EXP |
Number of polls cycles before expiration |
RW |
0xFFFF FFFF |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0040 |
||
|
Description |
Interrupt Status Register: The status fields in this register are set when the described event occurs and the interrupt is enabled in the mask register. When any of these bit fields are set, the interrupt output is asserted high. The fields are each cleared by writing a 1 to the field. Note that bit fields 6 thru 10 are only valid when legacy SPI mode is active. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:20 |
RESERVED_2 |
|
RO |
0x000 |
||
|
19 |
ECC_FAIL |
ECC failure This interrupt informs the system that Flash Device reported ECC error. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
18 |
TX_CRC_CHUNK_BRK |
TX CRC chunk was broken This interrupt informs the system that program page SPI transfer was discontinued somewhere inside the chunk. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
17 |
RX_CRC_DATA_VAL |
RX CRC data valid New RX CRC data was captured from Flash Device |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
16 |
RX_CRC_DATA_ERR |
RX CRC data error CRC data from Flash Device does not correspond to the one dynamically calculated by the controller. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
15 |
RESERVED |
|
RO |
0 |
||
|
14 |
STIG_REQ_INT |
The controller is ready for getting another STIG request. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
13 |
POLL_EXP_INT |
The maximum number of programmed polls cycles is expired |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
12 |
INDRD_SRAM_FULL |
Indirect Read Partition overflow: Indirect Read Partition of SRAM is full and unable to immediately complete indirect operation |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
11 |
RX_FIFO_FULL |
Small RX FIFO full: Current FIFO status can be ignored in non-SPI legacy mode |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
10 |
RX_FIFO_NOT_EMPTY |
Small RX FIFO not empty: Current FIFO status can be ignored in non-SPI legacy mode |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
9 |
TX_FIFO_FULL |
Small TX FIFO full: Current FIFO status can be ignored in non-SPI legacy mode |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
8 |
TX_FIFO_NOT_FULL |
Small TX FIFO not full: Current FIFO status can be ignored in non-SPI legacy mode |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
7 |
RECV_OVERFLOW |
Receive Overflow: This should only occur in Legacy SPI mode. Set if an attempt is made to push the RX FIFO when it is full. This bit is reset only by a system reset and cleared only when this register is read. If a new push to the RX FIFO occurs coincident with a register read this flag will remain set. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
6 |
INDIRECT_XFER_LEVEL_BREACH |
Indirect Transfer Watermark Level Breached |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
5 |
ILLEGAL_ACCESS_DET |
Illegal AHB access has been detected. AHB wrapping bursts and the use of SPLIT/RETRY accesses will cause this error interrupt to trigger. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
4 |
PROT_WR_ATTEMPT |
Write to protected area was attempted and rejected. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
3 |
INDIRECT_TRANSFER_REJECT |
Indirect operation was requested but could not be accepted. Two indirect operations already in storage. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
2 |
INDIRECT_OP_DONE |
Indirect Operation Complete: Controller has completed last triggered indirect operation |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
1 |
UNDERFLOW_DET |
Underflow Detected: |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
0 |
MODE_M_FAIL |
Mode M Failure: Mode M failure indicates the voltage on pin n_ss_in is inconsistent with the SPI mode. Set =1 if n_ss_in is low in master mode (multi-master contention). These conditions will clear the spi_enable bit and disable the SPI. This bit is reset only by a system reset and cleared only when this register is read. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
Address offset |
0x0000 0044 |
||
|
Description |
Interrupt Mask: 0 : the interrupt for the corresponding interrupt status register bit is disabled. |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:20 |
RESERVED_2 |
|
RO |
0x000 |
||
|
19 |
ECC_FAIL_MASK |
ECC failure Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
18 |
TX_CRC_CHUNK_BRK_MASK |
TX CRC chunk was broken Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
17 |
RX_CRC_DATA_VAL_MASK |
RX CRC data valid Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
16 |
RX_CRC_DATA_ERR_MASK |
RX CRC data error Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
15 |
RESERVED |
|
RO |
0 |
||
|
14 |
STIG_REQ_MASK |
STIG request completion Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
13 |
POLL_EXP_INT_MASK |
Polling expiration detected Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
12 |
INDRD_SRAM_FULL_MASK |
Indirect Read Partition overflow mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
11 |
RX_FIFO_FULL_MASK |
Small RX FIFO full Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
10 |
RX_FIFO_NOT_EMPTY_MASK |
Small RX FIFO not empty Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
9 |
TX_FIFO_FULL_MASK |
Small TX FIFO full Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
8 |
TX_FIFO_NOT_FULL_MASK |
Small TX FIFO not full Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
7 |
RECV_OVERFLOW_MASK |
Receive Overflow Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
6 |
INDIRECT_XFER_LEVEL_BREACH_MASK |
Transfer Watermark Breach Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
5 |
ILLEGAL_ACCESS_DET_MASK |
Illegal Access Detected Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
4 |
PROT_WR_ATTEMPT_MASK |
Protected Area Write Attempt Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
3 |
INDIRECT_TRANSFER_REJECT_MASK |
Indirect Read Reject Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
2 |
INDIRECT_OP_DONE_MASK |
Indirect Complete Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
1 |
UNDERFLOW_DET_MASK |
Underflow Detected Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
0 |
MODE_M_FAIL_MASK |
Mode M Failure Mask |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
Address offset |
0x0000 0050 |
||
|
Description |
Lower Write Protection Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
SUBSECTOR |
The block number that defines the lower block in the range of blocks that is to be locked from writing. The definition of a block in terms of number of bytes is programmable via the Device Size Configuration register. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0054 |
||
|
Description |
Upper Write Protection Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
SUBSECTOR |
The block number that defines the upper block in the range of blocks that is to be locked from writing. The definition of a block in terms of number of bytes is programmable via the Device Size Configuration register. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0058 |
||
|
Description |
Write Protection Control Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:2 |
RESERVED |
|
RO |
0x0000 0000 |
||
|
1 |
ENB |
Write Protection Enable Bit: When set to 1, any AHB write access with an address within the protection region defined in the lower and upper write protection registers is rejected. An AHB error response is generated and an interrupt source triggered. When set to 0, the protection region is disabled. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
0 |
INV |
Write Protection Inversion Bit: When set to 1, the protection region defined in the lower and upper write protection registers is inverted meaning it is the region that the system is permitted to write to. When set to 0, the protection region defined in the lower and upper write protection registers is the region that the system is not permitted to write to. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
Address offset |
0x0000 0060 |
||
|
Description |
Indirect Read Transfer Control Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:8 |
RESERVED |
|
RO |
0x00 0000 |
||
|
7:6 |
NUM_IND_OPS_DONE |
This field contains the number of indirect operations which have been completed. This is used in conjunction with the indirect completion status field (bit 5). It is incremented by hardware when an indirect operation has completed. Write a 1 to bit 5 of this register to decrement it. |
RO |
0x0 |
||
|
|
|
Read 0x0 |
MINIMUM |
|
||
|
|
|
Read 0x3 |
MAXIMUM |
|
||
|
5 |
IND_OPS_DONE_STAUS |
Indirect Completion Status: This field is set to 1 when an indirect operation has completed. Write a 1 to this field to clear it. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
4 |
RD_QUEUED |
Two indirect read operations have been queued |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
3 |
SRAM_FULL |
SRAM Full: SRAM full and unable to immediately complete an indirect operation. Write a 1 to this field to clear it.\"; indirect operation (status) |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
2 |
RD_STAUS |
Indirect Read Status: Indirect read operation in progress (status) |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
1 |
CANCEL |
Cancel Indirect Read: Writing a 1 to this bit will cancel all ongoing indirect read operations. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
0 |
START |
Start Indirect Read: Writing a 1 to this bit will trigger an indirect read operation. The assumption is that the indirect start address and the indirect number of bytes register is setup before triggering the indirect read operation. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
Address offset |
0x0000 0064 |
||
|
Description |
Indirect Read Transfer Watermark Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
LEVEL |
Watermark Value: This represents the minimum fill level of the SRAM before a DMA peripheral access is permitted. When the SRAM fill level passes the watermark, an interrupt is also generated. This field can be disabled by writing a value of all zeroes. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0068 |
||
|
Description |
Indirect Read Transfer Start Address Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ADDR |
This is the start address from which the indirect access will commence its READ operation. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 006C |
||
|
Description |
Indirect Read Transfer Number Bytes Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
VALUE |
This is the number of bytes that the indirect access will consume. This can be bigger than the configured size of SRAM. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0070 |
||
|
Description |
Indirect Write Transfer Control Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:8 |
RESERVED_2 |
|
RO |
0x00 0000 |
||
|
7:6 |
NUM_IND_OPS_DONE |
This field contains the number of indirect operations which have been completed. This is used in conjunction with the indirect completion status field (bit 5). It is incremented by hardware when an indirect operation has completed. Write a 1 to bit 5 of this register to decrement it. |
RO |
0x0 |
||
|
|
|
Read 0x0 |
MINIMUM |
|
||
|
|
|
Read 0x3 |
MAXIMUM |
|
||
|
5 |
IND_OPS_DONE_STAUS |
Indirect Completion Status: This field is set to 1 when an indirect operation has completed. Write a 1 to this field to clear it. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
4 |
WR_QUEUED |
Two indirect write operations have been queued |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
3 |
RESERVED |
|
RO |
0 |
||
|
2 |
WR_STAUS |
Indirect Write Status: Indirect write operation in progress (status) |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
1 |
CANCEL |
Cancel Indirect Write: Writing a 1 to this bit will cancel all ongoing indirect write operations. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
0 |
START |
Start Indirect Write: Writing a 1 to this bit will trigger an indirect write operation. The assumption is that the indirect start address and the indirect number of bytes register is setup before triggering the indirect write operation. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
Address offset |
0x0000 0074 |
||
|
Description |
Indirect Write Transfer Watermark Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
LEVEL |
Watermark Value: This represents the maximum fill level of the SRAM before a DMA peripheral access is permitted. When the SRAM fill level falls below the watermark, an interrupt is also generated. This field can be disabled by writing a value of all ones. |
RW |
0xFFFF FFFF |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0078 |
||
|
Description |
Indirect Write Transfer Start Address Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ADDR |
Start of Indirect Access: This is the start address from which the indirect access will commence its READ operation. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 007C |
||
|
Description |
Indirect Write Transfer Number Bytes Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
VALUE |
Indirect Number of Bytes: This is the number of bytes that the indirect access will consume. This can be bigger than the configured size of SRAM. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 0080 |
||
|
Description |
Indirect Trigger Address Range Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:4 |
RESERVED |
|
RO |
0x000 0000 |
||
|
3:0 |
IND_RANGE_WIDTH |
This is the address offset of Indirect Trigger Address Register. |
RW |
0x4 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0xF |
MAXIMUM |
|
||
|
Address offset |
0x0000 008C |
||
|
Description |
Flash Command Control Memory Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:29 |
RESERVED_3 |
|
RO |
0x0 |
||
|
28:20 |
MEM_BANK_ADDR |
The address of the Memory Bank which data will be read from. |
RW |
0x000 |
||
|
|
|
0x000 |
MINIMUM |
|
||
|
|
|
0x1FF |
MAXIMUM |
|
||
|
19 |
RESERVED_2 |
|
RO |
0 |
||
|
18:16 |
NB_OF_STIG_READ_BYTES |
It defines the number of read bytes for the extended STIG. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
15:8 |
MEM_BANK_READ_DATA |
Last requested data from the STIG Memory Bank. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
7:2 |
RESERVED |
|
RO |
0x00 |
||
|
1 |
MEM_BANK_REQ_IN_PROGRESS |
Memory Bank data request in progress. |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
0 |
TRIGGER_MEM_BANK_REQ |
Trigger the Memory Bank data request. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
Address offset |
0x0000 0090 |
||
|
Description |
Flash Command Control Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
CMD_OPCODE |
Command Opcode: The command opcode field should be setup before triggering the command. For example, 0x20 maps to SubSector Erase. Writing to the execute field (bit 0) of this register launches the command. NOTE : Using this approach to issue commands to the device will make use of the instruction type of the device instruction configuration register. If this field is set to 2'b00, then the command opcode, command address, command dummy bytes and command data will all be transferred in a serial fashion. If this field is set to 2'b01, then the command opcode, command address, command dummy bytes and command data will all be transferred in parallel using DQ0 and DQ1 pins. If this field is set to 2'b10, then the command opcode, command address, command dummy bytes and command data will all be transferred in parallel using DQ0, DQ1, DQ2 and DQ3 pins. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
23 |
ENB_READ_DATA |
Read Data Enable: Set to 1 if the command specified in the command opcode field (bits 31:24) requires read data bytes to be received from the device. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
22:20 |
NUM_RD_DATA_BYTES |
Number of Read Data Bytes: Up to 8 data bytes may be read using this command. Set to 0 for 1 byte and 7 for 8 bytes. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
19 |
ENB_COMD_ADDR |
Command Address Enable: Set to 1 if the command specified in bits 31:24 requires an address. This should be setup before triggering the command via writing a 1 to the execute field. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
18 |
ENB_MODE_BIT |
Mode Bit Enable: Set to 1 to ensure the mode bits as defined in the Mode Bit Configuration register are sent following the address bytes. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
17:16 |
NUM_ADDR_BYTES |
Number of Address Bytes: Set to the number of address bytes required (the address itself is programmed in the FLASH COMMAND ADDR REGISTERS). This should be setup before triggering the command via bit 0 of this register. 2'b00 : 1 address byte 2'b01 : 2 address bytes 2'b10 : 3 address bytes 2'b11 : 4 address bytes |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x3 |
MAXIMUM |
|
||
|
15 |
ENB_WRITE_DATA |
Write Data Enable: Set to 1 if the command specified in the command opcode field requires write data bytes to be sent to the device. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
14:12 |
NUM_WR_DATA_BYTES |
Number of Write Data Bytes: Up to 8 Data bytes may be written using this command Set to 0 for 1 byte, 7 for 8 bytes. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
11:7 |
NUM_DUMMY_CYCLES |
Number of Dummy cycles: Set to the number of dummy cycles required. This should be setup before triggering the command via the execute field of this register. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
6:3 |
CMD_GEN_FSM_STAE |
CMD_GEN_FSM_STAE ?is used to define the ?Polling flag?:? |
RO |
0x0 |
||
|
|
|
Read 0x0 |
IDLE |
|
||
|
|
|
Read 0x1 |
SEND_ADDR_BYTES |
|
||
|
|
|
Read 0x2 |
STIG_MODE_BYTE |
|
||
|
|
|
Read 0x3 |
STIG_DUMMY_BYTES |
|
||
|
|
|
Read 0x4 |
SEND_DATA |
|
||
|
|
|
Read 0x5 |
SEND_STIG_DATA_LOWER |
|
||
|
|
|
Read 0x6 |
SEND_STIG_DATA_UPPER |
|
||
|
|
|
Read 0x7 |
POLL_STAUS_AFTER_WRITE |
|
||
|
|
|
Read 0x8 |
POLL_STAUS_AFTER_WRITE2 |
|
||
|
|
|
Read 0xA |
LET_TXFIFO_EMPTY |
|
||
|
|
|
Read 0xB |
POLL_STAUS_WAIT |
|
||
|
|
|
Read 0xC |
SEND_DATA_PIPE |
|
||
|
2 |
STIG_MEM_BANK_EN |
STIG Memory Bank enable bit. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
1 |
CMD_EXEC_STAUS |
Command execution in progress. |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
0 |
CMD_EXEC |
Execute the command. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
Address offset |
0x0000 0094 |
||
|
Description |
Flash Command Address Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
ADDR |
Command Address: This should be setup before triggering the command with execute field (bit 0) of the Flash Command Control register. It is the address used by the command specified in the opcode field (bits 31:24) of the Flash Command Control register. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 00A0 |
||
|
Description |
Flash Command Read Data Register (Lower) |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
DATA |
This is the data that is returned by the flash device for any status or configuration read operation carried out by triggering the event in the control register. The register will be valid when the polling bit in the control register is low. |
RO |
0x0000 0000 |
||
|
|
|
Read 0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
Read 0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 00A4 |
||
|
Description |
Flash Command Read Data Register (Upper) |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
DATA |
This is the data that is returned by the FLASH device for any status or configuration read operation carried out by triggering the event in the control register. The register will be valid when the polling bit in the control register is low. |
RO |
0x0000 0000 |
||
|
|
|
Read 0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
Read 0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 00A8 |
||
|
Description |
Flash Command Write Data Register (Lower) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
DATA |
Command Write Data Lower Byte: This is the command write data lower byte. This should be setup before triggering the command with execute field (bit 0) of the Flash Command Control register. It is the data that is to be written to the flash for any status or configuration write operation carried out by triggering the event in the Flash Command Control register. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 00AC |
||
|
Description |
Flash Command Write Data Register (Upper) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:0 |
DATA |
Command Write Data Upper Byte: This is the command write data upper byte. This should be setup before triggering the command with execute field (bit 0) of the Flash Command Control register. It is the data that is to be written to the flash for any status or configuration write operation carried out by triggering the event in the Flash Command Control register. |
RW |
0x0000 0000 |
||
|
|
|
0xFFFF FFFF |
MAXIMUM |
|
||
|
|
|
0x0000 0000 |
MINIMUM |
|
||
|
Address offset |
0x0000 00B0 |
||
|
Description |
Polling Flash Status Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:21 |
RESERVED_2 |
|
RO |
0x000 |
||
|
20:16 |
DEVICE_STAUS_NB_DUMMY |
Number of dummy cycles for auto-polling |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x1F |
MAXIMUM |
|
||
|
15:9 |
RESERVED |
|
RO |
0x00 |
||
|
8 |
DEVICE_STAUS_VALID |
Device Status Valid: This should be set when value in bits from 7 to 0 is valid. |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
7:0 |
DEVICE_STAUS |
Defines actual Status Register of Device |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 00B4 |
||
|
Description |
PHY Configuration Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31 |
PHY_CONFIG_RESYNC |
This bit is used for re-synchronisation delay lines to update them with values from TX DLL Delay and RX DLL Delay fields. |
WO |
0 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
30 |
PHY_CONFIG_RESET |
DLL Reset bit: This bit is used for reset of Delay Lines by software. |
WO |
1 |
||
|
|
|
Write 0 |
DISABLE |
|
||
|
|
|
Write 1 |
EN |
|
||
|
29 |
PHY_CONFIG_RX_DLL_BYPASS |
RX DLL Bypass: This field determines id RX DLL is bypassed. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
28:23 |
RESERVED_2 |
|
RO |
0x00 |
||
|
22:16 |
PHY_CONFIG_TX_DLL_DELAY |
TX DLL Delay: This field determines the number of delay elements to insert on data path between ref_clk and spi_clk. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x7F |
MAXIMUM |
|
||
|
15:7 |
RESERVED |
|
RO |
0x000 |
||
|
6:0 |
PHY_CONFIG_RX_DLL_DELAY |
RX DLL Delay: This field determines the number of delay elements to insert on data path between ref_clk and rx_dll_clk. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x7F |
MAXIMUM |
|
||
|
Address offset |
0x0000 00B8 |
||
|
Description |
PHY DLL Master Control Register |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:25 |
RESERVED_3 |
|
RO |
0x00 |
||
|
24 |
PHY_MASTER_LOCK_MODE |
Determines if the master delay line locks on a full cycle or half cycle of delay. |
RW |
0 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
23 |
PHY_MASTER_BYPASS_MODE |
Controls the bypass mode of the master and slave DLLs. |
RW |
1 |
||
|
|
|
0 |
DISABLE |
|
||
|
|
|
1 |
EN |
|
||
|
22:20 |
PHY_MASTER_PHASE_DETECT_SELECTOR |
Selects the number of delay elements to be inserted between the phase detect flip-flops. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
19 |
RESERVED_2 |
|
RO |
0 |
||
|
18:16 |
PHY_MASTER_NB_INDICATIONS |
Holds the number of consecutive increment or decrement indications. |
RW |
0x0 |
||
|
|
|
0x0 |
MINIMUM |
|
||
|
|
|
0x7 |
MAXIMUM |
|
||
|
15:7 |
RESERVED |
|
RO |
0x000 |
||
|
6:0 |
PHY_MASTER_INITIAL_DELAY |
This value is the initial delay value for the DLL. |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0x7F |
MAXIMUM |
|
||
|
Address offset |
0x0000 00BC |
||
|
Description |
DLL Observable Register Lower |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
DLL_OBSERVABLE_LOWER_DLL_LOCK_INC |
Holds the state of the cumulative dll_lock_inc register. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
23:16 |
DLL_OBSERVABLE_LOWER_DLL_LOCK_DEC |
Holds the state of the cumulative dll_lock_dec register. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
15 |
DLL_OBSERVABLE_LOWER_LOOPBACK_LOCK |
This bit indicates that lock of loopback is done. |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
14:8 |
DLL_OBSERVABLE_LOWER_LOCK_VALUE |
Reports the DLL encoder value from the master DLL to the slave DLLs. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0x7F |
MAXIMUM |
|
||
|
7:3 |
DLL_OBSERVABLE_LOWER_UNLOCK_COUNTER |
Reports the number of increments or decrements required for the master DLL to complete the locking process. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0x1F |
MAXIMUM |
|
||
|
2:1 |
DLL_OBSERVABLE_LOWER_LOCK_MODE |
Defines the mode in which the DLL has achieved the lock. |
RO |
0x0 |
||
|
|
|
Read 0x0 |
MINIMUM |
|
||
|
|
|
Read 0x3 |
MAXIMUM |
|
||
|
0 |
DLL_OBSERVABLE_LOWER_DLL_LOCK |
Indicates status of DLL. |
RO |
0 |
||
|
|
|
Read 0 |
DISABLE |
|
||
|
|
|
Read 1 |
EN |
|
||
|
Address offset |
0x0000 00C0 |
||
|
Description |
DLL Observable Register Upper |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:23 |
RESERVED_2 |
|
RO |
0x000 |
||
|
22:16 |
DLL_OBSERVABLE_UPPER_TX_DECODER_OUTPUT |
Holds the encoded value for the TX delay line for this slice. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0x7F |
MAXIMUM |
|
||
|
15:7 |
RESERVED |
|
RO |
0x000 |
||
|
6:0 |
DLL_OBSERVABLE__UPPER_RX_DECODER_OUTPUT |
Holds the encoded value for the RX delay line for this slice. |
RO |
0x00 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0x7F |
MAXIMUM |
|
||
|
Address offset |
0x0000 00E0 |
||
|
Description |
Opcode Extension Register (Lower) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
EXT_READ_OPCODE |
Supplement byte of any Read Opcode |
RW |
0x13 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
23:16 |
EXT_WRITE_OPCODE |
Supplement byte of any Write Opcode |
RW |
0xED |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
15:8 |
EXT_POLL_OPCODE |
Supplement byte of any Polling Opcode |
RW |
0xFA |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
7:0 |
EXT_STIG_OPCODE |
Supplement byte of any STIG Opcode |
RW |
0x00 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
Address offset |
0x0000 00E4 |
||
|
Description |
Opcode Extension Register (Upper) |
||
|
Type |
RW |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
WEL_OPCODE |
First byte of any WEL Opcode |
RW |
0x06 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
23:16 |
EXT_WEL_OPCODE |
Supplement byte of any WEL Opcode |
RW |
0xF9 |
||
|
|
|
0x00 |
MINIMUM |
|
||
|
|
|
0xFF |
MAXIMUM |
|
||
|
15:0 |
RESERVED |
|
RO |
0x0000 |
||
|
Address offset |
0x0000 00FC |
||
|
Description |
Module ID Register |
||
|
Type |
RO |
||
|
Bits |
Field Name |
Description |
Type |
Reset |
||
|
31:24 |
FIX_PATCH |
Fix/path number related to revision described by 3 LSBs of this register |
RO |
0x04 |
||
|
|
|
Read 0x00 |
MINIMUM |
|
||
|
|
|
Read 0xFF |
MAXIMUM |
|
||
|
23:8 |
MODULE_ID |
Module/Revision ID number |
RO |
0x0003 |
||
|
|
|
Read 0x0000 |
MINIMUM |
|
||
|
|
|
Read 0xFFFF |
MAXIMUM |
|
||
|
7:2 |
RESERVED |
|
RO |
0x00 |
||
|
1:0 |
CONF |
Configuration ID number: 0 : OCTAL + PHY Configuration 1 : OCTAL Configuration 2 : QUAD + PHY Configuration 3 : QUAD Configuration |
RO |
0x0 |
||
|
|
|
Read 0x0 |
MINIMUM |
|
||
|
|
|
Read 0x3 |
MAXIMUM |
|
||