|
TRX Host Driver
|
| Module | Architecture doc | Interface |
|---|---|---|
| Host API | HOST API | trx_host.h |
| Platform HAL | Platform HAL layer | platform_spi.h platform_util.h |
| Example | Summary | Readme |
|---|---|---|
| rfPacketTx | Simple packet transmission using the TRX Host driver | README |
| rfPacketRx | Simple packet reception using the TRX Host driver | README |
| rfCarrierWave | Sends a continuous carrier wave or pseudo-random modulated signal on a fixed frequency | README |
| rfDiagnostics | Some of the most common TRX Host Driver commands have been exposed over an AT Command Interface such that it can be exercised by Host SW (running on an PC, MPU or MCU) or by a human using a serial terminal emulator | README |
| rfMdrRx | Simplified reception of packets using WiSUN Modulation and Data Rate (MDR) Negotiation | README |
| rfMdrTx | Simplified transmission of packets using WiSUN Modulation and Data Rate (MDR) Negotiation | README |
| rfMdrTxWithCca | Simplified transmission of packets with clear channel assessment (CCA) using WiSUN Modulation and Data Rate (MDR) Negotiation | README |
The SPI traffic between a host device and the TRX can be captured using a logic analyzer and processed with the provided plugin to be human-readable. For more information refer to the SPITRX Logic Analyzer Plugin documentation.