SimpleLink™ SDK Edge AI Plugin 1.10.00.00 Release Notes

Table of Contents

Introduction

The SimpleLink™ SDK EdgeAI Plugin (EDGEAI) from Texas Instruments is a plugin for enabling EdgeAI development on TI’s Wireless MCUs leveraging the TI’s Edge AIs Studio.

Documentation

The following documentation is provided with this release.

What’s New

With this release of the plugin, new examples have been added for the following devices, and previously supported examples now include support for additional devices.

NOTE: The Fan blade fault detection example enabled in the plugin allows the user to evaluate the Fan Imbalance Classification and Motor Bearing Fault Classification Edge AI Projects within EDGE-AI-STUDIO-MCU.

The plug-in contains the following features that have been developed:

Fixed Issues

No bug fixes or known issues addressed in this release.

Known Issues and Limitations

Device Example Base Example
CC2755P10 CC2745R10_Q1
CC1312R CC1312PSIP
CC1312R7 CC1312PSIP
CC1352P7 CC1352R1
CC1352P1 CC1352R1
CC1354P10-6 CC1354P10-1

Operating System Support

Dependencies

EDGEAI requires the following dependency versions (or compatible):

NOTE: For CC35xx SimpleLink™ wireless MCU examples, please ensure you are using SimpleLink™ Wi-Fi SDK version 10.10.01.08 or higher to avoid compilation errors.

Device Support

This SDK supports the following SimpleLink™ wireless MCUs:

Device Orderable Part Number (OPN) LaunchPad Product Page Migrate from these examples SDK Dependency
CC2755R10 CC2755R105E0WRHAR LP-EM-CC2745R10-Q1 CC2755R10 LP-EM-CC2745R10-Q1 SIMPLELINK-LOWPOWER-F3-SDK
CC2755P10 CC2755P105E0WRHA N/A CC2755P10 N/A SIMPLELINK-LOWPOWER-F3-SDK
CC2745R10-Q1 CC2745R10E0WRHARQ1 LP-EM-CC2745R10-Q1 CC2745R10-Q1 N/A SIMPLELINK-LOWPOWER-F3-SDK
CC2745R10-Q1 CC2745R10E1WRHARQ1 LP-EM-CC2745R10-Q1 CC2745R10-Q1 N/A SIMPLELINK-LOWPOWER-F3-SDK
CC1312R CC1312R1F3RGZ LAUNCHXL-CC1312R1 CC1312R CC1312PSIP SIMPLELINK-LOWPOWER-F2-SDK
CC1312R7 CC1312R74T0RGZR LP-CC1312R7 CC1312R7 CC1312PSIP SIMPLELINK-LOWPOWER-F2-SDK
CC1312PSIP CC1312PSIPMOT LP-EM-CC1312PSIP CC1312PSIP N/A SIMPLELINK-LOWPOWER-F2-SDK
CC1352P7 CC1352P74T0RGZR LP-CC1352P7-1, LP-CC1352P7-4 CC1352P7 CC1352R SIMPLELINK-LOWPOWER-F2-SDK
CC1352R CC1352R1F3RGZ LAUNCHXL-CC1352R1 CC1352R N/A SIMPLELINK-LOWPOWER-F2-SDK
CC1352P CC1352R1F3RGZ LAUNCHXL-CC1352P CC1352P CC1352R SIMPLELINK-LOWPOWER-F2-SDK
CC1314R10 CC1314R106T0RGZ LP-EM-CC1314R10 CC1314R10 N/A SIMPLELINK-LOWPOWER-F2-SDK
CC1354P10-6 CC1354P106T0RGZ LP-EM-CC1354P10 CC1354P10-6 CC1354P10-1 SIMPLELINK-LOWPOWER-F2-SDK
CC1354P10-1 CC1354P106T0RGZ LP-EM-CC1354P10 CC1354P10-1 N/A SIMPLELINK-LOWPOWER-F2-SDK
CC3551E CC3550ENJARSHR LP-EM-CC35X1 CC3551E N/A SIMPLELINK-WIFI-SDK

Versioning

All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 1.00.00.00_eng).

This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.

To support multiple side-by-side installations of the product, the product version is encoded in the top level directory.

Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.

Technical Support

Last updated: 2026-07-16