24 #ifndef __USBHHIDMOUSE_H__ 25 #define __USBHHIDMOUSE_H__ 54 uint32_t ui32MsgParam,
58 uint8_t *pui8Buffer, uint32_t ui32Size);
struct tUSBHMouse tUSBHMouse
Definition: usbhhidmouse.h:45
tUSBHMouse * USBHMouseOpen(tUSBHIDMouseCallback pfnCallback, uint8_t *pui8Buffer, uint32_t ui32Size)
Definition: usbhhidmouse.c:138
uint32_t USBHMouseClose(tUSBHMouse *psMsInstance)
Definition: usbhhidmouse.c:176
uint32_t USBHMouseInit(tUSBHMouse *psMsInstance)
Definition: usbhhidmouse.c:211
uint32_t USBHMouseLPMStatus(tUSBHMouse *psMsInstance)
Definition: usbhhidmouse.c:437
uint32_t USBHMouseLPMSleep(tUSBHMouse *psMsInstance)
Definition: usbhhidmouse.c:409
void(* tUSBHIDMouseCallback)(tUSBHMouse *psMsInstance, uint32_t ui32Event, uint32_t ui32MsgParam, void *pvMsgData)
Definition: usbhhidmouse.h:52