22 #ifndef __USBHCDCSERIAL_H__ 23 #define __USBHCDCSERIAL_H__ 49 #define USBHCDC_DEVICE_PRESENT 0x00000001 61 uint32_t ui32MsgParam,
73 uint8_t *ui8SendBuffer, uint8_t byteSize);
tUSBHCDCSerial * USBHCDCSerialOpen(tUSBHCDCSerialCallback pfnCallback)
Definition: usbhcdcserial.c:111
uint32_t USBHCDCSerialClose(tUSBHCDCSerial *psCdcSerialInstance)
Definition: usbhcdcserial.c:143
uint32_t USBHCDCSerialInit(tUSBHCDCSerial *psCdcInstance)
Definition: usbhcdcserial.c:242
void(* tUSBHCDCSerialCallback)(tUSBHCDCSerial *psCdcSerialInstance, uint32_t ui32Event, uint32_t ui32MsgParam, void *pvMsgData)
Definition: usbhcdcserial.h:59
uint32_t USBHCDCGetDataFromDevice(tUSBHCDCSerial *psCdcSerialInstance, uint32_t ui32Interface)
Definition: usbhcdcserial.c:290
uint32_t USBHCDCProcessData(tUSBHCDCSerial *psCdcSerialInstance, uint8_t ui8ArrayIndex)
Definition: usbhcdcserial.c:383
struct tUSBHCDCSerial tUSBHCDCSerial
Definition: usbhcdcserial.h:52
uint32_t USBHCDCSendDataToDevice(tUSBHCDCSerial *psCdcSerialInstance, uint32_t ui32Interface, uint8_t *ui8SendBuffer, uint8_t byteSize)
Definition: usbhcdcserial.c:338