Network Services API  2.75.00.17
Data Structures | Macros | Typedefs | Enumerations | Functions
slnetsock.h File Reference
#include <stdint.h>
#include <sys/time.h>
Include dependency graph for slnetsock.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  SlNetSock_InAddr_t
 Internet address. More...
 
struct  SlNetSock_In6Addr_t
 IpV6 or Ipv6 EUI64. More...
 
struct  SlNetSock_NoDelay_t
 The SlNetSock_NoDelay_t structure is used in SLNETSOCK_TCP_NODELAY TCP level option. More...
 
struct  SlNetSock_MaxSeg_t
 The SlNetSock_MaxSeg_t structure is used in SLNETSOCK_TCP_MAXSEG TCP level option. More...
 
struct  SlNetSock_NoPush_t
 The SlNetSock_NoPush_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option. More...
 
struct  SlNetSock_NoOpt_t
 The SlNetSock_NoOpt_t structure is used in SLNETSOCK_TCP_NOOPT TCP level option. More...
 
struct  SlNetSock_SackPermitted_t
 The SlNetSock_SackPermitted_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option. More...
 
struct  SlNetSock_MaxRtt_t
 The SlNetSock_MaxRtt_t structure is used in SLNETSOCK_TCP_MAXRTT TCP level option. More...
 
struct  SlNetSock_Keepalive_t
 The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option. More...
 
struct  SlNetSock_NonIpBoundary_t
 The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option. More...
 
struct  SlNetSock_Winsize_t
 The SlNetSock_Winsize_t structure is used in SLNETSOCK_OPSOCK_RCV_BUF socket level option. More...
 
struct  SlNetSock_Nonblocking_t
 The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option. More...
 
struct  SlNetSock_Broadcast_t
 The SlNetSock_Broadcast_t structure is used in SLNETSOCK_OPSOCK_BROADCAST socket level option. More...
 
struct  SlNetSock_SecAttribNode_t
 Secure socket attribute context. More...
 
struct  SlNetSock_SecureALPN_t
 Secure ALPN structure. More...
 
struct  SlNetSock_SecureMask_t
 Secure Mask structure. More...
 
struct  SlNetSock_SecureMethod_t
 Secure Method structure. More...
 
struct  SlNetSock_IpMreq_t
 The SlNetSock_IpMreq_t structure is used in SLNETSOCK_OPIP_ADD_MEMBERSHIP and SLNETSOCK_OPIP_DROP_MEMBERSHIP IP level option. More...
 
struct  SlNetSock_IpV6Mreq_t
 The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP and SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option. More...
 
struct  SlNetSock_linger_t
 The SlNetSock_linger_t structure is used in SLNETSOCK_OPSOCK_LINGER socket level option. More...
 
struct  SlNetSock_Addr_t
 IpV4 socket address. More...
 
struct  SlNetSock_AddrIn6_t
 SlNetSock IPv6 address, Internet style. More...
 
struct  SlNetSock_AddrIn_t
 SlNetSock IPv4 address, Internet style. More...
 
struct  SlNetSock_SockAddrStorage_t
 Generic socket address type to hold either IPv4 or IPv6 address. More...
 
struct  SlNetSock_SdSet_t
 The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function. More...
 
struct  SlNetSock_TransceiverRxOverHead_t
 The SlNetSock_TransceiverRxOverHead_t structure holds the data for Rx transceiver mode using a raw socket when using SlNetSock_recv function. More...
 

Macros

#define SLNETSOCK_MAX_CONCURRENT_SOCKETS   (32)
 
#define SLNETSOCK_AF_UNSPEC   (0)
 
#define SLNETSOCK_AF_INET   (2)
 
#define SLNETSOCK_AF_INET6   (3)
 
#define SLNETSOCK_AF_RF   (6)
 
#define SLNETSOCK_AF_PACKET   (17)
 
#define SLNETSOCK_PF_UNSPEC   SLNETSOCK_AF_UNSPEC
 
#define SLNETSOCK_PF_INET   SLNETSOCK_AF_INET
 
#define SLNETSOCK_PF_INET6   SLNETSOCK_AF_INET6
 
#define SLNETSOCK_SOCK_STREAM   (1)
 
#define SLNETSOCK_SOCK_DGRAM   (2)
 
#define SLNETSOCK_SOCK_RAW   (3)
 
#define SLNETSOCK_SOCK_RX_MTR   (4)
 
#define SLNETSOCK_SOCK_MAC_WITH_CCA   (5)
 
#define SLNETSOCK_SOCK_MAC_WITH_NO_CCA   (6)
 
#define SLNETSOCK_SOCK_BRIDGE   (7)
 
#define SLNETSOCK_SOCK_ROUTER   (8)
 
#define SLNETSOCK_PROTO_TCP   (6)
 
#define SLNETSOCK_PROTO_UDP   (17)
 
#define SLNETSOCK_PROTO_RAW   (255)
 
#define SLNETSOCK_PROTO_SECURE   (100)
 
#define SLNETSOCK_INADDR_ANY   (0)
 
#define SLNETSOCK_IN6ADDR_ANY   (0)
 
#define SLNETSOCK_LVL_SOCKET   (1)
 
#define SLNETSOCK_LVL_IP   (2)
 
#define SLNETSOCK_LVL_PHY   (3)
 
#define SLNETSOCK_OPSOCK_RCV_BUF   (8)
 
#define SLNETSOCK_OPSOCK_SND_BUF   (202)
 
#define SLNETSOCK_OPSOCK_RCV_TIMEO   (20)
 
#define SLNETSOCK_OPSOCK_SND_TIMEO   (21)
 
#define SLNETSOCK_OPSOCK_KEEPALIVE   (9)
 
#define SLNETSOCK_OPSOCK_KEEPALIVE_TIME   (37)
 
#define SLNETSOCK_OPSOCK_LINGER   (13)
 
#define SLNETSOCK_OPSOCK_NON_BLOCKING   (24)
 
#define SLNETSOCK_OPSOCK_NON_IP_BOUNDARY   (39)
 
#define SLNETSOCK_OPSOCK_ERROR   (58)
 
#define SLNETSOCK_OPSOCK_SLNETSOCKSD   (59)
 
#define SLNETSOCK_OPSOCK_BROADCAST   (200)
 
#define SLNETSOCK_OPSOCK_REUSEADDR   (201)
 
#define SLNETSOCK_OPSOCK_REUSEPORT   (203)
 
#define SLNETSOCK_OPIP_MULTICAST_TTL   (61)
 
#define SLNETSOCK_OPIP_ADD_MEMBERSHIP   (65)
 
#define SLNETSOCK_OPIP_DROP_MEMBERSHIP   (66)
 
#define SLNETSOCK_OPIP_HDRINCL   (67)
 
#define SLNETSOCK_OPIP_RAW_RX_NO_HEADER   (68)
 
#define SLNETSOCK_OPIP_RAW_IPV6_HDRINCL   (69)
 
#define SLNETSOCK_OPIPV6_ADD_MEMBERSHIP   (70)
 
#define SLNETSOCK_OPIPV6_DROP_MEMBERSHIP   (71)
 
#define SLNETSOCK_OPIPV6_MULTICAST_HOPS   (72)
 
#define SLNETSOCK_OPPHY_CHANNEL   (28)
 
#define SLNETSOCK_OPPHY_RATE   (100)
 
#define SLNETSOCK_OPPHY_TX_POWER   (101)
 
#define SLNETSOCK_OPPHY_NUM_FRAMES_TO_TX   (102)
 
#define SLNETSOCK_OPPHY_PREAMBLE   (103)
 
#define SLNETSOCK_OPPHY_TX_INHIBIT_THRESHOLD   (104)
 
#define SLNETSOCK_OPPHY_TX_TIMEOUT   (105)
 
#define SLNETSOCK_OPPHY_ALLOW_ACKS   (106)
 
#define SLNETSOCK_TCP_NODELAY   (203)
 
#define SLNETSOCK_TCP_MAXSEG   (204)
 
#define SLNETSOCK_TCP_NOPUSH   (205)
 
#define SLNETSOCK_TCP_NOOPT   (206)
 
#define SLNETSOCK_TCP_SACKPERMITTED   (207)
 
#define SLNETSOCK_TCP_MAXRTT   (208)
 
#define SLNETSOCK_SEC_METHOD_SSLV3   (0)
 
#define SLNETSOCK_SEC_METHOD_TLSV1   (1)
 
#define SLNETSOCK_SEC_METHOD_TLSV1_1   (2)
 
#define SLNETSOCK_SEC_METHOD_TLSV1_2   (3)
 
#define SLNETSOCK_SEC_METHOD_SSLv3_TLSV1_2   (4)
 
#define SLNETSOCK_SEC_METHOD_DLSV1   (5)
 
#define SLNETSOCK_SEC_CIPHER_SSL_RSA_WITH_RC4_128_SHA   (1 << 0)
 
#define SLNETSOCK_SEC_CIPHER_SSL_RSA_WITH_RC4_128_MD5   (1 << 1)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_256_CBC_SHA   (1 << 2)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_AES_256_CBC_SHA   (1 << 3)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_256_CBC_SHA   (1 << 4)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_RC4_128_SHA   (1 << 5)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_128_CBC_SHA256   (1 << 6)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_256_CBC_SHA256   (1 << 7)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_128_CBC_SHA256   (1 << 8)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA256   (1 << 9)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_128_CBC_SHA   (1 << 10)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_256_CBC_SHA   (1 << 11)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_128_GCM_SHA256   (1 << 12)
 
#define SLNETSOCK_SEC_CIPHER_TLS_RSA_WITH_AES_256_GCM_SHA384   (1 << 13)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_AES_128_GCM_SHA256   (1 << 14)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_AES_256_GCM_SHA384   (1 << 15)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_128_GCM_SHA256   (1 << 16)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_AES_256_GCM_SHA384   (1 << 17)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_128_GCM_SHA256   (1 << 18)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_AES_256_GCM_SHA384   (1 << 19)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_ECDSA_WITH_CHACHA20_POLY1305_SHA256   (1 << 20)
 
#define SLNETSOCK_SEC_CIPHER_TLS_ECDHE_RSA_WITH_CHACHA20_POLY1305_SHA256   (1 << 21)
 
#define SLNETSOCK_SEC_CIPHER_TLS_DHE_RSA_WITH_CHACHA20_POLY1305_SHA256   (1 << 22)
 
#define SLNETSOCK_SEC_CIPHER_FULL_LIST   (0xFFFFFFFF)
 
#define SLNETSOCK_SEC_ALPN_H1   (1 << 0)
 
#define SLNETSOCK_SEC_ALPN_H2   (1 << 1)
 
#define SLNETSOCK_SEC_ALPN_H2C   (1 << 2)
 
#define SLNETSOCK_SEC_ALPN_H2_14   (1 << 3)
 
#define SLNETSOCK_SEC_ALPN_H2_16   (1 << 4)
 
#define SLNETSOCK_SEC_ALPN_FULL_LIST   ((SLNETSOCK_SEC_ALPN_H2_16 << 1 ) - 1)
 
#define SLNETSOCK_SEC_START_SECURITY_SESSION_ONLY   (1 << 0)
 
#define SLNETSOCK_SEC_BIND_CONTEXT_ONLY   (1 << 1)
 
#define SLNETSOCK_SEC_IS_SERVER   (1 << 2)
 
#define SLNETSOCK_CREATE_IF_STATE_ENABLE   (1 << 0)
 
#define SLNETSOCK_CREATE_IF_STATUS_CONNECTED   (1 << 1)
 
#define SLNETSOCK_CREATE_ALLOW_PARTIAL_MATCH   (1 << 2)
 
#define SLNETSOCK_SHUT_RD   (0)
 
#define SLNETSOCK_SHUT_WR   (1)
 
#define SLNETSOCK_SHUT_RDWR   (2)
 
#define SLNETSOCK_INET6_ADDRSTRLEN   (46)
 
#define SLNETSOCK_INET_ADDRSTRLEN   (16)
 
#define SLNETSOCK_MSG_OOB   (0x0001)
 
#define SLNETSOCK_MSG_PEEK   (0x0002)
 
#define SLNETSOCK_MSG_WAITALL   (0x0004)
 
#define SLNETSOCK_MSG_DONTWAIT   (0x0008)
 
#define SLNETSOCK_MSG_DONTROUTE   (0x0010)
 
#define SLNETSOCK_MSG_NOSIGNAL   (0x0020)
 

Typedefs

typedef struct SlNetSock_InAddr_t SlNetSock_InAddr_t
 Internet address. More...
 
typedef struct SlNetSock_In6Addr_t SlNetSock_In6Addr_t
 IpV6 or Ipv6 EUI64. More...
 
typedef struct SlNetSock_NoDelay_t SlNetSock_NoDelay_t
 The SlNetSock_NoDelay_t structure is used in SLNETSOCK_TCP_NODELAY TCP level option. More...
 
typedef struct SlNetSock_MaxSeg_t SlNetSock_MaxSeg_t
 The SlNetSock_MaxSeg_t structure is used in SLNETSOCK_TCP_MAXSEG TCP level option. More...
 
typedef struct SlNetSock_NoPush_t SlNetSock_NoPush_t
 The SlNetSock_NoPush_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option. More...
 
typedef struct SlNetSock_NoOpt_t SlNetSock_NoOpt_t
 The SlNetSock_NoOpt_t structure is used in SLNETSOCK_TCP_NOOPT TCP level option. More...
 
typedef struct SlNetSock_SackPermitted_t SlNetSock_SackPermitted_t
 The SlNetSock_SackPermitted_t structure is used in SLNETSOCK_TCP_NOPUSH TCP level option. More...
 
typedef struct SlNetSock_MaxRtt_t SlNetSock_MaxRtt_t
 The SlNetSock_MaxRtt_t structure is used in SLNETSOCK_TCP_MAXRTT TCP level option. More...
 
typedef struct SlNetSock_Keepalive_t SlNetSock_Keepalive_t
 The SlNetSock_Keepalive_t structure is used in SLNETSOCK_OPSOCK_KEEPALIVE socket level option. More...
 
typedef struct SlNetSock_NonIpBoundary_t SlNetSock_NonIpBoundary_t
 The SlNetSock_NonIpBoundary_t structure is used in SLNETSOCK_OPSOCK_NON_IP_BOUNDARY socket level option. More...
 
typedef struct SlNetSock_Winsize_t SlNetSock_Winsize_t
 The SlNetSock_Winsize_t structure is used in SLNETSOCK_OPSOCK_RCV_BUF socket level option. More...
 
typedef struct SlNetSock_Nonblocking_t SlNetSock_Nonblocking_t
 The SlNetSock_Nonblocking_t structure is used in SLNETSOCK_OPSOCK_NON_BLOCKING socket level option. More...
 
typedef struct SlNetSock_Broadcast_t SlNetSock_Broadcast_t
 The SlNetSock_Broadcast_t structure is used in SLNETSOCK_OPSOCK_BROADCAST socket level option. More...
 
typedef struct SlNetSock_SecAttribNode_t SlNetSock_SecAttribNode_t
 Secure socket attribute context. More...
 
typedef SlNetSock_SecAttribNode_t * SlNetSockSecAttrib_t
 Secure socket attribute handler. More...
 
typedef struct SlNetSock_SecureALPN_t SlNetSock_SecureALPN_t
 Secure ALPN structure. More...
 
typedef struct SlNetSock_SecureMask_t SlNetSock_SecureMask_t
 Secure Mask structure. More...
 
typedef struct SlNetSock_SecureMethod_t SlNetSock_SecureMethod_t
 Secure Method structure. More...
 
typedef struct SlNetSock_IpMreq_t SlNetSock_IpMreq_t
 The SlNetSock_IpMreq_t structure is used in SLNETSOCK_OPIP_ADD_MEMBERSHIP and SLNETSOCK_OPIP_DROP_MEMBERSHIP IP level option. More...
 
typedef struct SlNetSock_IpV6Mreq_t SlNetSock_IpV6Mreq_t
 The SlNetSock_IpV6Mreq_t structure is used in SLNETSOCK_OPIPV6_ADD_MEMBERSHIP and SLNETSOCK_OPIPV6_DROP_MEMBERSHIP IP level option. More...
 
typedef struct SlNetSock_linger_t SlNetSock_linger_t
 The SlNetSock_linger_t structure is used in SLNETSOCK_OPSOCK_LINGER socket level option. More...
 
typedef struct timeval SlNetSock_Timeval_t
 The SlNetSock_Timeval_t structure is used in the SLNETSOCK_OPSOCK_RCV_TIMEO and SLNETSOCK_OPSOCK_SND_TIMEO socket level options. More...
 
typedef uint16_t SlNetSocklen_t
 The SlNetSocklen_t is used for declaring the socket length parameter. More...
 
typedef struct SlNetSock_Addr_t SlNetSock_Addr_t
 IpV4 socket address. More...
 
typedef struct SlNetSock_AddrIn6_t SlNetSock_AddrIn6_t
 SlNetSock IPv6 address, Internet style. More...
 
typedef struct SlNetSock_AddrIn_t SlNetSock_AddrIn_t
 SlNetSock IPv4 address, Internet style. More...
 
typedef struct SlNetSock_SockAddrStorage_t SlNetSock_SockAddrStorage_t
 Generic socket address type to hold either IPv4 or IPv6 address. More...
 
typedef struct SlNetSock_SdSet_t SlNetSock_SdSet_t
 The SlNetSock_SdSet_t structure holds the sd array for SlNetSock_select function. More...
 
typedef struct SlNetSock_TransceiverRxOverHead_t SlNetSock_TransceiverRxOverHead_t
 The SlNetSock_TransceiverRxOverHead_t structure holds the data for Rx transceiver mode using a raw socket when using SlNetSock_recv function. More...
 

Enumerations

enum  SlNetSockTxInhibitThreshold_e {
  SLNETSOCK_TX_INHIBIT_THRESHOLD_MIN = 1,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_LOW = 2,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_DEFAULT = 3,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_MED = 4,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_HIGH = 5,
  SLNETSOCK_TX_INHIBIT_THRESHOLD_MAX = 6
}
 The SlNetSockTxInhibitThreshold_e enumerations is used in SLNETSOCK_OPPHY_TX_INHIBIT_THRESHOLD PHY level option. More...
 
enum  SlNetSockSecAttrib_e {
  SLNETSOCK_SEC_ATTRIB_PRIVATE_KEY = 0,
  SLNETSOCK_SEC_ATTRIB_LOCAL_CERT = 1,
  SLNETSOCK_SEC_ATTRIB_PEER_ROOT_CA = 2,
  SLNETSOCK_SEC_ATTRIB_DH_KEY = 3,
  SLNETSOCK_SEC_ATTRIB_METHOD = 4,
  SLNETSOCK_SEC_ATTRIB_CIPHERS = 5,
  SLNETSOCK_SEC_ATTRIB_ALPN = 6,
  SLNETSOCK_SEC_ATTRIB_EXT_CLIENT_CHLNG_RESP = 7,
  SLNETSOCK_SEC_ATTRIB_DOMAIN_NAME = 8,
  SLNETSOCK_SEC_ATTRIB_DISABLE_CERT_STORE = 9
}
 The SlNetSockSecAttrib_e enumerations are used to declare security attribute objects in SlNetSock_secAttribSet(). More...
 

Functions

int32_t SlNetSock_init (int32_t flags)
 Initialize the SlNetSock module. More...
 
int16_t SlNetSock_create (int16_t domain, int16_t type, int16_t protocol, uint32_t ifBitmap, int16_t flags)
 Create an endpoint for communication. More...
 
int32_t SlNetSock_close (int16_t sd)
 Gracefully close socket. More...
 
int32_t SlNetSock_shutdown (int16_t sd, int16_t how)
 Shutting down parts of a full-duplex connection. More...
 
int16_t SlNetSock_accept (int16_t sd, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen)
 Accept a connection on a socket. More...
 
int32_t SlNetSock_bind (int16_t sd, const SlNetSock_Addr_t *addr, int16_t addrlen)
 Assign a name to a socket. More...
 
int32_t SlNetSock_listen (int16_t sd, int16_t backlog)
 Listen for connections on a socket. More...
 
int32_t SlNetSock_connect (int16_t sd, const SlNetSock_Addr_t *addr, SlNetSocklen_t addrlen)
 Initiate a connection on a socket. More...
 
int32_t SlNetSock_getPeerName (int16_t sd, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen)
 Return address info about the remote side of the connection. More...
 
int32_t SlNetSock_getSockName (int16_t sd, SlNetSock_Addr_t *addr, SlNetSocklen_t *addrlen)
 Get local address info by socket descriptor. More...
 
int32_t SlNetSock_select (int16_t nsds, SlNetSock_SdSet_t *readsds, SlNetSock_SdSet_t *writesds, SlNetSock_SdSet_t *exceptsds, SlNetSock_Timeval_t *timeout)
 Monitor socket activity. More...
 
int32_t SlNetSock_sdsSet (int16_t sd, SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t SET function. More...
 
int32_t SlNetSock_sdsClr (int16_t sd, SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t CLR function. More...
 
int32_t SlNetSock_sdsClrAll (SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t ZERO function. More...
 
int32_t SlNetSock_sdsIsSet (int16_t sd, SlNetSock_SdSet_t *sdset)
 SlNetSock_select's SlNetSock_SdSet_t ISSET function. More...
 
int32_t SlNetSock_setOpt (int16_t sd, int16_t level, int16_t optname, void *optval, SlNetSocklen_t optlen)
 Set socket options. More...
 
int32_t SlNetSock_getOpt (int16_t sd, int16_t level, int16_t optname, void *optval, SlNetSocklen_t *optlen)
 Get socket options. More...
 
int32_t SlNetSock_recv (int16_t sd, void *buf, uint32_t len, uint32_t flags)
 Read data from TCP socket. More...
 
int32_t SlNetSock_recvFrom (int16_t sd, void *buf, uint32_t len, uint32_t flags, SlNetSock_Addr_t *from, SlNetSocklen_t *fromlen)
 Read data from socket. More...
 
int32_t SlNetSock_send (int16_t sd, const void *buf, uint32_t len, uint32_t flags)
 Write data to TCP socket. More...
 
int32_t SlNetSock_sendTo (int16_t sd, const void *buf, uint32_t len, uint32_t flags, const SlNetSock_Addr_t *to, SlNetSocklen_t tolen)
 Write data to socket. More...
 
int32_t SlNetSock_getIfID (uint16_t sd)
 Get interface ID from socket descriptor (sd) More...
 
SlNetSockSecAttrib_t * SlNetSock_secAttribCreate (void)
 Creates a security attributes object. More...
 
int32_t SlNetSock_secAttribDelete (SlNetSockSecAttrib_t *secAttrib)
 Deletes a security attributes object. More...
 
int32_t SlNetSock_secAttribSet (SlNetSockSecAttrib_t *secAttrib, SlNetSockSecAttrib_e attribName, void *val, uint16_t len)
 set a security attribute More...
 
int32_t SlNetSock_startSec (int16_t sd, SlNetSockSecAttrib_t *secAttrib, uint8_t flags)
 Start a security session on an opened socket. More...
 
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale