Network Services Change Log
Table of Contents
NS 2.70
Bugs
| NS-263 |
HttpClient: Connection to HTTPS web server through Proxy fails |
| NS-262 |
Improve SlNetIf_loadSecObj's parameter validation |
| NS-254 |
SlNetSock should use POSIX sem's rather than pthread_mutexes |
| NS-249 |
SlNetSock_close() leaks memory if underlying interface's close() fails |
| NS-248 |
SlNetUtil_getHostByName() should lookup IP addr names rather than delegate to lower stacks |
| NS-247 |
SlNetUtil_inetPton does not return 0 for invalid inputs or -1 for invalid family |
| NS-246 |
HTTP Server error response buffer is too small to fit its longest message |
| NS-244 |
Failed TLS handshake in HTTP Server can leak sockets |
| NS-227 |
HTTPClient gets stuck parsing headers when header data size == 256 bytes |
| NS-174 |
HTTPClient_connect() should allow users to specify acceptable security errors |
| NS-156 |
Missing typedef for struct linger in BSD layer |
| NS-103 |
SlNetIf_query() should find interfaces that are ‘Connected’, not ‘Not Disconnected’ |
Enhancements
| NS-261 |
SlNetIf_loadSecObj should enable unloading a secure object |
| NS-257 |
Add M33/M33F (TICLANG) library support |
| NS-250 |
Provide SysConfig support for generating SlNet init code |
| NS-168 |
HTTPClient should enable CC3xxx option to disable certificate store |
NS 2.60
Bugs
| NS-209 |
HTTPClient documentation missing define explanations |
| NS-188 |
MQTTClient documentation missing functions |
Enhancements
| NS-224 |
Move JSON library from Network Services to TI Utilties |
| NS-222 |
Explicitly document that NS requires an RTOS |
| NS-217 |
The HTTP Server shall support secure connections (HTTPS) |
Compatibility Notes
- To address NS-224, the JSON builder/parser that was previously managed as part of the Network Services Component is now managed in the TI Utilities Component. You will now need to look there for documentation.
NS 2.50
Bugs
| NS-178 |
Internal global variables should be static to limit scope |
| NS-177 |
SlNetIf_setPriority() may corrupt interface list |
| NS-175 |
API Reference Guide documentation issues |
| NS-93 |
timeval definition conflict between POSIX <sys/time.h> and NS <sys/select.h> |
Enhancements
| NS-184 |
Add C66 (ccs) and C647x (ccs) libraries |
| NS-183 |
Add Arm9 (ccs) libraries |
| NS-10 |
Add HTTP Server |
Compatibility Notes
- To address NS-93, the SlNetSock headers introduced a dependency on the POSIX header
<sys/time.h>. This avoids a previous conflict between time-related structures defined by both POSIX and SlNetSock - now they are all defined by POSIX. This change is often source compatible, but if you didn’t previously have the POSIX header directory on your include path, it will need to be added.
NS 2.40
Bugs
| NS-172 |
Introduce several SLNETSOCK TCP socket options |
| NS-167 |
HTTPClient reconnects fail for secure connections |
| NS-166 |
Add support for ENETDOWN in ErrnoUtil_set |
| NS-159 |
TCP_NODELAY should be defined in netinet/tcp.h |
| NS-157 |
SlNetSock_create() does not use the highest priority interface |
| NS-155 |
Memory leak in HTTPClient_connect's call to startSecureMode |
| NS-129 |
gethostbyname is not returning correct data structure |
| NS-124 |
Add support for SLNETSOCK_OPSOCK_BROADCAST socket option |
Enhancements
| NS-107 |
Add A8F (gcc), A9F (gcc), A15F (gcc), A53F (gcc) and R5F (ccs) libraries |
Compatibility Notes
- To address NS-129,
gethostbyname() now correctly complies with the POSIX spec. Users should not expect the previous, errant implementation.
- To address NS-159,
TCP_NODELAY is now correctly declared in netinet/tcp.h. Previously it was errantly declared in sys/socket.h. Users of this definition should update their code to use the new, now-POSIX-compliant header.h
NS 2.30
Bugs
| NS-136 |
accept() should return ENFILE when no more sockets available |
| NS-135 |
SlNetUtils_getHostByName() can fail when searching multiple interfaces |
| NS-133 |
Internal symbol to HTTPClient.c should be made static |
| NS-130 |
inet_ntop() should expect/accept addresses in network byte order |
| NS-128 |
Enable HTTPClient to send custom headers in HTTP requests |
| NS-126 |
Memory Leak in the JSON lib |
| NS-125 |
Closing secure sockets causes a memory leak |
| NS-118 |
getaddrinfo: IPv6 DNS resolution failure eclipses prior IPv4 DNS success |
| NS-104 |
Add getaddrinfo() and freeaddrinfo() |
| NS-94 |
getaddrinfo() doesn't support family type AF_INET6 |
Enhancements
NS 2.20
Bugs
| NS-111 |
SlNetUtil_getHostByName() ipaddr arg should be single pointer, not double pointer |
| NS-101 |
SlNetSock_secAttribSet and SlNetSock_startSec documentation needs improvement |
| NS-99 |
ADDRSTRLEN definitions (both POSIX and SLNETSOCK) are wrong |
| NS-98 |
SlNetIf_getIDByName() compares pointers when it should be comparing strings |
| NS-97 |
SlNetUtil_inetNtop() fails for IPv6 addrs |
| NS-96 |
SlNetUtil_inetNtop() fails for IPv4 addr segments equal to zero |
| NS-88 |
move NS header #includes outside of __cplusplus guards |
Enhancements
| NS-112 |
Add a utility definition to indicate enabling all ciphers |
| NS-95 |
Add JSON parser/builder |
| NS-80 |
Add HTTP Client |
| NS-4 |
Add MQTT Client and Server |
NS 2.10
Bugs
| NS-83 |
MSG_DONTWAIT needs to be a bit-field |
| NS-77 |
inet_pton() is not thread safe |
Enhancements
| NS-86 |
Add MSG_WAITALL |
| NS-82 |
SlNetUtil_getHostByName() should return interface id |
| NS-81 |
Add SNTP client |
| NS-75 |
Add sockaddr_storage and AF_UNSPEC definitions |
NS 2.00
Bugs
| NS-47 |
Add debug/release libraries support to NS product |
Enhancements
| NS-74 |
Introduce SlNetSock abstraction over network and TLS stacks |
Compatibility Notes
The Network Services Modules have been “rebooted” to improve alignment across TI’s various networking stacks. As a result, NS 2.x is completely incompatible with NS 1.x releases, and there are gaps between the features available in NS 1.x and 2.x.