MSP432E4 DriverLib API Guide  1.11.00.03
Macros | Functions
usb.c File Reference
#include <ti/devices/msp432e4/inc/msp432e411y.h>
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include "inc/hw_sysctl.h"
#include "inc/hw_usb.h"
#include "debug.h"
#include "interrupt.h"
#include "sysctl.h"
#include "udma.h"
#include "usb.h"
Include dependency graph for usb.c:

Macros

#define USB_INTEP_RX_SHIFT   16
 
#define USB_RX_EPSTATUS_SHIFT   16
 
#define EP_OFFSET(Endpoint)   (Endpoint - 0x10)
 

Functions

void USBHostSuspend (uint32_t ui32Base)
 
void USBHostReset (uint32_t ui32Base, bool bStart)
 
void USBHighSpeed (uint32_t ui32Base, bool bEnable)
 
void USBHostResume (uint32_t ui32Base, bool bStart)
 
uint32_t USBHostSpeedGet (uint32_t ui32Base)
 
uint32_t USBDevSpeedGet (uint32_t ui32Base)
 
void USBIntDisableControl (uint32_t ui32Base, uint32_t ui32Flags)
 
void USBIntEnableControl (uint32_t ui32Base, uint32_t ui32Flags)
 
uint32_t USBIntStatusControl (uint32_t ui32Base)
 
void USBIntDisableEndpoint (uint32_t ui32Base, uint32_t ui32Flags)
 
void USBIntEnableEndpoint (uint32_t ui32Base, uint32_t ui32Flags)
 
uint32_t USBIntStatusEndpoint (uint32_t ui32Base)
 
void USBIntRegister (uint32_t ui32Base, void(*pfnHandler)(void))
 
void USBIntUnregister (uint32_t ui32Base)
 
uint32_t USBEndpointStatus (uint32_t ui32Base, uint32_t ui32Endpoint)
 
void USBHostEndpointStatusClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBDevEndpointStatusClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBHostEndpointDataToggle (uint32_t ui32Base, uint32_t ui32Endpoint, bool bDataToggle, uint32_t ui32Flags)
 
void USBEndpointDataToggleClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBHostEndpointPing (uint32_t ui32Base, uint32_t ui32Endpoint, bool bEnable)
 
void USBDevEndpointStall (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBDevEndpointStallClear (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBDevConnect (uint32_t ui32Base)
 
void USBDevDisconnect (uint32_t ui32Base)
 
void USBDevAddrSet (uint32_t ui32Base, uint32_t ui32Address)
 
uint32_t USBDevAddrGet (uint32_t ui32Base)
 
void USBHostEndpointConfig (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32MaxPayload, uint32_t ui32NAKPollInterval, uint32_t ui32TargetEndpoint, uint32_t ui32Flags)
 
void USBHostEndpointSpeed (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBDevEndpointConfigSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32MaxPacketSize, uint32_t ui32Flags)
 
void USBDevEndpointConfigGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t *pui32MaxPacketSize, uint32_t *pui32Flags)
 
void USBFIFOConfigSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32FIFOAddress, uint32_t ui32FIFOSize, uint32_t ui32Flags)
 
void USBFIFOConfigGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t *pui32FIFOAddress, uint32_t *pui32FIFOSize, uint32_t ui32Flags)
 
void USBEndpointDMAConfigSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Config)
 
void USBEndpointDMAEnable (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBEndpointDMADisable (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
uint32_t USBEndpointDataAvail (uint32_t ui32Base, uint32_t ui32Endpoint)
 
int32_t USBEndpointDataGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint8_t *pui8Data, uint32_t *pui32Size)
 
void USBDevEndpointDataAck (uint32_t ui32Base, uint32_t ui32Endpoint, bool bIsLastPacket)
 
void USBHostEndpointDataAck (uint32_t ui32Base, uint32_t ui32Endpoint)
 
int32_t USBEndpointDataPut (uint32_t ui32Base, uint32_t ui32Endpoint, uint8_t *pui8Data, uint32_t ui32Size)
 
int32_t USBEndpointDataSend (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32TransType)
 
void USBFIFOFlush (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBHostRequestIN (uint32_t ui32Base, uint32_t ui32Endpoint)
 
void USBHostRequestINClear (uint32_t ui32Base, uint32_t ui32Endpoint)
 
void USBHostRequestStatus (uint32_t ui32Base)
 
void USBHostAddrSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Addr, uint32_t ui32Flags)
 
uint32_t USBHostAddrGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBHostHubAddrSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Addr, uint32_t ui32Flags)
 
uint32_t USBHostHubAddrGet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Flags)
 
void USBHostPwrConfig (uint32_t ui32Base, uint32_t ui32Flags)
 
void USBHostPwrFaultEnable (uint32_t ui32Base)
 
void USBHostPwrFaultDisable (uint32_t ui32Base)
 
void USBHostPwrEnable (uint32_t ui32Base)
 
void USBHostPwrDisable (uint32_t ui32Base)
 
uint32_t USBFrameNumberGet (uint32_t ui32Base)
 
void USBOTGSessionRequest (uint32_t ui32Base, bool bStart)
 
uint32_t USBFIFOAddrGet (uint32_t ui32Base, uint32_t ui32Endpoint)
 
uint32_t USBModeGet (uint32_t ui32Base)
 
void USBHostMode (uint32_t ui32Base)
 
void USBDevMode (uint32_t ui32Base)
 
void USBOTGMode (uint32_t ui32Base)
 
void USBModeConfig (uint32_t ui32Base, uint32_t ui32Mode)
 
void USBPHYPowerOff (uint32_t ui32Base)
 
void USBPHYPowerOn (uint32_t ui32Base)
 
void USBEndpointPacketCountSet (uint32_t ui32Base, uint32_t ui32Endpoint, uint32_t ui32Count)
 
uint32_t USBNumEndpointsGet (uint32_t ui32Base)
 
void USBClockEnable (uint32_t ui32Base, uint32_t ui32Div, uint32_t ui32Flags)
 
void USBClockDisable (uint32_t ui32Base)
 
void USBDMAChannelIntEnable (uint32_t ui32Base, uint32_t ui32Channel)
 
void USBDMAChannelIntDisable (uint32_t ui32Base, uint32_t ui32Channel)
 
uint32_t USBDMAChannelIntStatus (uint32_t ui32Base)
 
void USBDMAChannelEnable (uint32_t ui32Base, uint32_t ui32Channel)
 
void USBDMAChannelDisable (uint32_t ui32Base, uint32_t ui32Channel)
 
void USBDMAChannelConfigSet (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Endpoint, uint32_t ui32Config)
 
uint32_t USBDMAChannelStatus (uint32_t ui32Base, uint32_t ui32Channel)
 
void USBDMAChannelStatusClear (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Status)
 
void USBDMAChannelAddressSet (uint32_t ui32Base, uint32_t ui32Channel, void *pvAddress)
 
void * USBDMAChannelAddressGet (uint32_t ui32Base, uint32_t ui32Channel)
 
void USBDMAChannelCountSet (uint32_t ui32Base, uint32_t ui32Channel, uint32_t ui32Count)
 
uint32_t USBDMAChannelCountGet (uint32_t ui32Base, uint32_t ui32Channel)
 
uint32_t USBDMANumChannels (uint32_t ui32Base)
 
void USBULPIConfig (uint32_t ui32Base, uint32_t ui32Config)
 
void USBULPIEnable (uint32_t ui32Base)
 
void USBULPIDisable (uint32_t ui32Base)
 
uint8_t USBULPIRegRead (uint32_t ui32Base, uint8_t ui8Reg)
 
void USBULPIRegWrite (uint32_t ui32Base, uint8_t ui8Reg, uint8_t ui8Data)
 
void USBHostLPMSend (uint32_t ui32Base, uint32_t ui32Address, uint32_t ui32Endpoint)
 
void USBHostLPMConfig (uint32_t ui32Base, uint32_t ui32ResumeTime, uint32_t ui32Config)
 
void USBHostLPMResume (uint32_t ui32Base)
 
void USBDevLPMRemoteWake (uint32_t ui32Base)
 
void USBDevLPMConfig (uint32_t ui32Base, uint32_t ui32Config)
 
void USBDevLPMEnable (uint32_t ui32Base)
 
void USBDevLPMDisable (uint32_t ui32Base)
 
uint32_t USBLPMLinkStateGet (uint32_t ui32Base)
 
uint32_t USBLPMEndpointGet (uint32_t ui32Base)
 
bool USBLPMRemoteWakeEnabled (uint32_t ui32Base)
 
uint32_t USBLPMIntStatus (uint32_t ui32Base)
 
void USBLPMIntEnable (uint32_t ui32Base, uint32_t ui32Ints)
 
void USBLPMIntDisable (uint32_t ui32Base, uint32_t ui32Ints)
 
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale