MSP432E4 DriverLib API Guide  1.11.00.03
Macros | Functions
hibernate.c File Reference
#include "types.h"
#include <stdbool.h>
#include <stdint.h>
#include <time.h>
#include "inc/hw_hibernate.h"
#include "inc/hw_sysctl.h"
#include "debug.h"
#include "hibernate.h"
#include "interrupt.h"
#include "sysctl.h"
Include dependency graph for hibernate.c:

Macros

#define DELAY_USECS   95
 
#define LOOP_CYCLES   3
 

Functions

void HibernateEnableExpClk (uint32_t ui32HibClk)
 
void HibernateDisable (void)
 
void HibernateClockConfig (uint32_t ui32Config)
 
void HibernateRTCEnable (void)
 
void HibernateRTCDisable (void)
 
void HibernateBatCheckStart (void)
 
uint32_t HibernateBatCheckDone (void)
 
void HibernateWakeSet (uint32_t ui32WakeFlags)
 
uint32_t HibernateWakeGet (void)
 
void HibernateLowBatSet (uint32_t ui32LowBatFlags)
 
uint32_t HibernateLowBatGet (void)
 
void HibernateRTCSet (uint32_t ui32RTCValue)
 
uint32_t HibernateRTCGet (void)
 
void HibernateRTCMatchSet (uint32_t ui32Match, uint32_t ui32Value)
 
uint32_t HibernateRTCMatchGet (uint32_t ui32Match)
 
void HibernateRTCSSMatchSet (uint32_t ui32Match, uint32_t ui32Value)
 
uint32_t HibernateRTCSSMatchGet (uint32_t ui32Match)
 
uint32_t HibernateRTCSSGet (void)
 
void HibernateRTCTrimSet (uint32_t ui32Trim)
 
uint32_t HibernateRTCTrimGet (void)
 
void HibernateDataSet (uint32_t *pui32Data, uint32_t ui32Count)
 
void HibernateDataGet (uint32_t *pui32Data, uint32_t ui32Count)
 
void HibernateRequest (void)
 
void HibernateIntEnable (uint32_t ui32IntFlags)
 
void HibernateIntDisable (uint32_t ui32IntFlags)
 
void HibernateIntRegister (void(*pfnHandler)(void))
 
void HibernateIntUnregister (void)
 
uint32_t HibernateIntStatus (bool bMasked)
 
void HibernateIntClear (uint32_t ui32IntFlags)
 
uint32_t HibernateIsActive (void)
 
void HibernateGPIORetentionEnable (void)
 
void HibernateGPIORetentionDisable (void)
 
bool HibernateGPIORetentionGet (void)
 
void HibernateCounterMode (uint32_t ui32Config)
 
void HibernateCalendarSet (struct tm *psTime)
 
int HibernateCalendarGet (struct tm *psTime)
 
void HibernateCalendarMatchSet (uint32_t ui32Index, struct tm *psTime)
 
void HibernateCalendarMatchGet (uint32_t ui32Index, struct tm *psTime)
 
void HibernateTamperEventsConfig (uint32_t ui32Config)
 
void HibernateTamperEnable (void)
 
void HibernateTamperDisable (void)
 
void HibernateTamperIOEnable (uint32_t ui32Input, uint32_t ui32Config)
 
void HibernateTamperIODisable (uint32_t ui32Input)
 
void HibernateTamperEventsClear (void)
 
void HibernateTamperEventsClearNoLock (void)
 
void HibernateTamperUnLock (void)
 
void HibernateTamperLock (void)
 
uint32_t HibernateTamperStatusGet (void)
 
bool HibernateTamperEventsGet (uint32_t ui32Index, uint32_t *pui32RTC, uint32_t *pui32Event)
 
void HibernateTamperExtOscRecover (void)
 
bool HibernateTamperExtOscValid (void)
 
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale