USBLib API Guide  1.00.00.01
Typedefs | Functions
usbhhidmouse.h File Reference
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Typedefs

typedef struct tUSBHMouse tUSBHMouse
 
typedef void(* tUSBHIDMouseCallback) (tUSBHMouse *psMsInstance, uint32_t ui32Event, uint32_t ui32MsgParam, void *pvMsgData)
 

Functions

tUSBHMouseUSBHMouseOpen (tUSBHIDMouseCallback pfnCallback, uint8_t *pui8Buffer, uint32_t ui32Size)
 
uint32_t USBHMouseClose (tUSBHMouse *psMsInstance)
 
uint32_t USBHMouseInit (tUSBHMouse *psMsInstance)
 
uint32_t USBHMouseLPMSleep (tUSBHMouse *psMsInstance)
 
uint32_t USBHMouseLPMStatus (tUSBHMouse *psMsInstance)
 
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale