USBLib API Guide  1.00.00.01
Macros | Typedefs | Functions
usbhcdcserial.h File Reference
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Macros

#define USBHCDC_DEVICE_PRESENT   0x00000001
 

Typedefs

typedef struct tUSBHCDCSerial tUSBHCDCSerial
 
typedef void(* tUSBHCDCSerialCallback) (tUSBHCDCSerial *psCdcSerialInstance, uint32_t ui32Event, uint32_t ui32MsgParam, void *pvMsgData)
 

Functions

tUSBHCDCSerialUSBHCDCSerialOpen (tUSBHCDCSerialCallback pfnCallback)
 
uint32_t USBHCDCSerialClose (tUSBHCDCSerial *psCdcSerialInstance)
 
uint32_t USBHCDCSerialInit (tUSBHCDCSerial *psCdcInstance)
 
uint32_t USBHCDCGetDataFromDevice (tUSBHCDCSerial *psCdcSerialInstance, uint32_t ui32Interface)
 
uint32_t USBHCDCProcessData (tUSBHCDCSerial *psCdcSerialInstance, uint8_t ui8ArrayIndex)
 
uint32_t USBHCDCSendDataToDevice (tUSBHCDCSerial *psCdcSerialInstance, uint32_t ui32Interface, uint8_t *ui8SendBuffer, uint8_t byteSize)
 
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale