USBLib API Guide  1.00.00.01
Data Structures | Macros | Enumerations | Functions
usbdhidmouse.h File Reference
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  tHIDMouseInstance
 
struct  tUSBDHIDMouseDevice
 
struct  PACKED
 USB_CDC_GET/SET_LINE_CODING request-specific data. More...
 

Macros

#define MOUSE_REPORT_SIZE   3
 
#define MOUSE_SUCCESS   0
 This return code from USBDHIDMouseStateChange() indicates success. More...
 
#define MOUSE_ERR_TX_ERROR   2
 
#define MOUSE_ERR_NOT_CONFIGURED   4
 
#define MOUSE_REPORT_BUTTON_1   0x01
 
#define MOUSE_REPORT_BUTTON_2   0x02
 
#define MOUSE_REPORT_BUTTON_3   0x04
 

Enumerations

enum  tMouseState { eHIDMouseStateUnconfigured, eHIDMouseStateIdle, eHIDMouseStateWaitData, eHIDMouseStateSend }
 

Functions

void * USBDHIDMouseInit (uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice)
 
void * USBDHIDMouseCompositeInit (uint32_t ui32Index, tUSBDHIDMouseDevice *psMouseDevice, tCompositeEntry *psCompEntry)
 
void USBDHIDMouseTerm (void *pvMouseDevice)
 
void * USBDHIDMouseSetCBData (void *pvMouseDevice, void *pvCBData)
 
uint32_t USBDHIDMouseStateChange (void *pvMouseDevice, int8_t i8DeltaX, int8_t i8DeltaY, uint8_t ui8Buttons)
 
void USBDHIDMousePowerStatusSet (void *pvMouseDevice, uint8_t ui8Power)
 
bool USBDHIDMouseRemoteWakeupRequest (void *pvMouseDevice)
 
© Copyright 1995-2020, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale