MSP432E4 USB Library Release Notes
Introduction
The Texas Instrument USB Library is a set of data types and functions for creating USB device, host or On-The-Go (OTG) applications.
This is 1.00.00.01 version of the MSP432E4 USB Library.
Documentation
What’s New
SDK version 3.40.00.08
- Introduces SysConfig support for USB Library
- This migrates most of the effort previously needed for modifying USB settings/configuration/interfaces to a user-friendly GUI.
- See the USB RTOS examples for a template on how to use SysConfig
- Updated USB RTOS examples to utilize SysConfig
- This introduces a new convention of including auto-generated configuration files (ti_usblib_config.c/.h) instead of existing handwritten usb_*_structs.c/.h.
- Please note that this may be a compatibility break from previous projects based off USB Library examples
History
- SDK version 2.40.00.11
- Implemented USB Library files and examples for the following:
- CDC Serial Host
- Single CDC Serial Device
- HID Temperature Sensor Device
- HID Mouse Device
- Java based HIDDemo tool for communicating with HID Temperature Device
- Updated documentation
- Implemented USB Library files and examples for the following:
- SDK version 1.60.00.10
- Implemented USB Library for MSP432E4 devices
- RTOS and No RTOS examples showcasing USB Library features
- User’s Guide describing how to use the library
- API Guide showing all APIs provided in the library
Upgrade and Compatibility Information
No code compatibility breaks since only new library files and examples added. Existing library files and examples should still work without issues.
Host Support
- Windows 7, Windows 8, Windows 10
- Ubuntu 14.04 64-bit, Ubuntu 16.04 64-bit
- macOS Sierra
Device Support
- MSP432E401Y
- MSP432E411Y
Known Issues
No known issues.
Versioning
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and b is an unrestricted set of digits used as an incrementing build counter.