![]() |
![]() |
USBLib API Guide
1.00.00.01
|
Go to the source code of this file.
Data Structures | |
struct | tUSBDSensorInstance |
struct | tUSBDHIDSensorDevice |
struct | PACKED |
USB_CDC_GET/SET_LINE_CODING request-specific data. More... | |
Macros | |
#define | USBDSENSOR_SUCCESS 0 |
More... | |
#define | USBDSENSOR_TX_ERROR 1 |
#define | USBDSENSOR_NOT_CONFIGURED 2 |
The device is not currently configured and cannot perform any operations. More... | |
Enumerations | |
enum | tSensorState { eHIDSensorStateNotConnected, eHIDSensorStateIdle, eHIDSensorStateSending } |
Functions | |
tUSBDHIDSensorDevice * | USBDHIDSensorInit (uint32_t ui32Index, tUSBDHIDSensorDevice *psHIDSensorDevice) |
tUSBDHIDSensorDevice * | USBDHIDSensorCompositeInit (uint32_t ui32Index, tUSBDHIDSensorDevice *psHIDSensorDevice, tCompositeEntry *psCompEntry) |
void | USBDHIDSensorTerm (tUSBDHIDSensorDevice *psSensor) |
uint32_t | USBDHIDSensorSendReport (tUSBDHIDSensorDevice *psHIDSensor, void *pvReport, uint32_t ui32Size) |