![]() |
![]() |
|
USBLib API Guide
1.00.00.01
|

Go to the source code of this file.
Data Structures | |
| struct | tUSBDGamepadInstance |
| struct | tUSBDHIDGamepadDevice |
| struct | PACKED |
| USB_CDC_GET/SET_LINE_CODING request-specific data. More... | |
Macros | |
| #define | USBDGAMEPAD_SUCCESS 0 |
| The USBDHIDGamepadSendReport() call successfully scheduled the report. More... | |
| #define | USBDGAMEPAD_TX_ERROR 1 |
| #define | USBDGAMEPAD_NOT_CONFIGURED 2 |
| The device is not currently configured and cannot perform any operations. More... | |
Enumerations | |
| enum | tGamepadState { eHIDGamepadStateNotConnected, eHIDGamepadStateIdle, eHIDGamepadStateSending } |
Functions | |
| tUSBDHIDGamepadDevice * | USBDHIDGamepadInit (uint32_t ui32Index, tUSBDHIDGamepadDevice *psGamepad) |
| tUSBDHIDGamepadDevice * | USBDHIDGamepadCompositeInit (uint32_t ui32Index, tUSBDHIDGamepadDevice *psGamepad, tCompositeEntry *psCompEntry) |
| void | USBDHIDGamepadTerm (tUSBDHIDGamepadDevice *psGamepad) |
| uint32_t | USBDHIDGamepadSendReport (tUSBDHIDGamepadDevice *psHIDGamepad, void *pvReport, uint32_t ui32Size) |