61 #ifndef ti_drivers_aesECB_AESECBMSP432E4__include 62 #define ti_drivers_aesECB_AESECBMSP432E4__include 94 int_fast16_t returnStatus;
95 uint32_t accessTimeout;
98 } AESECBMSP432E4_Object;
Hardware-specific configuration attributes.
Definition: AESECBMSP432E4.h:79
uint8_t dummy
Definition: AESECBMSP432E4.h:80
AESECB_ReturnBehavior
The way in which ECB function calls return after performing an encryption + authentication or decrypt...
Definition: AESECB.h:352
Struct containing the parameters required for encrypting/decrypting and a message.
Definition: AESECB.h:381
void(* AESECB_CallbackFxn)(AESECB_Handle handle, int_fast16_t returnValue, AESECB_Operation *operation, AESECB_OperationType operationType)
The definition of a callback function used by the AESECB driver when used in AESECB_RETURN_BEHAVIOR_C...
Definition: AESECB.h:422
AESECB_OperationType
Enum for the operation types supported by the driver.
Definition: AESECB.h:402