95 #ifndef ti_drivers_aescbc_AESCBCMSP432E4__include 96 #define ti_drivers_aescbc_AESCBCMSP432E4__include 136 typedef struct AESCBCMSP432E4_Object {
141 int_fast16_t returnStatus;
142 uint32_t accessTimeout;
146 } AESCBCMSP432E4_Object;
void(* AESCBC_CallbackFxn)(AESCBC_Handle handle, int_fast16_t returnValue, AESCBC_Operation *operation, AESCBC_OperationType operationType)
The definition of a callback function used by the AESCBC driver when used in AESCBC_RETURN_BEHAVIOR_C...
Definition: AESCBC.h:488
Struct containing the parameters required for encrypting/decrypting a message.
Definition: AESCBC.h:420
AESCBC_ReturnBehavior
The way in which CBC function calls return after performing an encryption or decryption operation...
Definition: AESCBC.h:391
uint8_t intPriority
Definition: AESCBCMSP432E4.h:114
Hardware-specific configuration attributes.
Definition: AESCBCMSP432E4.h:113
struct AESCBCMSP432E4_HWAttrs AESCBCMSP432E4_HWAttrs
Hardware-specific configuration attributes.
AESCBC_OperationType
Enum for the operation types supported by the driver.
Definition: AESCBC.h:449