NDK 3.61.00.09 Release Notes
Table of Contents
Introduction
The Network Developer’s Kit (NDK) is a platform for development and demonstration of network enabled applications on TI embedded processors.
Depending on your platform and distribution, you may need to separately obtain an appropriate NDK Support Package (NSP).
Documentation
The following documentation is provided with this release.
What’s New
3.61.00.09
Defects
The following Defects were resolved
ID | Summary |
---|---|
NDK-392 | General documentation updates |
NDK-390 | TI toolchain versions in release notes are incorrect |
NDK-387 | NDK's general syscfg module does not pass configuration to stack init hook |
NDK-382 | NDK services create memory leak when exiting their tasks |
NDK-381 | Broken link in ConfigDoc.html's DHCP.dhcpClientPcbServer description |
NDK-380 | Users cannot rebuild A53 libraries |
Enhancements
The following Enhancements were resolved
ID | Summary |
---|---|
NDK-353 | Add M33F (TICLANG) library support |
Upgrade and Compatibility Information
NDK 3.61 is compatible with 3.60.
If updating from a previous version of NDK, see the changelog for potential upgrade and compatibility information.
A few notable feature deprecation alerts:
- The NDK’s HTTP/1.0 Server will be removed in a future release, likely in late 2019. The Network Services Component is now providing a much more fully featured HTTP/1.1 Server, which is recommended for new development. Related scripts/tools (e.g. ti/ndk/tools/binsrc) are also deprecated and are planned for removal.
- The host executables provided in ti/ndk/winapps are also deprecated. These scripts do not provide significant value, and are also planned for removal in a future release, likely in late 2019.
Host Support
- Windows
- Linux
- Mac
Dependencies
This release requires the following software components and tools versions to successfully function:
- SYS/BIOS 6.76.00.08
- Network Services 2.60.00.07
Toolchain Support
The NDK supports building libraries for the following ISA/toolchain combinations, your SDK may provide a subset of these libraries:
ISA | TI/CCS | IAR | GCC |
---|---|---|---|
C674x | 8.3.2 | N/A | N/A |
C66 | 8.3.2 | N/A | N/A |
Arm9 | 18.12.1.LTS | N/A | N/A |
A8F | N/A | N/A | gcc-arm-none-eabi-7-2017-q4-major |
A9F | N/A | N/A | gcc-arm-none-eabi-7-2017-q4-major |
A15F | N/A | N/A | gcc-arm-none-eabi-7-2017-q4-major |
A53F | N/A | N/A | gcc-linaro-7.2.1-2017.11-x86_64_aarch64-elf |
M4 | 18.12.1.LTS | N/A | N/A |
M4F | 18.12.1.LTS | 8.32.2 | gcc-arm-none-eabi-7-2017-q4-major |
R5F | 18.12.1.LTS | N/A | N/A |
Device Support
Please refer to the SDK Release Notes for device support.
Known Issues
N/A
Versioning
All releases have 4 segment versions (M.mm.pp.bb). This includes GA and pre-releases (engineering, alpha/EA, beta, etc.). Pre-releases are denoted with a suffix (e.g. 3.40.00.00_eng).
This product’s version follows a version format, M.mm.pp.bb, where M is a single digit Major number, mm is 2 digit minor number, pp is a 2 digit patch number, and bb is an unrestricted set of digits used as an incrementing build counter.
Subsequent releases of patch upgrades will be identified by the patch number. Typically, these patches only include critical bug fixes.
Technical Support
Last updated: 2019-05-16