![]() |
![]() |
Network Developers Kit API
3.61.00.09
|
Go to the source code of this file.
Macros | |
#define | NC_PRIORITY_LOW OS_SCHEDULER_LOWPRI |
#define | NC_PRIORITY_HIGH OS_SCHEDULER_HIGHPRI |
#define | NC_OPMODE_POLLING 1 |
#define | NC_OPMODE_INTERRUPT 2 |
#define | NC_OPEN_SUCCESS 0 |
#define | NC_OPEN_ILLEGAL_PRIORITY -1 |
#define | NC_OPEN_ILLEGAL_OPMODE -2 |
#define | NC_OPEN_MEMINIT_FAILED -3 |
#define | NC_OPEN_EVENTINIT_FAILED -4 |
Functions | |
int | NC_SystemOpen (int Priority, int OpMode) |
Initiate a system session. More... | |
void | NC_SystemClose () |
Shutdown the system. More... | |
int | NC_NetStart (void *hCfg, void(*NetStartCb)(), void(*NetStopCb)(), void(*NetIPCb)(uint32_t, uint32_t, uint32_t)) |
Start network. More... | |
void | NC_NetStop (int rc) |
Stop the network. More... | |