![]() |
![]() |
Network Developers Kit API
3.61.00.09
|
Go to the source code of this file.
Data Structures | |
struct | _ntparam_http |
Macros | |
#define | HTTPPORT 80 |
#define | MAX_RESPONSE_SIZE 200 |
#define | http400(Sock) httpSendErrorResponse((Sock), HTTP_BAD_REQUEST) |
#define | http404(Sock) httpSendErrorResponse((Sock), HTTP_NOT_FOUND) |
#define | http405(Sock) httpSendErrorResponse((Sock), HTTP_NOT_ALLOWED) |
#define | http501(Sock) httpSendErrorResponse((Sock), HTTP_NOT_IMPLEMENTED) |
Typedefs | |
typedef struct _ntparam_http | NTPARAM_HTTP |
Enumerations | |
enum | HTTP_STATUS_CODE { HTTP_OK =200, HTTP_NO_CONTENT =204, HTTP_BAD_REQUEST =400, HTTP_AUTH_REQUIRED =401, HTTP_NOT_FOUND =404, HTTP_NOT_ALLOWED =405, HTTP_NOT_IMPLEMENTED =501, HTTP_STATUS_CODE_END } |
Functions | |
void * | httpOpen (NTARGS *pNTA, NTPARAM_HTTP *pNTP) |
Create an instance of the HTTP Server. More... | |
void | httpClose (void *hHTTP) |
Destroy an instance of the HTTP Server. More... | |
int | httpVersion (void) |
void | httpSendClientStr (SOCKET Sock, char *Response) |
void | httpSendStatusLine (SOCKET Sock, int StatusCode, char *ContentType) |
void | httpSendFullResponse (SOCKET Sock, int StatusCode, char *RequestedFile) |
void | httpSendEntityLength (SOCKET Sock, int32_t EntityLength) |
void | httpSendErrorResponse (SOCKET Sock, int StatusCode) |
Variables | |
char * | CONTENT_TYPE_APPLET |
char * | CONTENT_TYPE_AU |
char * | CONTENT_TYPE_CSS |
char * | CONTENT_TYPE_DOC |
char * | CONTENT_TYPE_GIF |
char * | CONTENT_TYPE_HTML |
char * | CONTENT_TYPE_JPG |
char * | CONTENT_TYPE_MPEG |
char * | CONTENT_TYPE_PDF |
char * | CONTENT_TYPE_WAV |
char * | CONTENT_TYPE_ZIP |
char * | CONTENT_TYPE |
char * | CONTENT_LENGTH |
char * | CRLF |
char * | DEFAULT_NAME |
char * | HTTP_VER |
char * | SPACE |
int(* | httpErrorResponseHook )(SOCKET Sock, int StatusCode) |