Timer.h
Go to the documentation of this file.
1 /*
2  * Copyright (c) 2016-2019, Texas Instruments Incorporated
3  * All rights reserved.
4  *
5  * Redistribution and use in source and binary forms, with or without
6  * modification, are permitted provided that the following conditions
7  * are met:
8  *
9  * * Redistributions of source code must retain the above copyright
10  * notice, this list of conditions and the following disclaimer.
11  *
12  * * Redistributions in binary form must reproduce the above copyright
13  * notice, this list of conditions and the following disclaimer in the
14  * documentation and/or other materials provided with the distribution.
15  *
16  * * Neither the name of Texas Instruments Incorporated nor the names of
17  * its contributors may be used to endorse or promote products derived
18  * from this software without specific prior written permission.
19  *
20  * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21  * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22  * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23  * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24  * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25  * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26  * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27  * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28  * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29  * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30  * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31  */
32 /*!*****************************************************************************
33  * @file Timer.h
34  * @brief Timer driver
35  *
36  * @anchor ti_drivers_Timer_Overview
37  * # Overview
38  * The timer driver allows you to measure elapsed time with simple and
39  * portable APIs.This driver does not have PWM or capture functionalities.
40  * These functionalities are addressed in both the capture and PWM driver.
41  *
42  * The timer driver also handles the general purpose timer resource allocation.
43  * For each driver that requires use of a general purpose timer, it calls
44  * Timer_open() to occupy the specified timer, and calls Timer_close() to
45  * release the occupied timer resource.
46  *
47  * @anchor ti_drivers_Timer_Usage
48  * # Usage
49  *
50  * This documentation provides a basic @ref ti_drivers_Timer_Synopsis
51  * "usage summary" and a set of @ref ti_drivers_Timer_Examples "examples"
52  * in the form of commented code fragments. Detailed descriptions of the
53  * APIs are provided in subsequent sections.
54  *
55  * @anchor ti_drivers_Timer_Synopsis
56  * ## Synopsis
57  * @anchor ti_drivers_Timer_Synopsis_Code
58  * @code
59  * // Import Timer Driver definitions
60  * #include <ti/drivers/Timer.h>
61  *
62  * Timer_Handle handle;
63  * Timer_Params params;
64  *
65  * Timer_Params_init(&params);
66  * params.periodUnits = Timer_PERIOD_HZ;
67  * params.period = 1000;
68  * params.timerMode = Timer_CONTINUOUS_CALLBACK;
69  * params.timerCallback = UserCallbackFunction;
70  *
71  * handle = Timer_open(Board_TIMER0, &params);
72 
73 
74 
75  *
76  * @code
77  * // Import Timer Driver definitions
78  * #include <ti/drivers/Timer.h>
79  *
80  * Timer_Handle handle;
81  * Timer_Params params;
82  *
83  * // Initialize Timer parameters
84  * Timer_Params_init(&params);
85  * params.periodUnits = Timer_PERIOD_HZ;
86  * params.period = 1000;
87  * params.timerMode = Timer_CONTINUOUS_CALLBACK;
88  * params.timerCallback = UserCallbackFunction;
89  *
90  * // Open Timer instance
91  * handle = Timer_open(Board_TIMER0, &params);
92  *
93  * sleep(10000);
94  *
95  * Timer_stop(handle);
96  * @endcode
97  *
98  * <hr>
99  * @anchor ti_drivers_Timer_Examples
100  * # Examples
101  *
102  * @li @ref ti_drivers_Timer_Examples_open "Opening a Timer Instance"
103  * @li @ref ti_drivers_Timer_Examples_mode "Configuring Timer mode and period"
104  *
105  * @anchor ti_drivers_Timer_Examples_open
106  * ## Opening a Timer instance
107  *
108  * @code
109  * Timer_Handle handle;
110  * Timer_Params params;
111  *
112  * Timer_Params_init(&params);
113  * handle = Timer_open(Board_TIMER0, &params);
114  *
115  * if (handle == NULL) {
116  * // Timer_open() failed
117  * while (1);
118  * }
119  @endcode
120  *
121  * @anchor ti_drivers_Timer_Examples_mode
122  * ##Configuring Timer mode and period
123  *
124  * The following example code opens a timer in continuous callback mode. The
125  * period is set to 1000 Hz.
126  *
127  * @code
128  * Timer_Handle handle;
129  * Timer_Params params;
130  *
131  * Timer_Params_init(&params);
132  * params.periodUnits = Timer_PERIOD_HZ;
133  * params.period = 1000;
134  * params.timerMode = Timer_CONTINUOUS_CALLBACK;
135  * params.timerCallback = UserCallbackFunction;
136  *
137  * handle = Timer_open(Board_TIMER0, &params);
138  *
139  * if (handle == NULL) {
140  * // Timer_open() failed
141  * while (1);
142  * }
143  *
144  * status = Timer_start(handle);
145  *
146  * if (status == Timer_STATUS_ERROR) {
147  * //Timer_start() failed
148  * while (1);
149  * }
150  *
151  * sleep(10000);
152  *
153  * Timer_stop(handle);
154  * @endcode
155  *
156  * ### Initializing the Timer Driver #
157  *
158  * Timer_init() must be called before any other timer APIs. This function
159  * calls the device implementation's timer initialization function, for each
160  * element of Timer_config[].
161  *
162  * <hr>
163  * @anchor ti_drivers_Timer_Configuration
164  * # Configuration
165  *
166  * Refer to the @ref driver_configuration "Driver's Configuration" section
167  * for driver configuration information.
168  * <hr>
169 *******************************************************************************
170  */
171 
172 #ifndef ti_drivers_Timer__include
173 #define ti_drivers_Timer__include
174 
175 #include <stdint.h>
176 
177 #ifdef __cplusplus
178 extern "C"
179 {
180 #endif
181 
193 #define Timer_CMD_RESERVED (32)
194 
206 #define Timer_STATUS_RESERVED (-32)
207 
211 #define Timer_STATUS_SUCCESS (0)
212 
216 #define Timer_STATUS_ERROR (-1)
217 
225 #define Timer_STATUS_UNDEFINEDCMD (-2)
226 
230 typedef struct Timer_Config_ *Timer_Handle;
231 
242 typedef enum {
277 } Timer_Mode;
278 
285 typedef enum {
292 
302 typedef void (*Timer_CallBackFxn)(Timer_Handle handle);
303 
311 typedef struct {
313  Timer_Mode timerMode;
314 
316  Timer_PeriodUnits periodUnits;
317 
321 
323  uint32_t period;
324 } Timer_Params;
325 
330 typedef int_fast16_t (*Timer_ControlFxn)(Timer_Handle handle,
331  uint_fast16_t cmd, void *arg);
332 
337 typedef void (*Timer_CloseFxn)(Timer_Handle handle);
338 
343 typedef uint32_t (*Timer_GetCountFxn)(Timer_Handle handle);
344 
349 typedef void (*Timer_InitFxn)(Timer_Handle handle);
350 
355 typedef Timer_Handle (*Timer_OpenFxn)(Timer_Handle handle,
356  Timer_Params *params);
357 
362 typedef int32_t (*Timer_StartFxn)(Timer_Handle handle);
363 
368 typedef void (*Timer_StopFxn)(Timer_Handle handle);
369 
375 typedef struct {
378 
381 
384 
387 
390 
393 
397 
409 typedef struct Timer_Config_ {
412 
414  void *object;
415 
417  void const *hwAttrs;
418 } Timer_Config;
419 
430 extern void Timer_close(Timer_Handle handle);
431 
451 extern int_fast16_t Timer_control(Timer_Handle handle, uint_fast16_t cmd,
452  void *arg);
453 
470 extern uint32_t Timer_getCount(Timer_Handle handle);
471 
472 
483 extern void Timer_init(void);
484 
509 extern Timer_Handle Timer_open(uint_least8_t index, Timer_Params *params);
510 
523 extern void Timer_Params_init(Timer_Params *params);
524 
537 extern int32_t Timer_start(Timer_Handle handle);
538 
549 extern void Timer_stop(Timer_Handle handle);
550 
551 #ifdef __cplusplus
552 }
553 #endif
554 
555 #endif /* ti_drivers_Timer__include */
Timer_FxnTable const * fxnTablePtr
Definition: Timer.h:411
Timer_Handle(* Timer_OpenFxn)(Timer_Handle handle, Timer_Params *params)
A function pointer to a driver specific implementation of Timer_open().
Definition: Timer.h:355
Timer_CallBackFxn timerCallback
Definition: Timer.h:320
Timer_PeriodUnits
Timer period unit enum.
Definition: Timer.h:285
Timer_InitFxn initFxn
Definition: Timer.h:386
Timer_CloseFxn closeFxn
Definition: Timer.h:377
Timer_PeriodUnits periodUnits
Definition: Timer.h:316
Timer_Handle Timer_open(uint_least8_t index, Timer_Params *params)
Function to initialize a given timer peripheral specified by the index argument. The Timer_Params spe...
Definition: Timer.h:271
void Timer_init(void)
Function to initialize a timer module. This function will go through all available hardware resources...
Definition: Timer.h:287
struct Timer_Config_ Timer_Config
Timer Global configuration.
void const * hwAttrs
Definition: Timer.h:417
void Timer_Params_init(Timer_Params *params)
Function to initialize the Timer_Params struct to its defaults.
Timer Global configuration.
Definition: Timer.h:409
uint32_t(* Timer_GetCountFxn)(Timer_Handle handle)
A function pointer to a driver specific implementation of Timer_getCount().
Definition: Timer.h:343
Timer_StopFxn stopFxn
Definition: Timer.h:395
Definition: Timer.h:286
void Timer_close(Timer_Handle handle)
Function to close a timer. The corresponding timer to the Timer_Handle becomes an available timer res...
int32_t(* Timer_StartFxn)(Timer_Handle handle)
A function pointer to a driver specific implementation of Timer_start().
Definition: Timer.h:362
Definition: Timer.h:262
void(* Timer_CloseFxn)(Timer_Handle handle)
A function pointer to a driver specific implementation of Timer_close().
Definition: Timer.h:337
void * object
Definition: Timer.h:414
void(* Timer_StopFxn)(Timer_Handle handle)
A function pointer to a driver specific implementation of Timer_stop().
Definition: Timer.h:368
Timer_GetCountFxn getCountFxn
Definition: Timer.h:383
Definition: Timer.h:289
int_fast16_t Timer_control(Timer_Handle handle, uint_fast16_t cmd, void *arg)
Function performs device specific features on a given Timer_Handle.
uint32_t Timer_getCount(Timer_Handle handle)
Function to get the current count of a timer. The value returned represents timer counts...
Timer_OpenFxn openFxn
Definition: Timer.h:389
Timer_ControlFxn controlFxn
Definition: Timer.h:380
Timer Parameters.
Definition: Timer.h:311
void Timer_stop(Timer_Handle handle)
Function to stop timer. If the timer is already stopped, this function has no effect.
Timer_Mode
Timer mode settings.
Definition: Timer.h:242
The definition of a timer function table that contains the required set of functions to control a spe...
Definition: Timer.h:375
uint32_t period
Definition: Timer.h:323
Definition: Timer.h:254
int_fast16_t(* Timer_ControlFxn)(Timer_Handle handle, uint_fast16_t cmd, void *arg)
A function pointer to a driver specific implementation of Timer_control().
Definition: Timer.h:330
Timer_StartFxn startFxn
Definition: Timer.h:392
void(* Timer_CallBackFxn)(Timer_Handle handle)
Timer callback function.
Definition: Timer.h:302
void(* Timer_InitFxn)(Timer_Handle handle)
A function pointer to a driver specific implementation of Timer_init().
Definition: Timer.h:349
Definition: Timer.h:243
Timer_Mode timerMode
Definition: Timer.h:313
int32_t Timer_start(Timer_Handle handle)
Function to start the timer.
struct Timer_Config_ * Timer_Handle
A handle that is returned from a Timer_open() call.
Definition: Timer.h:230
© Copyright 1995-2019, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale