exports
tidrivers_msp432e4
source
ti
drivers
Board.h
Go to the documentation of this file.
1
/*
2
* Copyright (c) 2015-2018, Texas Instruments Incorporated
3
* All rights reserved.
4
*
5
* Redistribution and use in source and binary forms, with or without
6
* modification, are permitted provided that the following conditions
7
* are met:
8
*
9
* * Redistributions of source code must retain the above copyright
10
* notice, this list of conditions and the following disclaimer.
11
*
12
* * Redistributions in binary form must reproduce the above copyright
13
* notice, this list of conditions and the following disclaimer in the
14
* documentation and/or other materials provided with the distribution.
15
*
16
* * Neither the name of Texas Instruments Incorporated nor the names of
17
* its contributors may be used to endorse or promote products derived
18
* from this software without specific prior written permission.
19
*
20
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
21
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
22
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
23
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
24
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
25
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
26
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
27
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
28
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
29
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
30
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
31
*/
32
33
/*!****************************************************************************
34
* @file Board.h
35
* @brief Portable board-specific symbols
36
*
37
* The Board header file should be included in an application as follows:
38
* @code
39
* #include "Board.h"
40
* @endcode
41
*
42
* This header serves as device-independent interface for applications using
43
* peripherals connected to the device via standard digital interfaces; e.g,
44
* GPIO, SPI, I2C, UART, etc. Its purpose is to enable application code that
45
* references a peripheral to be portable to any device and board that
46
* supports the peripheral.
47
*
48
* ## Usage ##
49
*
50
* @anchor ti_drivers_Board_Synopsis
51
* ### Synopsis #
52
* @anchor ti_drivers_Board_Synopsis_Code
53
* @code
54
* #include "Board.h"
55
*
56
* void main(void)
57
* {
58
* Board_init();
59
* :
60
* }
61
* @endcode
62
*
63
* ## Initializing the hardware ##
64
*
65
* \p Board_init() must be called before any other driver API. This function
66
* calls the device specific initialization code that is required to as soon
67
* as possible after a device reset; e.g., to initialize clocks and power
68
* management functionality.
69
*
70
* ## Portable peripheral usage
71
*
72
* Each driver module declares symbols in \p Board.h that, if used, will
73
* improve code portability between both different devices and boards.
74
*
75
* @anchor ti_drivers_I2C_Example_portable
76
* For example, the I2C driver adds \p Board.h symbol definitions of the form
77
* * <I>bus_name</I> - the I2C bus instance ID,
78
* * <I>bus_name</I>_MAXBITRATE - the maximum supported BITRATE for the bus
79
* <I>bus_name</I>, and
80
* * Board_I2C_<I>comp_name</I>_ADDR - the slave address for the named I2C
81
* component
82
* where <I>comp_name</I> is the name given to an I2C peripheral by the
83
* board manufacturer, and <I>bus_name</I> is the user defined name of the
84
* I2C bus instance. These symbols enable applications to portably acquire
85
* an I2C bus handle and control an I2C slave on that bus.
86
* @code
87
* #include <ti/drivers/I2C.h>
88
* #include "Board.h"
89
*
90
* // portably open an I2C bus instance
91
* I2C_Params i2cParams;
92
* I2C_Params_init(&i2cParams);
93
* i2cParams.bitRate = Board_I2C0_MAXBITRATE; // bus name == Board_I2C0
94
* i2cHandle = I2C_open(Board_I2C0, &i2cParams);
95
*
96
* // portably read from an I2C slave
97
* I2C_Transaction trans;
98
* trans.slaveAddress = Board_I2C_TMP006_ADDR; // component name = TMP006
99
* trans.readBuf = ...;
100
* trans.readCount = ...;
101
* trans.writeCount = 0;
102
* I2C_transfer(i2cHandle, &trans);
103
* @endcode
104
******************************************************************************
105
*/
106
107
#ifndef ti_boards_Board__include
108
#define ti_boards_Board__include
109
110
#ifdef __cplusplus
111
extern
"C"
{
112
#endif
113
128
extern
void
Board_init
(
void
);
129
130
#ifdef __cplusplus
131
}
132
#endif
133
134
#endif
/* ti_boards_Board_include */
Board_init
void Board_init(void)
Performs "early" board-level initialization required by TI-DRIVERS.
© Copyright 1995-2019
, Texas Instruments Incorporated. All rights reserved.
Trademarks
|
Privacy policy
|
Terms of use
|
Terms of sale