81 #ifndef ti_drivers_aesgcm_AESGCMMSP432E4__include 82 #define ti_drivers_aesgcm_AESGCMMSP432E4__include 122 typedef struct AESGCMMSP432E4_Object {
124 int_fast16_t returnStatus;
127 uint32_t accessTimeout;
130 } AESGCMMSP432E4_Object;
AESGCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESGCM.h:480
void(* AESGCM_CallbackFxn)(AESGCM_Handle handle, int_fast16_t returnValue, AESGCM_Operation *operation, AESGCM_OperationType operationType)
The definition of a callback function used by the AESGCM driver when used in AESGCM_RETURN_BEHAVIOR_C...
Definition: AESGCM.h:519
AESGCM_ReturnBehavior
The way in which GCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESGCM.h:399
uint8_t intPriority
Definition: AESGCMMSP432E4.h:100
struct AESGCMMSP432E4_HWAttrs AESGCMMSP432E4_HWAttrs
Hardware-specific configuration attributes.
Hardware-specific configuration attributes.
Definition: AESGCMMSP432E4.h:99
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a me...
Definition: AESGCM.h:428