71 #ifndef ti_drivers_aesctr_AESCTRMSP432E4__include 72 #define ti_drivers_aesctr_AESCTRMSP432E4__include 112 typedef struct AESCTRMSP432E4_Object {
117 int_fast16_t returnStatus;
118 uint32_t accessTimeout;
121 } AESCTRMSP432E4_Object;
struct AESCTRMSP432E4_HWAttrs AESCTRMSP432E4_HWAttrs
Hardware-specific configuration attributes.
AESCTR_OperationType
Enum for the operation types supported by the driver.
Definition: AESCTR.h:436
AESCTR_ReturnBehavior
The way in which CTR function calls return after performing an encryption or decryption operation...
Definition: AESCTR.h:380
uint8_t intPriority
Definition: AESCTRMSP432E4.h:90
Struct containing the parameters required for encrypting/decrypting a message.
Definition: AESCTR.h:412
Hardware-specific configuration attributes.
Definition: AESCTRMSP432E4.h:89
void(* AESCTR_CallbackFxn)(AESCTR_Handle handle, int_fast16_t returnValue, AESCTR_Operation *operation, AESCTR_OperationType operationType)
The definition of a callback function used by the AESCTR driver when used in AESCTR_RETURN_BEHAVIOR_C...
Definition: AESCTR.h:480