108 #ifndef ti_drivers_aesccm_AESCCMMSP432E4__include 109 #define ti_drivers_aesccm_AESCCMMSP432E4__include 149 typedef struct AESCCMMSP432E4_Object {
151 int_fast16_t returnStatus;
154 uint32_t accessTimeout;
157 } AESCCMMSP432E4_Object;
Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a me...
Definition: AESCCM.h:446
Hardware-specific configuration attributes.
Definition: AESCCMMSP432E4.h:126
struct AESCCMMSP432E4_HWAttrs AESCCMMSP432E4_HWAttrs
Hardware-specific configuration attributes.
void(* AESCCM_CallbackFxn)(AESCCM_Handle handle, int_fast16_t returnValue, AESCCM_Operation *operation, AESCCM_OperationType operationType)
The definition of a callback function used by the AESCCM driver when used in AESCCM_RETURN_BEHAVIOR_C...
Definition: AESCCM.h:539
uint8_t intPriority
Definition: AESCCMMSP432E4.h:127
AESCCM_OperationType
Enum for the operation types supported by the driver.
Definition: AESCCM.h:500
AESCCM_ReturnBehavior
The way in which CCM function calls return after performing an encryption + authentication or decrypt...
Definition: AESCCM.h:417