60 #ifndef ti_drivers_i2c_I2CMSP432E4__include 61 #define ti_drivers_i2c_I2CMSP432E4__include 71 #include <ti/devices/msp432e4/inc/msp432.h> 73 #include <ti/devices/msp432e4/driverlib/gpio.h> 74 #include <ti/devices/msp432e4/driverlib/pin_map.h> 76 #include <ti/drivers/dpl/SemaphoreP.h> 77 #include <ti/drivers/dpl/HwiP.h> 112 #define I2CMSP432E4_PB2_I2C0SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 2, GPIO_PB2_I2C0SCL) 117 #define I2CMSP432E4_PB3_I2C0SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 3, GPIO_PB3_I2C0SDA) 122 #define I2CMSP432E4_PG0_I2C1SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 0, GPIO_PG0_I2C1SCL) 127 #define I2CMSP432E4_PR0_I2C1SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 0, GPIO_PR0_I2C1SCL) 132 #define I2CMSP432E4_PG1_I2C1SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 1, GPIO_PG1_I2C1SDA) 137 #define I2CMSP432E4_PR1_I2C1SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 1, GPIO_PR1_I2C1SDA) 142 #define I2CMSP432E4_PL1_I2C2SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTL, 1, GPIO_PL1_I2C2SCL) 147 #define I2CMSP432E4_PP5_I2C2SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 5, GPIO_PP5_I2C2SCL) 152 #define I2CMSP432E4_PN5_I2C2SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 5, GPIO_PN5_I2C2SCL) 157 #define I2CMSP432E4_PG2_I2C2SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 2, GPIO_PG2_I2C2SCL) 162 #define I2CMSP432E4_PR2_I2C2SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 2, GPIO_PR2_I2C2SCL) 167 #define I2CMSP432E4_PL0_I2C2SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTL, 0, GPIO_PL0_I2C2SDA) 172 #define I2CMSP432E4_PN4_I2C2SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTN, 4, GPIO_PN4_I2C2SDA) 177 #define I2CMSP432E4_PP6_I2C2SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTP, 6, GPIO_PP6_I2C2SDA) 182 #define I2CMSP432E4_PG3_I2C2SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 3, GPIO_PG3_I2C2SDA) 187 #define I2CMSP432E4_PR3_I2C2SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 3, GPIO_PR3_I2C2SDA) 192 #define I2CMSP432E4_PK4_I2C3SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 4, GPIO_PK4_I2C3SCL) 197 #define I2CMSP432E4_PG4_I2C3SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 4, GPIO_PG4_I2C3SCL) 202 #define I2CMSP432E4_PR4_I2C3SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 4, GPIO_PR4_I2C3SCL) 207 #define I2CMSP432E4_PK5_I2C3SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 5, GPIO_PK5_I2C3SDA) 212 #define I2CMSP432E4_PG5_I2C3SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 5, GPIO_PG5_I2C3SDA) 217 #define I2CMSP432E4_PR5_I2C3SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 5, GPIO_PR5_I2C3SDA) 222 #define I2CMSP432E4_PK6_I2C4SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 6, GPIO_PK6_I2C4SCL) 227 #define I2CMSP432E4_PG6_I2C4SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 6, GPIO_PG6_I2C4SCL) 232 #define I2CMSP432E4_PR6_I2C4SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 6, GPIO_PR6_I2C4SCL) 237 #define I2CMSP432E4_PK7_I2C4SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTK, 7, GPIO_PK7_I2C4SDA) 242 #define I2CMSP432E4_PG7_I2C4SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTG, 7, GPIO_PG7_I2C4SDA) 247 #define I2CMSP432E4_PR7_I2C4SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTR, 7, GPIO_PR7_I2C4SDA) 252 #define I2CMSP432E4_PB0_I2C5SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 0, GPIO_PB0_I2C5SCL) 257 #define I2CMSP432E4_PB4_I2C5SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 4, GPIO_PB4_I2C5SCL) 262 #define I2CMSP432E4_PB1_I2C5SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 1, GPIO_PB1_I2C5SDA) 267 #define I2CMSP432E4_PB5_I2C5SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 5, GPIO_PB5_I2C5SDA) 272 #define I2CMSP432E4_PA6_I2C6SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 6, GPIO_PA6_I2C6SCL) 277 #define I2CMSP432E4_PB6_I2C6SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 6, GPIO_PB6_I2C6SCL) 282 #define I2CMSP432E4_PA7_I2C6SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 7, GPIO_PA7_I2C6SDA) 287 #define I2CMSP432E4_PB7_I2C6SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTB, 7, GPIO_PB7_I2C6SDA) 292 #define I2CMSP432E4_PD0_I2C7SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 0, GPIO_PD0_I2C7SCL) 297 #define I2CMSP432E4_PA4_I2C7SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 4, GPIO_PA4_I2C7SCL) 302 #define I2CMSP432E4_PD1_I2C7SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 1, GPIO_PD1_I2C7SDA) 307 #define I2CMSP432E4_PA5_I2C7SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 5, GPIO_PA5_I2C7SDA) 312 #define I2CMSP432E4_PD2_I2C8SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 2, GPIO_PD2_I2C8SCL) 317 #define I2CMSP432E4_PA2_I2C8SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 2, GPIO_PA2_I2C8SCL) 322 #define I2CMSP432E4_PD3_I2C8SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTD, 3, GPIO_PD3_I2C8SDA) 327 #define I2CMSP432E4_PA3_I2C8SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 3, GPIO_PA3_I2C8SDA) 332 #define I2CMSP432E4_PA0_I2C9SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 0, GPIO_PA0_I2C9SCL) 337 #define I2CMSP432E4_PE6_I2C9SCL GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 6, GPIO_PE6_I2C9SCL) 342 #define I2CMSP432E4_PA1_I2C9SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTA, 1, GPIO_PA1_I2C9SDA) 347 #define I2CMSP432E4_PE7_I2C9SDA GPIOMSP432E4_pinConfigMask(GPIOMSP432E4_PORTE, 7, GPIO_PE7_I2C9SDA) size_t writeCountIdx
Definition: I2CMSP432E4.h:461
I2CMSP432E4 Hardware attributes.
Definition: I2CMSP432E4.h:406
volatile I2CMSP432E4_Mode mode
Definition: I2CMSP432E4.h:448
I2CMSP432E4 Object.
Definition: I2CMSP432E4.h:431
Structure used to perform I2C bus transfers.
Definition: I2C.h:431
uint32_t intNum
Definition: I2CMSP432E4.h:410
I2C_Transaction * tailPtr
Definition: I2CMSP432E4.h:455
uint32_t intPriority
Definition: I2CMSP432E4.h:412
I2C_TransferMode transferMode
Definition: I2CMSP432E4.h:442
uint32_t sdaPin
Definition: I2CMSP432E4.h:416
enum I2C_TransferMode_ I2C_TransferMode
Specifies the behavior of I2C_Transfer().
uint8_t masterCode
Definition: I2CMSP432E4.h:423
uint8_t bitRate
Definition: I2CMSP432E4.h:458
I2CMSP432E4_Mode
I2CMSP432E4 mode.
Definition: I2CMSP432E4.h:359
Definition: I2CMSP432E4.h:363
Definition: I2CMSP432E4.h:362
bool isOpen
Definition: I2CMSP432E4.h:464
const I2C_FxnTable I2CMSP432E4_fxnTable
The definition of an I2C function table that contains the required set of functions to control a spec...
Definition: I2C.h:589
uint32_t baseAddr
Definition: I2CMSP432E4.h:408
struct I2CMSP432E4_Object_ I2CMSP432E4_Object
I2CMSP432E4 Object.
uint8_t * writeBufIdx
Definition: I2CMSP432E4.h:460
SemaphoreP_Handle mutex
Definition: I2CMSP432E4.h:433
I2C_CallbackFxn transferCallbackFxn
Definition: I2CMSP432E4.h:445
uint8_t * readBufIdx
Definition: I2CMSP432E4.h:462
struct I2CMSP432E4_HWAttrs_ I2CMSP432E4_HWAttrs
I2CMSP432E4 Hardware attributes.
size_t readCountIdx
Definition: I2CMSP432E4.h:463
SemaphoreP_Handle transferComplete
Definition: I2CMSP432E4.h:436
void(* I2C_CallbackFxn)(I2C_Handle handle, I2C_Transaction *transaction, bool transferStatus)
I2C callback function prototype.
Definition: I2C.h:502
HwiP_Handle hwiHandle
Definition: I2CMSP432E4.h:439
I2C_Transaction * currentTransaction
Definition: I2CMSP432E4.h:451
uint32_t sclPin
Definition: I2CMSP432E4.h:414
I2C_Transaction * headPtr
Definition: I2CMSP432E4.h:454
Inter-Integrated Circuit driver interface.
Definition: I2CMSP432E4.h:361
Definition: I2CMSP432E4.h:360