bool selected
Definition: checkbox.h:46
struct Graphics_CheckBox Graphics_CheckBox
This structure defines the characteristics of a Checkbox.
This structure describes a font used for drawing text onto the screen.
Definition: grlib.h:189
uint16_t yPosition
Definition: checkbox.h:45
Graphics_Context g_sContext
void Graphics_drawSelectedCheckBox(const Graphics_Context *context, const Graphics_CheckBox *checkBox)
Definition: checkbox.c:157
This structure defines the characteristics of a Checkbox.
Definition: checkbox.h:42
uint8_t numbOfChar
Definition: checkbox.h:51
uint32_t selectedColor
Definition: checkbox.h:50
uint8_t gap
Definition: checkbox.h:47
uint32_t backgroundColor
Definition: checkbox.h:49
bool Graphics_isCheckBoxSelected(const Graphics_CheckBox *checkBox, uint16_t x, uint16_t y)
Definition: checkbox.c:130
uint16_t xPosition
Definition: checkbox.h:44
const Graphics_Font * font
Definition: checkbox.h:52
uint32_t textColor
Definition: checkbox.h:48
void Graphics_drawCheckBox(const Graphics_Context *context, const Graphics_CheckBox *checkBox)
Definition: checkbox.c:58
int8_t * text
Definition: checkbox.h:53
void Graphics_drawReleasedCheckBox(const Graphics_Context *context, const Graphics_CheckBox *checkBox)
Definition: checkbox.c:196