#include <stdint.h>
#include <stdbool.h>
Go to the source code of this file.
Functions | |
void | SysTickEnable (void) |
void | SysTickDisable (void) |
void | SysTickIntRegister (void(*pfnHandler)(void)) |
void | SysTickIntUnregister (void) |
void | SysTickIntEnable (void) |
void | SysTickIntDisable (void) |
void | SysTickPeriodSet (uint32_t ui32Period) |
uint32_t | SysTickPeriodGet (void) |
uint32_t | SysTickValueGet (void) |